Solid Edge Part Type Library
Vent Object Members
Overview 
Public Methods
Public Method DeleteDeletes the referenced object.
Public Method GetBoundaryCurvesReturns the boundary curves for the referenced object.
Public Method GetDimensionsReturns the Dimensions collection object for the referenced object.
Public Method GetRibCurvesReturns the rib curves for the referenced object.
Public Method GetSparCurvesReturns the spar curves.
Public Method GetStatusExReturns the status of the specified object.
Public Method GetStyleReturns the feature style.
Public Method RangeReturns the high and low range values for the referenced object.
Public Method ReorderInserts the referenced object in front of or behind another feature.
Public Method RollToFeatureRolls the referenced Model object back to a specified feature.
Public Method SetBoundaryCurvesSets the boundary curves for the referenced object.
Public Method SetRibCurvesSets the rib curves for the referenced object.
Public Method SetSparCurvesSets the spar curves.
Public Method SetStyleSets the feature style.
Public Properties
Public Property ApplicationReturns the active application object.
Public Property AttributeSetsReturns the AttributeSets collection object for the referenced object.
Public Property DisplayNameThis read-only String property returns the display name for the referenced object.
Public Property DraftAngleSpecifies the draft angle.
Public Property DraftEnabledSpecifies whether draft is enabled.
Public Property DraftFromOutsideEdgesSpecifies how draft angle is measured for the referenced object.
Public Property DraftSideSpecifies the draft side.
Public Property EdgebarNameThis read-only property returns the Edgebar name of the referenced object.
Public Property EdgesReturns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces.
Public Property ExtentDepthSets and returns the extent depth.
Public Property ExtentSideSets and returns the extent side.
Public Property ExtentTypeSets and returns the extent type.
Public Property FacesReturns a collection of faces of a specified type that belong to a model, a feature, or a topology object.
Public Property FacesByRayReturns a collection of faces that are intersected by a specified vector.
Public Property IsAttributeSetPresentReturns True if a specified Attribute Set exists on the referenced object.
Public Property ModelingModeTypeReturns the modeling mode of the referenced object.
Public Property NameReturns the name of the referenced object.
Public Property ParentReturns the parent object for the referenced object.
Public Property RibDepthSpecifies the rib depth.
Public Property RibExtensionSpecifies the distance the ribs extend past the exterior boundary.
Public Property RibOffsetSpecifies the distance the ribs are offset from the entrance surface.
Public Property RibThicknessSpecifies the rib thickness.
Public Property RoundEnabledSpecifies whether rounding is enabled for the referenced object.
Public Property RoundRadiusSpecifies the round radius.
Public Property ShowDimensionsControls the display of dimensions for the feature object.
Public Property SparDepthSpecifies the spar depth.
Public Property SparExtensionSpecifies the distance the spars extend past the exterior boundary.
Public Property SparOffsetSpecifies the distance the spars are offset from the entrance surface.
Public Property SparThicknessSpecifies the spar thickness.
Public Property StatusReturns the status of the specified object.
Public Property SuppressTemporarily suppresses the referenced object.
Public Property SuppressVariableReturns the suppress variable object.
Public Property SystemNameThis read-only String property returns the system name for the referenced object.
Public Property TypeSpecifies the type of the object being referenced.
Public Property VisibleSpecifies whether or not the referenced object is displayed to the screen.
See Also

Vent Object