Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
DisplayName | This read-only String property returns the display name for the referenced object. |
EdgebarName | This read-only property returns the Edgebar name of the referenced object. |
Edges | Returns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces. |
ExtentType | Sets and returns the extent type for the referenced object. |
Faces | Returns a collection of faces of a specified type that belong to a model, a feature, or a topology object. |
FacesByRay | Returns a collection of faces that are intersected by a specified vector. |
FiniteDepth | Sets and returns the depth of the referenced WebNetwork object. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
ModelingModeType | Returns the modeling mode of the referenced object. |
Name | Returns the name of the referenced object. |
Parent | Returns the parent object for the referenced object. |
Profile | Sets and returns the Profile object used to construct the referenced feature object. |
ProfileExtensionType | Sets and returns the extend mode of the profile from which the referenced object was constructed. |
ShowDimensions | Controls the display of dimensions for the feature object. |
Status | Returns the status of the specified object. |
Suppress | Temporarily suppresses the referenced object. |
SuppressVariable | Returns the suppress variable object. |
SystemName | This read-only String property returns the system name for the referenced object. |
Thickness | Sets and returns the thickness of the referenced feature object. |
Type | Specifies the type of the object being referenced. |
Visible | Specifies whether or not the referenced object is displayed to the screen. |
WebDirection | Sets and returns the direction the profile is to be projected to form the body of the rib. |