| Solid Edge Part Type Library : WeldRevolvedCutout Object |
Delete | Deletes the referenced object. |
GetInputModels | Returns the objects that are input to the weldment feature. |
GetProfiles | Returns the profiles associated with the referenced feature object. |
GetRangeByModel | Returns the range of a part occurrence specified by an input model. |
GetStatusEx | Returns the status of the specified object. |
GetStyleByModel | Returns an object that describes the style of the referenced feature. |
SetProfiles | Sets the profiles associated with the referenced feature object. |
SetStyle | Sets the feature style. |
Angle | Sets and returns the angular rotation of the referenced object. |
Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
Axis | Sets and returns the Axis object about which the referenced object revolves. |
DisplayName | This read-only String property returns the display name for the referenced object. |
EdgebarName | This read-only property returns the Edgebar name of the referenced object. |
ExtentSide | Sets and returns the reference plane side for the referenced object. |
ExtentType | Sets and returns the extent type for the referenced object. |
GetBottomCapsByModel | Returns a collection of bottom cap faces for the specified model. |
GetEdgesByModel | Returns the edges of a part occurrence specified by the input model. |
GetFacesByModel | Returns the faces of a part occurrence specified by the input model. |
GetFacesByModelAndRay | Returns the faces of a part occurrence specified by the input model and a ray. |
GetSideFacesByModel | Returns a collection of side faces of the weldment feature from the specified model. |
GetTopCapsByModel | Returns a collection of top cap faces of the weldment feature for the specified model. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
Name | Returns the name of the referenced object. |
Parent | Returns the parent object for the referenced object. |
ProfileSide | Sets and returns the side of the profile to which material is added or removed. |
ShowDimensions | Controls the display of dimensions for the feature object. |
Status | Returns the status of the specified object. |
Suppress | Temporarily suppresses the referenced object. |
SystemName | This read-only String property returns the system name for the referenced object. |
Type | Specifies the type of the object being referenced. |