StructureEditor Namespace
Application Object Members
Overview 
Public Methods
Public Method GetBOMViewSetInCombo 
Public Method GetDisplayAlertsThis API is used to get the status of display alerts property whether it is ON or OFF.
Public Method QuitThis API is used to quit the structure editor application.
Public Method SetBOMViewInCombo 
Public Method SetDisplayAlertsThis API is used to set the display alerts property ON or OFF. If this property is ON then certain alerts and messages will be displayed while the application is running. If this property is OFF then the operation will be performed silently without any alerts and messages.
Public Properties
Public Property Application 
Public Property Parent 
Public Property SEECStructureEditor 
Public Property SEECStructureEditorATP 
Public Property Visible 
See Also

Application Object