Solid Edge ST7 SDK
Solid Edge V16 SP1 - Readme

--------------
Legal Notices
--------------
© 2004,
UGS Corp.

All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of UGS Corp.; which is protected by
copyright and trade secret law.  Such materials may not be reproduced or
transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of
the Software License Agreement, or as specifically authorized in writing by
UGS Corp.

UGS Corp.
5800 Granite Parkway
Suite 600
Plano, TX. 75024

--------------------
End of Legal Notices
--------------------

--------------
Release Notes:
--------------

Product:        Solid Edge
Version:        16.00.01.05
Date:           08-OCT-2004

This release of Solid Edge has been certified to run on the following:
 • Windows 2000 Professional® operating system running Service Pack 4.
 • Windows XP Professional® operating system running Service Pack 1 or 2.
 • Internet Explorer 6.0 or higher


This Update should be installed on top of Solid Edge Version 16.00.00.63.


--------------------
End of Release Notes
--------------------

---------------------------------
Update 1 addresses the following:
---------------------------------

=====Assembly=====

PR 2040689: Fixed a crash during delete of a frame part reference outside the context of frame edit
PR 5025209: Fixed a crash on exit after saving an assembly to UG Bookmark.
PR 5025369: Fixed a crash observed when replacing alternate assembly components.
PR 5028318: Fixed a crash during Phong displays that can occur when formatting face styles.
PR 5028578: Fixed a crash during pipe edit.
PR 5029146: Fixed a crash when selecting cross sections in Frames with QuickPick
PR 1347438: Fixed a problem with parts disappearing when applying a subassembly config.
PR 2031584: Fixed a display problem with PathFinder in Assembly and work area
PR 4864191: Fixed a problem where imported styles and body styles were not displayed in Web Publisher.
PR 4996692: Fixed a clipping problem when switching FOA members.
PR 5012273: Fixed a problem where changing a Top Hole randomly changes bolt type
PR 5017867: Fixed a problem with delete and undo where pipe routes are concerned.
PR 5017932: Fixed a problem where modifying the radius override end condition for Frame was not working.
PR 5019957: Fixed a problem where some parts would move to an invalid location in higher level assemblies.
PR 5020369: Fixed a problem with pipe segment lengths during edit of a pipe.
PR 5020473: Fixed a problem where incorrect Frame length was reported in Draft
PR 5020701: Fixed a problem where the wrong bolt was getting placed after update
PR 5020834: Fixed a problem with segments flipping when using them to create pipe routes.
PR 5020974: Fixed a problem with placing Y fittings in a Pipe-route.
PR 5021406: Fixed a problem where alternate Components is not available for Dynamic Configuration
PR 5021414: Fixed a problem where automatic placement of pipe fittings does not work with custom fittings.
PR 5021686: Fixed a problem with losing styles and assembly features while in-place active in a subassembly.
PR 5022224: Fixed a problem where 2 different sized return fittings are being placed when only 1 should be
PR 5022513: Fixed a problem where the second part placed from the handbook fails to update the frame window.
PR 5023158: Fixed a performance problem with highlighting pipe routes.
PR 5023793: Fixed a problem with placing of fittings at free ends of a pipe route.
PR 5025117: Fixed a problem where Assembly open would get in a loop and never open
PR 5025211: Fixed a problem where you cannot save AP/FOA assemblies to PLMXML
PR 5025676: Fixed a problem where Piping is not defaulting to Pipe Penetration cut if no fitting is assigned
PR 5025679: Fixed a problem were FOA UI is disabled when doing Edit-Open of FOA member
PR 5026479: Fixed a problem where a bolt is placed upside-down if Din 6798 J Washer is used
PR 5027102: Fixed a problem of washer disappearing after reordering during edit.
PR 5027650: Fixed a problem where auto positioning in Structural Frames is not working with Butt joint
PR 5027967: Fixed a problem where the FS group is not failed on opening FOA file.
PR 5028529: Fixed a crash when transferring part from top-level to subassembly
PR 5029359: Fixed a problem where Edit was available for Frames in Subassemblies.
PR 5029401: Fixed a crash when editing an assembly feature
PR 1252236: Fixed a problem in WebPub where part colors missing in published assembly.
PR 1327156: Modified Expand to open hidden subassemblies.
PR 2040623: Fixed a problem where the computation of cut lengths for frames is incorrect.
PR 5025172: Disabled pattern occurrence entries in the Alternate Assemblies table editing UI.
PR 5029344: Fixed a problem where cross-sections of frames could not be seen in an IPA assembly.
PR 5031340: Fixed a problem in trimming circular frames wrt to the previous frame parts
PR 1344312: Fixed a problem with assembly patterns not working with construction surface patterns
PR 5035316: Fixed a problem where the arrow keys do not work when modifying a frame cross-section
PR 5037107: Fixed a problem where you cannot Edit Profile Dimensions of Assembly Features
PR 5037167: Fixed a problem where you are unable to generate Standard Parts on French locale
PR 5037897: Fixed a problem where you are unable to add a custom part in French Standard parts
PR 5035324: Updated translations for Japanese version Standard Parts
PR 5037471: Fixed a Layout problem (string too long) in French Part Editor (std parts) i/f
PR 5032214 : Fixed a problem with the Autoconfig.txt for ATI mobility series
PR 5037972: Fixed a problem where Predefined scenes do not render properly.
PR 2041700: Fixed a problem where placing system library will abort.
PR 5042449: Fixed a problem where certain asm files would not open because a ref plane had missing parents
PR 5046867: Fixed a problem where using the "parts currently shown" report option is also listing hidden parts.

=====Part=====

PR 5027706: Enabled ThinWall in Design and Drafting.
PR 5026193: Fixed a crash while editing a sketch.
PR 1349115: Fixed a problem where patterned information was not being mirrored.
PR 2040749: Fixed a performance problem when a lot of style information is applied on part faces.
PR 5016894: Fixed a problem where part of the model is no longer visible after SmartBoss cmd.
PR 5022702: Added support for reading NX3 files into Solid Edge
PR 5027517: Fixed a crash that occurred when opening a draft file.
PR 2039338: Fixed a crash when closing custom properties.
PR 5033272: Fixed a problem where a feature created using Select from Sketch could not be copied.
PR 4876050: Fixed a problem with the size of the status bar in Part.
PR 4984593: Fixed a scaling problem in Sat translator.
PR 5033912: Fixed a problem in GetAlternateBody method for automation
PR 5036327: Fixed a problem where pickquick items do not highlight when placing components
PR 5038277: Fixed a problem getting a system error performing an undo after changing a variable name
PR 5039536: Fixed a problem to insure that the version number is set properly for the oldest hole attribute definition.
PR 5043197: Fixed a problem where License Wizard was generating an incorrect server_id feature line.
PR 1307170: Fixed a problem where using RMB in the Move/Copy command is causing problems.
PR 5038498: Fixed a problem where Trim Corner was only trimming an arc in one direction.

=====Draft=====

PR 1346865: Fixed a crash that occurred copying section views in some cases.
PR 5027724: Fixed a problem that would cause Draft files to crash on file open.
PR 1346232: The problem where the dimensions on broken views are showing wrong values
PR 2040152: Fixed a problem a center mark moves after detaching when the draft is re-opened
PR 4954919: Fixed a problem where the API DrawingView.Annotation fails with automation error
PR 4993403: Fixed a problem where flow lines of an exploded view of an assembly fail to export to AutoCAD
PR 5018254: Fixed a problem of 2d polylines importing as jagged continuous lines
PR 5018652: Fixed a problem where AutoCAD control characters preceding text strings on imported DWG files
PR 5020426: Fixed a problem where dimension tolerance text is importing large
PR 5021336: Fixed a problem of angular dimensions importing improperly.
PR 5021337: Fixed a problem where a parts list balloon didn't show 'N/A' for an excluded part.
PR 5021468: Fixed a problem where View Alignment between 2 model views is easily broken
PR 5022402: Fixed a problem with shaded drawing view and pipes in a pipe route
PR 5022834: Fixed a problem where parts list with excluded parts updates incorrectly.
PR 5023901: Fixed a problem where template parts list could not be repopulated
PR 5026528: Fixed a problem were arc boundary for hatch being created incorrectly for imported dwg files
PR 5026862: Fixed a problem where invisible attributes are importing as visible.
PR 5027043: Fixed a problem where dimensions increase in size when saved using different view scale.
PR 1350350: Fixed a problem where parts list starts with item number 5 instead of 1
PR 5029109: Fixed a problem where Dimensions are in error after save and reopening the draft file.
PR 5039377: Disable automatic drawing view creation in the layout product.
PR 1353107: Fixed a problem where lines are disoriented when converting from mds to Solid Edge.
PR 5040284: Fixed a problem getting double balloon numbers updating a view.
PR 5041641: Fixed a crash that occurred when the Area Properties command was run multiple times.

=====API=====

PR 5026448: Fixed a problem with exposed variables API
PR 2041126: Fixed a problem with contour flange creation via API.
PR 2041523: Fixed a problem installing assemblies to GAC if .NET Framework is not installed.

=====Insight=====

PR 1332317: Fixed a problem with floating point Error with SEPartX
PR 5027247: Fixed a crash when saving to pcf after taking measurements
PR 5022366: Fixed a problem where BOM view is not working for WebParts.
PR 5025866: Fixed a problem opening a .htm file by double clicking from windows explorer.
PR 5030689: Fixed a problem where you can not use an underscore as a Revision Delimiter
PR 5034919: Fixed a problem where an assembly file will not migrate - Add to Library aborts.
PR 5028424: Fixed a problem with "where used" finding draft files that cannot be rename even though option is set
PR 5031387: Fixed a problem where after revising a file, the new file does not show up in Delete From Library dialog
PR 5039517: Fixed a problem of slow open performance when cache is not populated.
PR 5043347: Fixed a problem with property names not displaying as localized using webparts.
PR 5045916: Fixed a problem where secure links is searching for existing broken links
PR 5044104: Fixed a problem where, a warning was logged for "Value in the document was retained because value in the library was empty"


---
End
---