Solid Edge ST7 SDK
Solid Edge V16 SP9 - Readme

--------------
Legal Notices
--------------
© 2005,
UGS Corp.

All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of UGS Corp.; which is protected by
copyright and trade secret law.  Such materials may not be reproduced or
transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of
the Software License Agreement, or as specifically authorized in writing by
UGS Corp.

UGS Corp.
5800 Granite Parkway
Suite 600
Plano, TX. 75024

--------------------
End of Legal Notices
--------------------

--------------
Release Notes:
--------------

Product:        Solid Edge
Version:        16.00.09.02
Date:           31-Aug-2005

This release of Solid Edge has been certified to run on the following:
 • Windows 2000 Professional® operating system running Service Pack 4.
 • Windows XP Professional® operating system running Service Pack 1 or 2.
 • Internet Explorer 6.0 or higher


This Update should be installed on top of Solid Edge Version:
16.00.00.63, 16.00.01.05, 16.00.02.04, 16.00.03.04, 16.00.04.03, 16.00.05.02,
16.00.06.03, 16.00.07.04, 16.00.08.02


--------------------
End of Release Notes
--------------------

------------------------------------
This Update addresses the following:
------------------------------------

=====Assembly=====

PR 1401263: Fixed a problem where Solid Edge crashes in VS+ after SaveAsImage.
PR 1403241: Fixed a problem in which you could not save the file after creating a CAM constraint.
PR 1404524: Fixed a problem with portions of a weldment being absent when placed in an assembly.
PR 1406724: Fixed a problem where selection of faces is not possible after replacing asm with pwd
PR 1409665: Fixed a problem where Editing dimensions in XpresRoute let other dims change to zero
PR 5177957: Fixed a problem where new parts were visible after applying a config.
PR 5158354: Fixed a problem where an Assembly driven part hole features had missing holes after edit
PR 2049631: Fixed a problem where assembly had bad links that could not be deleted
PR 1392663: Fixed a problem where a macro fails to create interpar t constructions
PR 2049631: Fixed a problem that will allow clean up invalid links created by variant sites.
PR 5158354: Fixed a problem where Assembly driven part hole features had missing holes after edit

=====Part=====

PR 1403796: Fixed a problem that caused an abort when populating FOP members.
PR 5199297: Fixed a problem where Solid Edge hangs when updating Solid Edge Admin file location.
PR 5232029: Fixed a crash when solving detached dimensions (missing geometry parent).
PR 1398448: Fixed a problem that cuased an out of memory message using copy/paste in profile.
PR 1412596: Fixed a problem where a part copy did not update when the FOP member was changed.
PR 2047371: Fixed a problem with License-File List, for users with both admin and non-admin privileges.
PR 2049678: Fixed a problem that caused Solid Edge to hang in 'GoTo' while rolling back to the last feature.
PR 5206402: Changed the message that displays when an out of memory condition occurs during file open.
 
=====Draft=====

PR 1394050: Fixed a problem that caused crashes with many cases when updating Drawing Views.
PR 1405887: Fixed a problem where Solid Edge crashed when opening certain .DFT files.
PR 5208393: Fixed many crashes based on Crashlog files caputed and submitted to Solid Edge.
PR 1390217: Fixed a problem with detached dimensions after copy / paste drawing views.
PR 1412886: Fixed a problem where some dimensions are disappearing on file open.

=====API=====

PR 1412431: Added DrawingView.IsBroken API to indicate if a view is in the broken state.
PR 1392663: Fixed a problem where a macro failed to create interpart constructions.
PR 1410684: Fixed a problem where an addin could encounter an invalid argument exception when working with the edgebar.
PR 1406741: UpdateAll automation api updates only the modified documents when debug registry switch UPDATE_ALLMODIFIED_DOCUMENTS is set to 1.

=====Insight=====

PR 5164307: "Open in Dashboard" menu will now be shown if the user Right clicks on Share point URL in search results.


---
End
---