Solid Edge ST7 SDK
Solid Edge V17 SP14 - Readme

--------------
Legal Notices
--------------
© 2006,
UGS Corp.

All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of UGS Corp.; which is protected by
copyright and trade secret law.  Such materials may not be reproduced or
transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of
the Software License Agreement, or as specifically authorized in writing by
UGS Corp.

UGS Corp.
5800 Granite Parkway
Suite 600
Plano, TX. 75024

--------------------
End of Legal Notices
--------------------

--------------
Release Notes:
--------------

Product:        Solid Edge
Version:        17.00.14.01
Date:           14-Sep-2006


This release of Solid Edge has been certified to run on the following:
 • Windows 2000 Professional® operating system running Service Pack 4.
 • Windows XP Professional® operating system running Service Pack 1 or 2.
 • Internet Explorer 6.0 or higher

This Update can be instaled installed on top of Version:
17.00.00.65, 17.00.01.06, 17.00.02.04, 17.00.03.04, 17.00.04.03, 17.00.05.03,
17.00.06.03, 17.00.07.03, 17.00.08.03, 17.00.09.03, 17.00.10.02, 17.00.11.03,
17.00.12.01, or 17.00.13.01


Note: Updates are all inclusive and can be installed on top of the base release
or any released UPdate.


--------------------
End of Release Notes
--------------------

------------------------------------
This Update addresses the following:
------------------------------------

=====Assembly=====
 
PR 5559905: Fixed a problem that caused a crash in JAsmSmartLocateCmd
PR 5562290: Fixed a problem that caused a crash in JDocOle::Set/GetClientSite
PR 5562502: Added code to prevent crashes while accessing stale pointers.
PR 5564472: Fixed a problem that caused a crash in JOLEMembassy methods
PR 1530114: Fixed a problem where a specific file could not be opened.
PR 5190469: Fixed a problem where Sharpen Display setting #5 (finest setting) is not working correctly
 
=====Part=====
 
PR 5562358: Fixed an abort based on crashlog info.
PR 5569600: Fixed a problem that caused a crash in SignificantEvents::MouseTrackHook
PR 1482704: Fixed a problem where Insert > Partcopy (FOP) causes to insert wrong members
PR 2067805: Fixed a problem where element highlighted incorrectly by Include command.
PR 5561336: Fixed a problem where MRU list created with bad characters in place of http
 
=====Draft=====
 
PR 2065591: Fixed a problem that caused an abort when manipulating objects.
PR 2068664: Fixed a problem that caused an abort when updating hole table.

---
End
---