Solid Edge ST7 SDK
Solid Edge V17 SP3 - Readme

--------------
Legal Notices
--------------
© 2005,
UGS Corp.

All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of UGS Corp.; which is protected by
copyright and trade secret law.  Such materials may not be reproduced or
transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of
the Software License Agreement, or as specifically authorized in writing by
UGS Corp.

UGS Corp.
5800 Granite Parkway
Suite 600
Plano, TX. 75024

--------------------
End of Legal Notices
--------------------

--------------
Release Notes:
--------------

Product:        Solid Edge
Version:        17.00.03.04
Date:           04-Aug-2005

This release of Solid Edge has been certified to run on the following:
 • Windows 2000 Professional® operating system running Service Pack 4.
 • Windows XP Professional® operating system running Service Pack 1 or 2.
 • Internet Explorer 6.0 or higher


This Update should be installed on top of Solid Edge Version:
17.00.00.65, 17.00.01.06, 17.00.02.04


--------------------
End of Release Notes
--------------------

------------------------------------
This Update addresses the following:
------------------------------------

=====Assembly=====

PR 5209985: Fixed a problem where Render Mode editor (in VS+) is causing an abort.
PR 1404650: Fixed a problem with incorrect part names being displayed in the relationship list in ribbon bar.
PR 5138419: Fixed a problem where assembly cutout fails to place with hidden subassemblies
PR 5177957: Fixed a problem with new parts being visible after applying a config.
PR 5198053: Fixed a problem where Assembly locks up selecting STATUS tab on Properties dialog
PR 1410084: Fixed a problem where System Library was not getting placed in Design & Drafting or Academic.
PR 5204617: Fixed a problem where you were unable to pattern parts based on a weldment
PR 5169324: Fixes a problem where some assembly hole features are not displaying.
PR 5176583: Fixes a problem with not being able to locate parts when using the relationship commands from the 'Relationships' toolbar.

=====Part=====

PR 1402241: Fixed a problem in which you could not include reference planes while in-place activated.
PR 1408108: Fixed a problem with callout "Bend angle - property text"
PR 5210892: Fixed a problem with value rounding and/or truncation due to precision readout.
PR 5220673: Fixed a problem where adding special characters in the material name empties the material table.
PR 1401079: Corrected a problem accessing the Hardware property via ExtendedSummaryInformation.
PR 1411296: Fixed a problem with recognizing perpendicular relationship in Intellisketch.
PR 5187061: FLEXlm License Administrator Server Status crash has been fixed.
PR 5210008: FLEXlm License Administrator Server Status crash has been fixed.
PR 2049678: Fixes a problem with goto feature hanging.
PR 5225616: Fixed a file-specific crash when copying Fill/Hatch style.
 
=====Draft=====

PR 1405887: Fixed a problem where v16 and v17 was crashing when certain .DFT files were displayed.
PR 5208393: Fixed a series of random aborts, based on crashlogs, during document transition.
PR 1390217: Fixed a problem with detached dimensions after a copy / paste of a drawing view.
PR 1398799: Fixed a problem where extra information is exported to DXF
PR 1404575: Fixed a problem where dimensions are moving to origin.
PR 1409224: Fixed a problem where "hidden edge display" option is not honoring the global setting in section views.
PR 5181132: Fixed a problem where pipe fittings associated with a v16 sub-assembly pipe route would disappear.
PR 5190218: Fixed a problem where section view won't update if source view is deleted.
PR 5217362: Revert to pre V17 behavior which displays a 1 digit number for status in property text and parts list.
 
=====API=====

PR 1412415: Method "GetDocNum" now succeeds if used in C++
PR 5228326: Fixes a problem with stitch surface api getsurfaces.

=====Insight=====

PR 1409451: Fixed a problem where members were not shown for PSM master files.
PR 5194631: Fixed a problem where a rename of a file with a link to itself would fail.
PR 5202070: Fixed a problem where Insight Connect would not open STL files in View and Markup.

---
End
---