Solid Edge ST7 SDK
Solid Edge V17 SP5 - Readme

--------------
Legal Notices
--------------
© 2005,
UGS Corp.

All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of UGS Corp.; which is protected by
copyright and trade secret law.  Such materials may not be reproduced or
transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of
the Software License Agreement, or as specifically authorized in writing by
UGS Corp.

UGS Corp.
5800 Granite Parkway
Suite 600
Plano, TX. 75024

--------------------
End of Legal Notices
--------------------

--------------
Release Notes:
--------------

Product:        Solid Edge
Version:        17.00.05.03
Date:           28-Sep-2005


This release of Solid Edge has been certified to run on the following:
 • Windows 2000 Professional® operating system running Service Pack 4.
 • Windows XP Professional® operating system running Service Pack 1 or 2.
 • Internet Explorer 6.0 or higher


This Update should be installed on top of Solid Edge Version:
17.00.00.65, 17.00.01.06, 17.00.02.04, 17.00.03.04, 17.00.04.03


--------------------
End of Release Notes
--------------------

------------------------------------
This Update addresses the following:
------------------------------------

=====Assembly=====

PR 1383720: Fixed a problem that caused a crash when creating an assembly cutout feature.
PR 5249028: Fixed a problem that caused a crash using Close and Return on several documents after IPA.
PR 1416842: Fixed a problem with part naming for multiple occurrences of standard parts
PR 1418627: Fixed a problem with adding custom parts created in V15 to V17 standard parts database.
PR 2049631: Fixed a problem with invalid links created by variant sites.
PR 1352921: Fixed a problem with "Activate all" performance
PR 1420008: Fixed a problem with updating of associative sketches that contain patterns.
PR 2053234: Fixed a problem of updating sub occurrence objects after "Unload Hidden parts" is used.
PR 5310192: Fixed a problem with error assistant.
PR 5314556: Fixed a problem with the CMM-based IDeas->SE Migration process.

=====Part=====

PR 1413130: Fixed a problem with interpart copy performance with lots of faces to copy.
PR 1413586: Fixed a problem with the calculation of Mass in Inspect->Physical Properties.
PR 2052767: Fixed a problem with chain locate
PR 5224755: Fixed a problem where closing part documents was not releasing memory.
PR 1419494: Fixed a problem where features were not correctly oriented after placing a feature library
PR 1420976: Fixed a problem that caused SE to hang.
PR 1444931: Fixed a problem where Draft Face Analysis was storing the draft direction.
PR 5314218: Fixed aborts based on reported via auto crashlog
PR 5314625: Fixed a problem where density values persist across locales.
PR 1445781: Fixed a problem where Save as Flat creates incorrect geometry.
 
=====Draft=====

PR 5313912: Fixed a problem where "Convert to 2d View" generates blank views.
PR 2047719: Fixed a problem that caused an abort when saving to dxf or dwg using layer and attribute mapping.
PR 1416584: Fixed a problem where dimensions attached to bspline curves fail on opening document in V17.
PR 1416996: Fixed a problem with the display of surface texture symbols
PR 5303209: Fixed a problem where some older draft files would not open.
PR 5312519: Fixed a problem that caused copy/paste to fail for some drawing views.

=====API=====

PR 5302500: Fixed a problem where DeleteHoles.Add no longer works.
PR 1419792: Provided an API for Draft to fix the bend radius problem.
PR 2052477: Fixed a problem with the display of dimension changing when GetDisplayData method is used.

---
End
---