Solid Edge ST7 SDK
Solid Edge V18 SP1 - Readme

--------------
Legal Notices
--------------
© 2005,
UGS Corp.

All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of UGS Corp.; which is protected by
copyright and trade secret law.  Such materials may not be reproduced or
transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of
the Software License Agreement, or as specifically authorized in writing by
UGS Corp.

UGS Corp.
5800 Granite Parkway
Suite 600
Plano, TX. 75024

--------------------
End of Legal Notices
--------------------

--------------
Release Notes:
--------------

Product:        Solid Edge
Version:        18.00.01.08
Date:           14-Dec-2005


This release of Solid Edge has been certified to run on the following:
    • Windows XP Professional® operating system (32-bit) running Service Pack 2
    • Windows XP Professional® operating system (64-bit) running on EM64T hardware
    • Windows 2000 Professional® operating system running Service Pack 4
    • Internet Explorer 6.0 or higher

This Update should be installed on top of Solid Edge Version:
18.00.00.69


--------------------
End of Release Notes
--------------------

------------------------------------
This Update addresses the following:
------------------------------------

=====Assembly=====

Note: SEEC = Solid Edge Embedded Client

PR 5337783: Fixed a problem where changing a revision filter caused a crash.
PR 5338604: Fixed a problem that caused a crash when performing Insert Part Copy.
PR 5346549: Fixed a problem where executing a search which is not saved would cause a crash in SEEC .
PR 5348527: Fixed a crash when editing a failed Groove weld when clicking in the select method drop list
PR 5330898: Fixed a problem where the definition for Alternate Positions of Assembly is not saved.
PR 5335106: Fixed a problem where new revision cache status was not displayed correctly.
PR 5335168: Fixed a problem where cache Assistant was showing checked out status, instead of Modified status
PR 5335303: Fixed a problem where synchronize was not working correctly on XP.
PR 5335576: Fixed a problem where delete All does not remove all files
PR 5339319: Fixed a problem where display Configurations not saved.
PR 5339365: Fixed a problem where Drag and Drop an Asm file in Draft does not create Valid Drawing Views.
PR 5340876: Fixed a problem when saving a new file user cannot change action.
PR 5341221: Fixed a problem with BOM synchronization for new assembly.
PR 5341222: Fixed a problem where a Part file in the assembly is shown as Read-only.
PR 5341947: Fixed a problem where Save as allows creation of New revision with Restrict Revision By Group
PR 5342212: Fixed a problem where Update Status Info command doesn't update status info
PR 5342496: Fixed a problem where Property list not updated on Search dialog
PR 5342518: Fixed a problem where Open Lookin not updated to show Saved Search name
PR 5342846: Fixed a problem where Selecting Cancel on login dialog doesn't stop command
PR 5343083: Fixed a problem where on the Common Properties dialog user can turn on a second Action column
PR 5343554: Fixed a problem where Undocheckout sets the status to Unknown instead of Up-to-date
PR 5343586: Fixed a problem when trying to revise, the on the Upload screen the Item name is blank
PR 5343932: Fixed a problem where Assign All does not work for the revision dialog
PR 5344305: Fixed a problem where User is given write-access error trying to save multiple new files
PR 5345714: Fixed a problem where Closing X143001_B.asm leaves SEEC is a hung state
PR 5346345: Fixed a problem where Teamcenter Managed Templates missing-shows C: drive
PR 5346539: Fixed a problem where Cache status incorrect after doing Checkin All
PR 5346622: Fixed a problem where Activation override option works only when Saved as Default.
PR 5348221: Fixed a problem where Key "EnableTcFavorites"=dword:00000001 is not set if we have TcX
PR 5349044: Fixed a problem where File Checkin with Action Upload Document Causes Check-In.
PR 5349060: Fixed a problem where saving Physical Property displays "Unable to determine Dataset type from extension" message.
PR 5349065: Fixed a problem where FOA member status not displayed in the Assembly Pathfinder.
PR 5349841: Fixed a problem where New document revision remains checked out after closing the document.
PR 5349848: Fixed a problem where PSE Synchronization is broken.
PR 5350950: Fixed a problem where Delete from cache does not remove all files associated with that file
PR 5351890: Fixed a problem where File properties not assigned to draft file.
PR 2055667: Fixed a problem where Can not open Sub assembly from Main assembly
PR 5342145: Fixed a problem where Place Part is not honoring the simplified setting on the library tab
PR 5342753: Fixed a problem where File Open dialog do no remember last Column Sort preference.
PR 5343054: Fixed a problem where Teamcenter Parts Library tab missing when opening an assembly from TcE
PR 5352645: Fixed a problem where Cache Assist should show TcE release status
PR 1468239: Fixed a problem activating a display configuration of a subassembly
PR 5345815: Fixed a problem where Position of Revision Column on Common Property dialog Keeps Changing.
PR 5348651: Fixed a problem where FOA not behaving correctly when changing members.
PR 5349577: Fixed a problem where Assembly features not showing graphically in the display.
PR 5349722: Fixed a problem where Insight managed asm always uploads on close
PR 5349838: Fixed a problem where Status not shown on applying Update status info for the second time.
PR 5350764: Fixed a problem where doing an Update status info after synchronize shows synchronize did not work
PR 5354818: Fixed a problem where you Checkout an assembly that is already open in causes Undo-Checkout.
PR 5354822: Fixed a problem that caused a Crash when canceling FOA member Select dialog.
PR 5354824: Fixed a problem when creating a new revision of FOA Member
PR 5356007: Fixed a problem that caused a Crash opening Assembly imported using Bulkloader.
PR 5355466: Fixed a problem where that caused a crash during a specific customer workflow
PR 5319655: Fixed a problem where The Update Status Info does not work for few changes made by another user.
PR 5355927: Fixed a problem where Common Property Dialog is not displayed following Save/Close
PR 5355952: Fixed a problem where Common Property Dialog, Type column changes value on Save
PR 5356085: Fixed a problem where Obtain TcE Release Status during "Update Status Info" and store in ixf file
PR 5356247: Fixed a problem where File status shown in green in Cache assistant & not in pathfinder.
PR 5356251: Fixed a problem where Incorrect Revision rule Text in path finder when asm is opened Read Only.
PR 5356356: Fixed a problem where During performance testing the close actions is taking longer then in EMv4
PR 5356892: Fixed a problem where file listed with no properties after deleting from cache.
PR 2055300: Fixed a problem where problem inactivating a large assembly.
PR 2059763: Fixed a problem where Several Windows Show Up by Collapsing All windows
PR 5356184: Fixed a problem that caused a crash creating new revisions from cache Assistant -> Show Revisions
PR 5359294: Fixed a problem with performance - memory increases when resizing pathfinder
PR 5348127: Fixed a problem where you get an Out of memory when selecting property for view.
PR 5354838: Fixed a problem where Change in the SEStatus is not reflected after Performing Update Status Info.
PR 5356233: Fixed a problem where File shown Checked out even when opened as Read only.
PR 5357633: Fixed a problem where SEEC does not respect EM_item_type
PR 5357675: Fixed a problem where Reset connection + Select Connection Dir + File New does not download Templates
PR 5357693: Fixed a problem where New revision listed in Cache Assistant but not in Pathfinder.
PR 5360203: Fixed a problem that caused a Crash Canceling Image Browse for Render Setup.
PR 1470190: Fixed a problem where Problems with Simplified Assemblies and Pattern of Parts.
PR 1471061: Fixed a problem where patterns get lost when switching to "use designed assembly"
PR 5332470: Fixed a problem where Extra lines display on context menu
PR 5345272: Fixed a problem where RMC on an inactive file then clicking in space causes file to activate
PR 5356888: Fixed a problem where No Tc Feature Lib tab when the .par file is opened from the .asm file.
PR 5357635: Fixed a problem where Cache Assistant Dialog resize behavior.
PR 5359300: Fixed a problem where Mirror ASM save to Teamcenter produces Insight Message box
PR 5360211: Fixed a problem where assembly is not opened with Selected Display Configuration.
PR 5360875: Fixed a problem where the Check Out Reason and Change ID is swapped when written to Teamcenter.
PR 2059883: Fixed a problem where Solid Edge aborted when Undo command was used
PR 5358201: Fixed a problem where Save Selected Model aborts Solid Edge
PR 5360879: Fixed a problem where User Visible crash Uploading Part Created In-Place after doing Inter-Part Copy.
PR 2059865: Fixed a problem where A hidden part stays showing in the view
PR 5348841: Fixed a problem where adding a 2nd draft get "filename conflicts" warning
PR 5360928: Fixed a problem where Same icon shown for .par & .dft files in the "Revisions" dialog.
PR 5360945: Fixed a problem where Part file is Checked out even after closing.

=====Part=====

PR 5340319: Fixed a problem where The Newly Created + Saved + Closed SE documents remain Checked Out
PR 5342580: Fixed a problem where Hourglass not displayed while processing common prop dialog
PR 5342599: Fixed a problem where Selecting Cancel on Folder dialog clears folder on common property dialog
PR 5346537: Fixed a problem where After doing upload the status is "Checked out to" and not "Checked out to you"
PR 1466602: Fixed a problem where changing material name does not fire off recompute for custom formula.
PR 5346552: Fixed a problem where Saving a FOP requires you to save each part twice
PR 5357637: Fixed a problem where Divide Part - Save Selected Files does not persist to Teamcenter
PR 5357700: Fixed a problem where The file is not uploaded if opened again after switching to new connection
PR 5358476: Fixed a problem where The File opened from Tc Part Lib remains Checked out after file closure.
PR 5350733: Fixed a problem where Tapered Pipe Thread doesn’t properly generate
PR 5358511: Fixed a problem where Item ID not displayed for the part created as a member of FOP.
PR 5359284: Fixed a problem where managed data memory 100+M larger than Unmanaged
PR 2059707: Fixed a problem that caused an Abort right after shortcut menu comes up
PR 5359864: Fixed a problem that cased a crash during a "close and return" after canceling FeMap Express
PR 2059862: Fixed a problem where Feature commands are disabled.
PR 2059864: Fixed a problem where the direction of the offset face does not change
PR 5363366: Fixed a problem where File Properties not listed for the members of FOP.

=====Draft=====

PR 5335033: Fixed a problem where No Block View for Symbol is selected in My Searches on TcE Symbol Lib.
PR 5337465: Fixed a problem where AutoCAD block is repositioned on import of dwg file.
PR 5345069: Fixed a problem where It is possible to save two draft docs under same Item ID with same file name.
PR 5348562: Fixed a problem that caused an abort when not letting SE determine thread axis tolerance
PR 5348833: Fixed a problem where Item name not pre-populated when creating draft.
PR 5350457: Fixed a problem where Placing Feature Control Frame is causing abort
PR 5341095: Fixed a problem where Independent detail views on sheet metal flat patterns are empty or rotated.
PR 5342511: Fixed a problem where long dimension text in off-center location causes dimension line to shorten.
PR 5344868: Fixed a problem where Line connector isn't connecting properly to the end terminator.
PR 5345985: Fixed a problem where Detached center marks are not being reported in Dimension Tracker
PR 5360263: Fixed a problem where Surface Lay symbol does not move when number of triangles is increased.
PR 5361248: Fixed a problem where you cannot open a draft file saved in V18
PR 5353116: Fixed a problem where Import AutoCAD options not working correctly
PR 5364049: Fixed a problem where File -> Check-In of new created Assembly Draft Lists xyz.dft.tmp in Upload dlg.

=====API=====

PR 5353233: Fixed a problem underdefined property not implemented on the SKETCH API

=====Insight=====

PR 5347229: Fixed a problem where Update Status info fails if there is a new file in cache
PR 1470129: Fixed a problem where Typical not accepted LCA workflow (slow, lots of warnings, lots of user input)
PR 5339914: Fixed a problem where Cache Assistant is showing Up-to-date status after exiting and restarting
PR 5347635: Fixed a problem where Property Manager does not list any FOP Children when in the master file
PR 5348653: Fixed a problem where Double clicking on managed pcf is not working correctly
PR 5355559: Fixed a problem with computed column and get deep list
PR 1472103: Fixed a problem where add-to-lib stops with an internal Error.
PR 5353054: Fixed a problem where you can't do a full text search on draft file.
PR 1471917: Fixed a problem where Connection to Library failed error going from LCA Step 1 to Step 2
PR 5193105: Fixed a problem where Trying to change a Part Copy of an NX2 w/NX3 file in a SE .par file.
PR 5361319: Fixed a problem where contents of a lib need to be sorted for view and selection
PR 5362558: Fixed a problem where Transaction log file location wrong after changing cache location
 
---
End
---