Solid Edge ST7 SDK
Solid Edge V18 SP2 - What's New
Problem Reports
Item Description
PR 5365704 Fixed a problem that caused a crash in CUnknownEnumDataHolder::SetData.
PR 5368064 Fixed a problem where .NET addins fail to add their menus and toolbars.
PR 2059928 Enhancements have been made to the Application Display Automation controls to allow programmatic selection of Application Display settings.
PR 5362288 Properties and methods have been added to the assembly automation objects SegmentDistanceRel ation3d, SegmentRadiusRelation3d, SegmentAngularRelation3d and SegmentTangentRelation3d so that additional information about these objects can be obtained. The method GetPathSegmentsRelations has been added to the Tube automation object so that the segment relations of a tubes path can easily be found.
New APIs
SolidEdgeAssembly
SolidEdgeConstants
See Also