Solid Edge ST7 SDK
Solid Edge V18 SP6 - Readme

--------------
Legal Notices
--------------
© 2006,
UGS Corp.

All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of UGS Corp.; which is protected by
copyright and trade secret law.  Such materials may not be reproduced or
transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of
the Software License Agreement, or as specifically authorized in writing by
UGS Corp.

UGS Corp.
5800 Granite Parkway
Suite 600
Plano, TX. 75024

--------------------
End of Legal Notices
--------------------

--------------
Release Notes:
--------------

Product:        Solid Edge
Version:        18.00.06.06
Date:           14-Jun-2006


This release of Solid Edge has been certified to run on the following:
    • Windows XP Professional® operating system (32-bit) running Service Pack 2
    • Windows XP Professional® operating system (64-bit) running on EM64T hardware
    • Windows 2000 Professional® operating system running Service Pack 4
    • Internet Explorer 6.0 or higher


This Update can be instaled installed on top of Version: 18.00.00.69, 18.00.01.08,
18.00.02.04, 18.00.03.04, 18.00.04.07 or 18.00.05.05.


Note: Updates are all inclusive and can be installed on top of the base release
or any released UPdate.

Note: PR#5434509 was uncovered while preparing to release / post Update 4. A decision
was made to release Update 4 with this known issue. - - PR#5434509: When Hide Previous
Level is enabled, parts cannot be graphically (geometry in the screen) located in a
subassy that has been in-place activated. Workaround: You can locate these parts by;
turning off Hide Previous Level, or locate them in path-finder, or by dragging the
cursor to create a small fence locate. This will be addressed in V18 Update 5.


--------------------
End of Release Notes
--------------------

------------------------------------
This Update addresses the following:
------------------------------------

=====Assembly=====

PR 5444208: Fixed a problem where SE aborts while trying to edit a stitch weld feature.
PR 2065675: Fixed a problem with the Construction Display button not working for subassemblies.
PR 5433768: Fixed a problem where patterned parts are not positioned properly when assembly features are involved
PR 5442338: Fixed a problem where deleting an adjustable part from one FOA member deletes graphically from all members
PR 5449039: Fixed a problem where you cannot add values to the title field of family members
PR 5418443: Added a new "NO_LINK_RESOLUTION" property on the Revision Manager Object.
PR 5449513: Fixed a problem where Solid Edge aborts using save all members on the FOA tab
PR 5517684: Fixed a problem where Solid Edge aborts when selecting a assembly feature inside a pattern.
PR 5423370: Fixed a problem where you are unable to open assembly file
PR 1406244: Fixed a problem where coordinate system based constraints fail.
PR 1452134: Fixed a problem where setting the time caused the wrong date in custom properties
PR 2065830: Fixed a problem where the date changes when clicking on date property.
PR 5522477: Fixed a problem where part highlight is in the wrong location.
PR 5440957: Fixed a problem where parts disappear when activated.
PR 1498424: Fixed a problem where LinkMgnt.txt Search Path will not be used to solve broken links to texture files
PR 1514832: Fixed a problem using a German or French SE, Standard Parts name is in English in Asm pathfinder
PR 1525896: Fixed a problem where the user is not being to open a file.
PR 2066585: Fixed a problem where the user is not being able to IPA into a part.
PR 5512146: Fixed a problem where Assembly files would not open.
PR 5526217: Deliver registry files to control FlashFit as default relationship option.
PR 5532307: Fixed a problem where the connect value can not be changed via variable table.

=====Part=====

PR 1507306: Fixed a problem where deleting a cutout causes other unrelated features to get a warning.
PR 1510680: Fixed a problem where a part is not displaying when it contains a Part Copy.
PR 1516445: Fixed a problem where the calculation of physical properties gives incorrect results
PR 5359018: Fixed a problem where associative feature extents are created even if the Interpart options are off.
PR 5528413: Fixed a problem where the profile or feature fails after profile edit
PR 1498677: Fixed a problem where Material Table is not keeping bend radius for new gages in metric sheet metal files
PR 5386408: Fixed a problem where unsuppressing a pattern after parameters that control the pattern have changed.

=====Draft=====

PR 1512029: Fixed a problem where a V17 draft file aborts when opened in V18
PR 1496752: Fixed a problem where automatic center lines were causing a file save failure.
PR 1510415: Fixed a problem where a Draft file failed to save after adding a callout or detail view
PR 1510437: Fixed a problem where Blocks do not export to AutoCAD Model Space
PR 1512179: Fixed a problem in V18 where edges hidden with the hide edge command could not be shown
PR 2065677: Fixed a problem where Solid Edge aborts when truing on the 'Show' option of view properties.
PR 5435296: Fixed a problem where it is taking a long time to open draft file containing a parts list of a simplified assembly.
PR 5443372: Fixed a problem where exporting to AutoCAD was causing broken view frames
PR 5443575: Fixed a problem where a draft file can no longer be saved after attempting to copy a section view
PR 5513912: Fixed a problem where a Datum on a dimension becomes detached
PR 1507702: Fixed a problem where a large V17 draft won't open in V18
PR 1508552: Fixed a problem where the text in surface texture symbol is at the wrong position
PR 1514300: Fixed a problem where exporting to AutoCAD results in a blank detail view.
PR 5342477: Fixed a problem where tapered pipe threads do not show in drawing views if part is too thin.
PR 5427495: Fixed a problem where a Part does not display in a cutaway view that should display.
PR 5517004: Fixed a problem where Show Edge overrides are lost when updating a view.
PR 5524024: Fixed a problem where a QuickSheet Template box is not displayed.
PR 2066477: Fixed a problem where Solid Edge aborts when opening a draft file
PR 1396157: Fixed a problem where a section view of a FOA does not update
PR 1521554: Fixed a problem where a view of flat pattern aborted on creation.
PR 1521871: Fixed a problem where Solid Edge aborts when changing text color for Detail View and Detail Envelope
PR 5525254: Fixed a problem where a parts list would not go out-of-date when the material was changed
PR 1523964: Fixed a problem where V18 does not import a DWG file
PR 5347529: Fixed a problem where a draft file will not open in V18
PR 1517975: Fixed a problem where Callout text goes blank after edit.
PR 2066379: Fixed a problem where this Draft File cannot be converted into DXF
PR 1526326: Fixed a problem where Draft aborts when dimensions are retrieved on top view
PR 1522658: Fixed a problem where a hole in the Hole Table isn't displaying note properly
PR 1525448: Fixed a problem where a Draft file fails to open
PR 2066296: Fixed a problem where Dimension tolerance text disappears when selecting two dimensions in a row.
PR 5331611: Fixed a problem where thread lines extend too far.
PR 5516670: Fixed a problem where Radial dimensions disappear on DV update
PR 5517004: Fixed a problem where Show Edge overrides are lost when updating a view.

=====API=====

PR 1450780: Provided a new API GetBendCenterLineAttributesEx() that returns the desired result.
PR 5404153: Fixed a problem where the API "GetBendCenterLineAttributes" is inconsistent in sheetmetal
PR 5516661: Fixed a problem where Solid Edge aborts when attempting to access Documents.ActiveSheet object.

=====Insight=====

PR 5519675: Fixed a problem where you are unable to open an assembly, Incorrect Internal name " " for the property " SEDocID
PR 5438630: Fixed a problem where a user starts Solid Edge, then Insight Connect, and both licenses are checked out
PR 5511789: Fixed a problem where LCA fails to move files after upgrading to V18
PR 5526091: Fixed a problem with View&Markup performance with Insight
PR 1521862: Fixed a problem where Solid Edge is unable to open a simple part file
PR 5340572: Fixed a problem where you could get all of the status cells set to read only thus making LCA useless
PR 1518765: Fixed a problem where doc libraries failed to generate property mapping information

---
End
---