Solid Edge ST7 SDK
Solid Edge V19 SP6 - Readme

--------------
Legal Notices
--------------
© 2007,
UGS Corp.

All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of UGS Corp.; which is protected by
copyright and trade secret law.  Such materials may not be reproduced or
transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of
the Software License Agreement, or as specifically authorized in writing by
UGS Corp.

UGS Corp.
5800 Granite Parkway
Suite 600
Plano, TX. 75024

--------------------
End of Legal Notices
--------------------

--------------
Release Notes:
--------------

Product:        Solid Edge
Version:        19.00.06.04
Date:           23-May-2007

This release of Solid Edge has been certified to run on the following:
    • Windows XP Professional® operating system (32 bit or 64 bit)
    • Internet Explorer 6.0 or higher

This Update can be instaled installed on top of Version: 19.00.00.66, 19.00.01.06,
19.00.02.06, 19.00.03.06, 19.00.04.06, or 19.00.05.03.

Note: Updates are all inclusive and can be installed on top of the base release
or any released UPdate.

--------------------
End of Release Notes
--------------------

-------------------
Installation Notes:
-------------------

After downloading the Update to your machine, dbl click the downloaded file and the Update will install.

-------------------
End of Installation
-------------------

----------------------------------------------------------
This Update addresses the following Customer Reported PRs:
----------------------------------------------------------

=====Assembly=====

PR 5703545: Fixed a problem where occurrence overrides not always being set up correctly.
PR 2080435: Fixed a problem where switching members results in a message displayed about not having write-access to cfg file
PR 5726327: Fixed a problem where assembly pathfinder is not showing any subassemblies or parts.
PR 5737415: Fixed a problem where you do not get mimimum distance measurement results
PR 1589329: Fixed a problem where assembly features fail to recompute
PR 5600154: Fixed a problem where subassembly selection is not honored for cut items in a section.
PR 5737987: Fixed a problem where assembly features do now show up correctly
PR 1576343: Fixed a problem where assembly features are not updating when updating variables driving it.
PR 1589086: Fixed a problem where Occurrence Properties X,Y,Z fields no longer editable in Read-only
PR 5743069: Fixed a problem where assembly features was causing Solid Edge to crash on open.
PR 5731968: Fixed a problem where you were unable to create assembly arc pattern features.
PR 5742057: Fixed a problem where you were unable to edit a circular assembly pattern feature to be an arc feature.
PR 5747601: Added code to prevent one way of creation of loops in assembly documents with assembly features.

=====Part=====

PR 5734088: Added support for NX5 files in V19
PR 1585846: Fixed a problem where a tab with a contour flange flattens to a different size than a hem
PR 2077594: Fixed a problem where protrusion extent does not stay associative to keypoint.
PR 1588317: Fixed a problem where modifying a thread using 'edit definition'-step does not work
PR 5734088: Added support to read NX5 files in V19
PR 1592749: Fixed a problem where edge highlight is not accurate in large size parts.
PR 5746678: Fixed a problem where dimensioning between holes in 64bit V19 caused Solid Edge to crash.

=====Draft=====

PR 5681877: Fixed a problem where a 3D DWG file does not import SAT from ACAD 2004
PR 1579671: Fixed a problem where a V16 draft file cannot be opened in V19
PR 1564455: Fixed a problem where a Draft file aborts when opened
PR 5687761: Fixed a problem where PMI property text gives bad data w/simplified assemblies
PR 5676161: Fixed a problem where a painted edge is going away on DV update
PR 5733516: Fixed a problem where it is not possible to select some text elements by drawing a fence.
PR 5745631: Fixed a problem where edge display was incorrect.
PR 5738081: Fixed a problem where a drawing view would not update
PR 1564455: Fixed a problem where a Draft file aborts when opened

=====API=====

PR 1534463: Fixed a problem with the Insight.CopyFiles API
PR 1587824: Fixed a problem with Assembly Structure API performance

=====Insight=====

PR 5712946: Fixed a problem where Doc Number Property is being cleared in File Properties using Set action to revise.
PR 2080142: Fixed a problem where Japanese text is not displayed correctly in View & Markup
PR 1571569: Fixed a problem creating a revision from within Solid Edge
PR 1590305: Fixed a problem where Columns in Properties Manager are not shown in SE V19 64 bit version
PR 1590941: Fixed a problem where Revision Manager is updating the wrong links

---
End
---