Solid Edge ST7 SDK
Solid Edge V19 SP7 - Readme

--------------
Legal Notices
--------------
© 2007,
UGS Corp.

All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of UGS Corp.; which is protected by
copyright and trade secret law.  Such materials may not be reproduced or
transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of
the Software License Agreement, or as specifically authorized in writing by
UGS Corp.

UGS Corp.
5800 Granite Parkway
Suite 600
Plano, TX. 75024

--------------------
End of Legal Notices
--------------------

--------------
Release Notes:
--------------

Product:        Solid Edge
Version:        19.00.07.03
Date:           20-Jun-2007

This release of Solid Edge has been certified to run on the following:
    • Windows XP Professional® operating system (32 bit or 64 bit)
    • Internet Explorer 6.0 or higher

This Update can be instaled installed on top of Version: 19.00.00.66, 19.00.01.06,
19.00.02.06, 19.00.03.06, 19.00.04.06, 19.00.05.03, or 19.00.06.04.

Note: Updates are all inclusive and can be installed on top of the base release
or any released UPdate.

--------------------
End of Release Notes
--------------------

-------------------
Installation Notes:
-------------------

After downloading the Update to your machine, dbl click the downloaded file and the Update will install.

-------------------
End of Installation
-------------------

----------------------------------------------------------
This Update addresses the following Customer Reported PRs:
----------------------------------------------------------

=====Assembly=====

PR 5567709: Fixed a problem where Solid Edge crashes after saving an assembly (based on submitted crashlog)
PR 2076901: Fixed a problem where a wire path changes shape during edit
PR 2082171: Fixed a problem where RMB "Open" can't be executed when parts have changed on assembly.
PR 5583836: Fixed a problem where all parts are not displaying when showing a model view the first time.
PR 5750168: Fixed a problem with cyclic constraints... assy get's into loop on changes
PR 1591214: Fixed performance issues while editing mirror and pattern assembly features.
PR 5761979: Fixed a problem where Delete of assembly features causes multiple recomputes
PR 5763922: Fixed a problem where Solid Edge aborts in manual explode cmd after explode and undo
PR 5761579: Fixed a problem where Groove Weld does not work correctly in test case.
PR 1598454: Fixed a problem where extruded protrusions are failed, indicate do not modify any parts.

=====Part=====

PR 2082577: Fixed a problem where a DWG file imported into Solid Edge does not match AutoCAD
PR 1524898: Fixed a problem with Reversed text in Sketch "Insert Text Profile" [ABCD=DCBA] when using Hebrew
PR 1547595: Fixed a performance problem with 2D draft files.
PR 1596218: Fixed a problem where Solid Edge aborts when editing a Move Face feature.

=====Draft=====

PR 2081981: Fixed a problem where the AutoCAD Wizard has duplicate entries for color to width mapping
PR 1590133: Fixed an abort that occurred when opening draft files with invalid property text entries.
PR 2082696: Fixed a problem where a Symbol cannot be embedded in Japanese Solid Edge.
PR 5766467: Fixed a problem where Solid Edge aborts importing the given DWG file
PR 1583661: Fixed a problem where exporting to DWG results in missing dimensions (64bit only)
PR 1598390: Fixed a problem with Mirror with copy not working in the block environment.
PR 5765119: Fixed a problem with Save As PDF forces draft documents being saved to be active.

=====API=====

PR 1590864: Fixed a problem with the use of Loftedprotrusion.Add API in a C# sample
PR 2083398: Fixed a problem with API function RevisionManager.PropertySets.Open() throwing exception error
PR 2082859: Need a sample code for ContourFlanges.Add method

=====Insight=====

PR 5757588: Fixed a problem where Redefine Links is changing some Uppercase letters to Lowercase letters
PR 5752643: Fixed a problem where Edit Table Curve in Insight managed part causes SE to terminate
PR 5757030: Fixed a problem where Search doesn't work immediately after clearing cache from SE

---
End
---