--------------
Legal Notices
--------------
© 2007,
UGS Corp.
All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of UGS Corp.; which is protected by
copyright and trade secret law. Such materials may not be reproduced or
transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of
the Software License Agreement, or as specifically authorized in writing by
UGS Corp.
UGS Corp.
5800 Granite Parkway
Suite 600
Plano, TX. 75024
--------------------
End of Legal Notices
--------------------
--------------
Release Notes:
--------------
Product: Solid Edge
Version: 19.00.08.04
Date: 26-Jul-2007
This release of Solid Edge has been certified to run on the following:
• Windows XP Professional® operating system (32 bit or 64 bit)
• Internet Explorer 6.0 or higher
This Update can be instaled installed on top of Version: 19.00.00.66, 19.00.01.06,
19.00.02.06, 19.00.03.06, 19.00.04.06, 19.00.05.03, 19.00.06.04, or 19.00.07.03.
Note: Updates are all inclusive and can be installed on top of the base release
or any released UPdate.
--------------------
End of Release Notes
--------------------
-------------------
Installation Notes:
-------------------
After downloading the Update to your machine, dbl click the downloaded file and the Update will install.
-------------------
End of Installation
-------------------
----------------------------------------------------------
This Update addresses the following Customer Reported PRs:
----------------------------------------------------------
=====Assembly=====
PR 1592734: Fixed a problem where a drawing view did not update after changing an assembly feature.
PR 1597791: Fixed a problem with Assembly Feature performance
PR 5774079: Fixed a problem that caused Solid Edge to hang.
PR 1601204 & 5785801, 1601204: Fixed a problem where Solid Edge was not properly freeing memory.
PR 5783092: Fixed a problem with Assembly and Part file save.
PR 1604936: Fixed a problem where Windows .NET 2.0 update KB928365 causes Standard Parts to stop working.
PR 1604886: Fixed an inconsistency in Czech Standard Parts localization
PR 5783494: Fixed a problem where Solid Edge aborts using Peer Variables.
PR 1599049: Fixed a problem where Parasolid based assembly translator needs to maintain structure and bring in multiple bodies into the same part ( if name attrib matches). Note: Run/dbl-click AsmXlatorSheetsAndSolidsTogetherOn.reg file to turn on this fix, then recreate the Parasolid file and step files before round-tripping into Solid Edge
=====Part=====
PR 2083853: Fixed a problem where an Extruded Surface is always capping one end when From-To extent is used.
PR 5661146: Fixed a problem where save as .tif does not work on SEx64
PR 5770295: Fixed a problem with Cannot borrow a solidedgecatiav4 translator license
PR 5773849: Fixed a problem where formulas are not recalculating correctly.
PR 1605256: Fixed a problem where Solid Edge aborts when trying to create a projection of a curve
=====Draft=====
PR 1599332: Fixed a problem that caused a crash during DWG import
PR 1600466: Fixed a problem where replace block does not work
PR 5772730: Fixed a problem where you are unable to locate images.
PR 5779513: Modified the Mouse wheel behavior in Draft to be consistent with 3D modeling environments.
PR 5765119: Fixed a problem where Save As PDF forces draft documents being saved to be active
PR 1594976: Fixed a problem where blocks were being corrupted through copy.
---
End
---