--------------
Legal Notices
--------------
© 2007,
UGS Corp.
All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of UGS Corp.; which is protected by
copyright and trade secret law. Such materials may not be reproduced or
transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of
the Software License Agreement, or as specifically authorized in writing by
UGS Corp.
UGS Corp.
5800 Granite Parkway
Suite 600
Plano, TX. 75024
--------------------
End of Legal Notices
--------------------
--------------
Release Notes:
--------------
Product: Solid Edge
Version: 19.00.09.03
Date: 04-Sep-2007
This release of Solid Edge has been certified to run on the following:
• Windows XP Professional® operating system (32 bit or 64 bit)
• Internet Explorer 6.0 or higher
This Update can be instaled installed on top of Version: 19.00.00.66, 19.00.01.06,
19.00.02.06, 19.00.03.06, 19.00.04.06, 19.00.05.03, 19.00.06.04, 19.00.07.03, or
19.00.08.04.
Note: Updates are all inclusive and can be installed on top of the base release
or any released UPdate.
--------------------
End of Release Notes
--------------------
-------------------
Installation Notes:
-------------------
After downloading the Update to your machine, dbl click the downloaded file
and the Update will install.
-------------------
End of Installation
-------------------
----------------------------------------------------------
This Update addresses the following Customer Reported PRs:
----------------------------------------------------------
=====Assembly=====
PR 5786319: Fixed a problem where objects are not updating when moving a part with Move Part.
PR 1599319: Fixed a problem where Solid Edge crashed when editing dimensions in a profile
PR 5790158: Fixed a problem that improved assembly feature performance.
PR 2085681: Fixed a problem where the option "Save to document" gets unchecked in the Unassigned Density dialog
PR 1601204: Fixed a problem with memory management.
PR 2085688: Fixed a problem where Pathfinder taking a long time to rebuild during Close & Return
PR 2085586: Fixed a problem where a Preview is not generated in FOA SaveMemberAs operation.
PR 5779779: Fixed an abort in the Motion environment base on a submitted crashlog
PR 5798459: Fixed a problem where Solid Edge is crashing in assemblies that have section views or simplified assemblies.
PR 2085626: Fixed a problem that caused Solid Edge to crash
PR 2084310: Fixed a problem where using linkmgmt.txt file causes delays in open ASM file.
PR 2084823: Fixed a problem where the Icons in Pathfinder are incorrect
PR 5569116: Fixed a problem where Save as Movie is giving different results from SE motor simulation.
=====Part=====
PR 5783402: Fixed a problem where bend lines do not show up when part is modeled completely.
PR 2086250: Fixed a problem where the shortcut menu takes too long to come up in large part files.
PR 5802014: Fixed a problem with flat pattern
PR 2086252: Fixed a problem where adding a hole feature takes a long time on large parts.
=====Draft=====
PR 5727318: Fixed a problem that caused Solid Edge to abort when selecting callouts
PR 5805552: Fixed a problem where show edges disappear when views are updated.
PR 5801445: Fixed a problem where annotations and geometry do not translate to Solid Edge
=====API=====
PR 1579103: Fixed a problem with a COM Exception on a computer with Internet explorer 7.0
PR 2085071: Fixed a problem where SheetWindow object.SaveAsImage() method gives error.
PR 5806718: Added a API from CADPartner to aid the data prep tools interaction with STD parts
=====Insight=====
PR 5803835: Added automation method to get "Created" & "Last Saved" versions
---
End
---