Solid Edge ST7 SDK
Solid Edge V20 SP11 - Readme

--------------
Legal Notices
--------------
©2009 Siemens Product Lifecycle Management Software Inc.

All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of Siemens Product Lifecycle Management Software Inc.; which is
protected by copyright and trade secret law. Such materials may not be reproduced
or transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of the
Software License Agreement, or as specifically authorized in writing by Siemens
Product Lifecycle Management Software Inc.

Siemens Product Lifecycle Management Software Inc.
5800 Granite Parkway
Suite 600
Plano, TX. 75024


--------------------
End of Legal Notices
--------------------

--------------
Release Notes:
--------------

Product:        Solid Edge
Version:        20.00.11.06
Date:           09-Jan-2009


This release of Solid Edge has been certified to run on the following:
    • Windows XP Professional® operating system (32 bit or 64 bit)
    • Windows Vista Business® or Vista Enterprise® operating system (32 bit or 64 bit)
    • Internet Explorer 7.0 (IE 6.0 minimum)

This Update can be installed on top of Version:
20.00.00.96, 20.00.01.08, 20.00.02.03, 20.00.03.03, 20.00.04.04, 20.00.05.05,
20.00.06.06, 20.00.07.04, 20.00.08.04, 20.00.09.03, or 20.00.10.03

Note: Updates are all inclusive and can be installed on top of the base release
      or any released Update.

--------------------
End of Release Notes
--------------------

-------------------
Installation Notes:
-------------------

After downloading the Update to your machine, dbl click the downloaded file
and the Update will install.

-------------------
End of Installation
-------------------

----------------------------------------------------------
This Update addresses the following Customer Reported PRs:
----------------------------------------------------------

=====Assembly=====

PR 5996010: Cam relationship problem
PR 5728763: Adding a single constraint to an adjustable assembly fails
PR 6015494: Move Part with physical motion crashes
PR 2098270: Solid Edge crashes when clicking white area of Display Configurations
PR 5918252: Pattern not updating in this file when Height is set to original value
PR 6061245: Error in Column Designer when calculating Moments of inertia
PR 1668883: Moving a part causes duplicate occurrences to be created in Edgebar
PR 1693966: Out of context tube still updates after a Save As of the assembly
PR 2110043: Solid Edge aborts when deleting master part of pattern
PR 6045268: Assembly not found error when opening a read-only upper-level FOA
PR 5981608: Adding a sketch causes unrealistic file size growth
PR 2097365: Variable renamed by user in V19 is not being displayed with variable table filter
PR 6061778: Solid Edge aborts when printing

=====Part=====

PR 5886153: Unable to create Sheet Metal features on a Contour Flange
PR 2111593: Strange lines appear in the provided draft file
PR 1674428: Memory issue with large FOP master file
PR 1688195: Wrong cut-size after flattening a part
PR 6044788: Accessing material table causes an abort
PR 2110210: When "Go To" command is executed, Solid Edge will soon abort
PR 2111993: Link being created even with Interpart options turned off
PR 6075309: XpresRoute floating license not functioning properly

=====Draft=====

PR 1682459: Solid Edge line width to ACAD color mapping doesn't work
PR 2108454: Draft file will not open
PR 1683725: Unable to drive position of text profile with dimensions
PR 1698339: Draft file aborts when a fit is performed
PR 2070745: Text position of a Chamfer Dimension value is shifted
PR 5938516: Weld Symbol Properties dialog missing on General tab at times
PR 1687099: Dimensions disappear when views are converted to 2D
PR 2100529: When a DXF file is opened, Double byte characters are not displayed
PR 2110404: Cannot show hidden edge with "Show Edge" command
PR 1672422: Solid Edge is locking up when adding geometry on the working sheet
PR 1686469: Solid Edge will crash when editing a callout with property text
PR 1692306: Drawing views disappear when file is opened
PR 1694320: Mirror command does not create connect constraints
PR 2095507: Fill is applied to an area outside the selection
PR 2110529: Dimension value is lying on top of Dimension line
PR 2111938: AutoCAD file with multiple text color is not imported
PR 6064282: Angular dimensions incorrect when saving to AutoCAD

=====API=====
 
PR 1675689: SE x64 crashes in Models::AddSweptProtrusion
PR 4007438: Added the ability to create preview under properties via automation
PR 1663220: Added Block delete API

=====Insight/=====
 
PR 6048198: Not able to select a zone on the File -> Open dialog for Insight managed files
PR 6045318: Insight: LCA not changing “In Work” back to “Available”
PR 1687267: Changing display configurations of subassembly will crash


---
End
---