Solid Edge ST7 SDK
Solid Edge V20 SP14 - Readme

--------------
Legal Notices
--------------
©2009 Siemens Product Lifecycle Management Software Inc.

All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of Siemens Product Lifecycle Management Software Inc.; which is
protected by copyright and trade secret law. Such materials may not be reproduced
or transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of the
Software License Agreement, or as specifically authorized in writing by Siemens
Product Lifecycle Management Software Inc.

Siemens Product Lifecycle Management Software Inc.
5800 Granite Parkway
Suite 600
Plano, TX. 75024


--------------------
End of Legal Notices
--------------------

--------------
Release Notes:
--------------

Product:        Solid Edge
Version:        20.00.14.02
Date:           10-Apr-2009

This Update can be installed on top of Versions:
20.00.00.96, 20.00.01.08, 20.00.02.03, 20.00.03.03, 20.00.04.04, 20.00.05.05,
20.00.06.06, 20.00.07.04, 20.00.08.04, 20.00.09.03, 20.00.10.03, 20.00.11.06,
20.00.12.02, 20.00.13.04.

Note: Updates are all inclusive and can be installed on top of the base release
      or any released Update.

--------------------
End of Release Notes
--------------------

-------------------
Installation Notes:
-------------------

After downloading the Update to your machine, dbl click the downloaded file
and the Update will install.

-------------------
End of Installation
-------------------

----------------------------------------------------------
This Update addresses the following Customer Reported PRs:
----------------------------------------------------------

=====Draft=====

PR 1718497: Numeric Keypad values react like mouse keys for snapping a keypoint
PR 1711103: Solid Edge will export elliptical arcs as splines

===SEEC===

PR 1678740: Dataset Keep Limit is ignored
PR 1691073: Not possible to search from SE with integer LoV attached to query
PR 6023631: JT override is not used in a top level assembly


---
End
---