Solid Edge ST7 SDK
Solid Edge V20 SP15 - Readme

--------------
Legal Notices
--------------
©2009 Siemens Product Lifecycle Management Software Inc.

All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of Siemens Product Lifecycle Management Software Inc.; which is
protected by copyright and trade secret law. Such materials may not be reproduced
or transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of the
Software License Agreement, or as specifically authorized in writing by Siemens
Product Lifecycle Management Software Inc.

Siemens Product Lifecycle Management Software Inc.
5800 Granite Parkway
Suite 600
Plano, TX. 75024


--------------------
End of Legal Notices
--------------------

--------------
Release Notes:
--------------

Product:        Solid Edge
Version:        20.00.15.05
Date:           29-May-2009

This Update can be installed on top of Versions:
20.00.00.96, 20.00.01.08, 20.00.02.03, 20.00.03.03, 20.00.04.04, 20.00.05.05,
20.00.06.06, 20.00.07.04, 20.00.08.04, 20.00.09.03, 20.00.10.03, 20.00.11.06,
20.00.12.02, 20.00.13.04, 20.00.14.02.

Note: Updates are all inclusive and can be installed on top of the base release
      or any released Update.

--------------------
End of Release Notes
--------------------

-------------------
Installation Notes:
-------------------

After downloading the Update to your machine, dbl click the downloaded file
and the Update will install.

-------------------
End of Installation
-------------------

----------------------------------------------------------
This Update addresses the following Customer Reported PRs:
----------------------------------------------------------

===Assembly===

PR 1673892: Selecting new base plane results in wrong orientation
PR 1698824: Scroll to Part not working properly with patterned sub-assembly
PR 1706516: Groove Weld missing in View & Markup
PR 6144280: Virtual Component support commands not enabled with Foundation

===Draft===

PR 1643072: Problem saving a pdf from SE in to a path with a comma
PR 1694065: Scaled dimension is no longer scaled after being re-attached
PR 2091452: Incorrect transform for highlight thru automation
PR 1707553: Save failures in Draft
PR 2112715: The preview of "saved setting" of Draft callout is wrong
PR 6088507: Crash placing a Dimension to an arc center
PR 1712799: Viewer data being incorrect
PR 6084779: Non-native symbols not honoring fence settings
PR 6147847: Provided Draft file will not open

===Insight Connect===

PR 1716735: Rev Mgr generates wrong links to FOA/Variables.

===Part/Profile/Sheetmetal====

PR 2112417: Cannot select Datum Target and Datum Point with Move Dimension command
PR 6138584: Problem with 2D constraints
PR 2121561: Solid Edge aborts placing a collinear constraint
PR 2115638: Can't analyze in "Femap Express" because the error message is displayed
PR 2115753: Solid Edge aborts after clicking [Undo] after [Copy to PMI] command
PR 1711881: Ideas JT files are not going in Solid Edge sub assemblies

===SEEC===

PR 6125319: JT over-rides created by SEEC do not contain BREP data as specified in the ini
PR 1707560: "save as" doesn`t change origination date on title block
PR 6150125: SEEC TAL Update to Tc2007.1.7 Client Framework
PR 1680912: Saving from SEEC- the quantity of the non-graphical part is DELETED
PR 6049892: SEEC structure editor will crash when switching between parts list and exploded


---
End
---