Solid Edge ST7 SDK
Solid Edge V20 SP5 - Readme

--------------
Legal Notices
--------------
© 2007,
UGS Corp.

All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of UGS Corp.; which is protected by
copyright and trade secret law.  Such materials may not be reproduced or
transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of
the Software License Agreement, or as specifically authorized in writing by
UGS Corp.

UGS Corp.
5800 Granite Parkway
Suite 600
Plano, TX. 75024

--------------------
End of Legal Notices
--------------------

--------------
Release Notes:
--------------

Product:        Solid Edge
Version:        20.00.05.05
Date:           05-Mar-2008

This release of Solid Edge has been certified to run on the following:
    • Windows XP Professional® operating system (32 bit or 64 bit)
    • Windows Vista Business® or Vista Enterprise® operating system (32 bit or 64 bit)
    • Internet Explorer 7.0 (IE 6.0 minimum)

This Update can be instaled installed on top of Version: 20.00.00.96, 20.00.01.08,
20.00.02.03, 20.00.03.03, or 20.00.04.04.

Note: Updates are all inclusive and can be installed on top of the base release
      or any released UPdate.

--------------------
End of Release Notes
--------------------

-------------------
Installation Notes:
-------------------

After downloading the Update to your machine, dbl click the downloaded file
and the Update will install.

-------------------
End of Installation
-------------------

----------------------------------------------------------
This Update addresses the following Customer Reported PRs:
----------------------------------------------------------

=====Assembly=====

PR 1560877: Fixed a problem where movement simulation via a variable makes relationships fail.
PR 1627326: Fixed a problem where the user is unable to create Fastener systems.
PR 5883274: Fixed a problem were the Assembly Select Tool is not selecting nearest geometry first
PR 1620155: Fixed a problem where the focus is not set to input box with Angle Relations
PR 1634626: Fixed a problem where you are not prompted to save when closing asm after editing parts.
PR 5794020: Fixed a problem where editing an Engineering Reference component results in an error
PR 5882948: Fixed a problem where an imported NX assembly is missing parts
PR 1635879: Fixed a problem where Automatic explode is not working correctly
PR 1636815: Fixed a problem where exporting an assembly with adjustable parts results in errors
PR 2089145: Fixed a problem where you could not save a Display Configurations in an older file.
PR 5893065: Fixed a problem where Solid Edge crashes when you mouse over PathFinder Model Views in assembly
PR 2091832: Fixed a problem where opening a JT assembly aborts
PR 1617474: Fixed a problem where Save As causes an Include - link to be deleted in the new assy
PR 1607483: Fixed a problem where a pattern applied to adjustable part does not follow when part is rotated.
PR 5710806: Fixed a problem where clicking on "+" is not downloading the sub-assembly files to cache.
PR 5445638: Fixed a problem where include creates results in the incorrect location.
PR 5861000: Fixed a problem where a section view is not getting applied properly.
PR 5214177: Fixed a problem where making a subasm adjustable places patterns in wrong location

=====Part=====

PR 1613317: Fixed a problem where a drawing view will not update.
PR 1400919: Fixed a problem with conflicting relationships when using Dimension Axis
PR 5849418: Fixed a problem where editing protrusion size twice in a row results in an incorrect solve.
PR 2072611: Fixed a problem where a sheet metal model will not unbend.
PR 2091083: Fixed a problem where the a converted sheet metal file crashes after Undo.
PR 2090732: Fixed a problem where a flange will not change to a round Bend-relief
PR 5892313: Fixed a problem with Opening DM Documents in V20 give inappropriate messages
PR 2089507: Fixed a problem where a Flange is not created on outside of profile
PR 2090039: Fixed a problem where Trim failed after the first trim on a B-Spline with a PointON constraint
PR 1641535: Fixed a problem where Ideas TDM Migration is very slow

=====Draft=====

PR 5875995: Fixed a problem where assembly section views do not display.
PR 1636828: Fixed a problem where property text misinterpreting a date format as number format.
PR 5827906: Fixed a problem where sheet bodies are not shown in drawing views when a section is applied.
PR 5853510: Fixed a problem where you are unable to set Annotation text size for a style.
PR 5895624: Fixed a problem where property text to non-existent named reference is showing error.
PR 5864209: Fixed a problem where dimensions sometimes detach on document transition or save.
PR 1640177: Fixed a problem where textbox attributes are not correctly copied in copy/paste
PR 1641373: Fixed a problem where Solid Edge crashes when opening the supplied DXF file
PR 5901150: Fixed a problem where geometry is missing in an imported DXF created from NX
PR 2094827: Fixed a problem where the display of Tab char. in textbox is different in Windows2000 and WindowsXP.

=====API=====

PR 5814912: Fixed an indexing problem with the API for the Configurations Collection

=====Insight=====
 
PR 5593456: Fixed a problem where TAB and ENTER is not working correctly in property manager.
PR 1639321: Fixed a problem where Search results display the wrong value for user defined type number
PR 5880790: Fixed a problem where the Yes/No columns in Search results do not display values
PR 5896983: Fixed a problem that was causing Solid Edge to crash based on auto submitted crashlogs.
PR 1642257: Fixed a problem where the wrong revision and names are generated for a Asm
PR 1634422: Fixed a problem where subassemblies are not carried over to a new revision.
PR 1639853: Fixed a problem where User A can overwrite a modification by User B
PR 1585130: Fixed a problem where the Document number is not correctly managed by Insight in Italian version
PR 1626882: Fixed a problem where you are unable to revise or copy managed files using Revision Manager
PR 5908397: Fixed a problem with Revision manager operations make linked files read only
PR 1645360: Fixed a problem where opening SE file from the SharePoint interface is returning Insight error

---
End
---