Solid Edge ST7 SDK
Solid Edge V20 SP6 - Readme

--------------
Legal Notices
--------------
© 2007,
UGS Corp.

All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of UGS Corp.; which is protected by
copyright and trade secret law.  Such materials may not be reproduced or
transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of
the Software License Agreement, or as specifically authorized in writing by
UGS Corp.

UGS Corp.
5800 Granite Parkway
Suite 600
Plano, TX. 75024

--------------------
End of Legal Notices
--------------------

--------------
Release Notes:
--------------

Product:        Solid Edge
Version:        20.00.06.06
Date:           07-May-2008

This release of Solid Edge has been certified to run on the following:
    • Windows XP Professional® operating system (32 bit or 64 bit)
    • Windows Vista Business® or Vista Enterprise® operating system (32 bit or 64 bit)
    • Internet Explorer 7.0 (IE 6.0 minimum)

This Update can be instaled installed on top of Version: 20.00.00.96, 20.00.01.08,
20.00.02.03, 20.00.03.03, 20.00.04.04, or 20.00.05.05.

Note: Updates are all inclusive and can be installed on top of the base release
      or any released UPdate.

--------------------
End of Release Notes
--------------------

-------------------
Installation Notes:
-------------------

After downloading the Update to your machine, dbl click the downloaded file
and the Update will install.

-------------------
End of Installation
-------------------

----------------------------------------------------------
This Update addresses the following Customer Reported PRs:
----------------------------------------------------------

=====Assembly=====

PR 1633466: Fixed a problem where the Adjustable Part dialog appears only once
PR 1642090: Fixed a problem where tubes are not updating properly inside a FOA file.
PR 5918490: Fixed a problem where Assembly features are taking a long time to create/update in this file.
PR 2090861: Fixed a problem where Solid Edge aborts when double clicking on an X_T file on desktop
PR 1648907: Fixed a problem where the Preview is not updating in Property Manager

=====Part=====

PR 5875755: Fixed a problem where a large Step File is not translating properly
PR 5864044/2095252: Fixed a problem where files are not saved even though "save" is selected on the memory warning dialog
PR 5864044/1628784: Fixed a problem where some features are not updating after Editing Profile
PR 1626397: Fixed a problem where Solid Edge crashes when editing a pattern.
PR 5923272: Fixed a noticeable performance difference between V18 and V20 when creating an extrusion in-place active
PR 5796903: Fixed a problem where Solid Edge would crash when deleting a line from profile in a Tab.
PR 5876754: Fixed a problem where Solid Edge was taking a long time to validate/checkout a second and third license
PR 2084055: Fixed a problem where resizing a hole in the is file caused Solid Edge to lock up.
PR 1637173: Fixed a problem where an Unbend feature modifies existing tabs located in a bend zone
PR 1619304: Fixed a problem where Solid Edge closes after editing a text profile within a cutout.
PR 5852431:  Fixed a problem where tab creation results in multiple faces.

=====Draft=====

PR 5901846: Fixed a problem where Solid Edge crashed when creating Detail View
PR 5911708: Fixed a problem where a Hole callout was wrong in section view.
PR 1651030: Fixed a problem where a User table was corrupted after rows were deleted.
PR 1638310: Fixed a problem where DWG and DXF files were not generated correctly.
PR 1635223: Fixed a problem where a drawing view of a model with simplified subassemblies did not update correctly
PR 1640473: Fixed a problem where copying a drawing view w/assembly overrides caused subsequent views to be placed incorrectly.
PR 5930003: Fixed a problem where Solid Edge was crashing when trying to create a section view from a detail view.
PR 5932877: Fixed a problem where a drawing view of an Assembly created erroneous geometry
PR 1646959: Fixed a problem where revolved section views became corrupt after an independent detail view was deleted.
PR 1645262: Fixed a problem where copy/paste between documents was very slow
PR 2097038: Fixed a problem where dimension values in this file displayed incorrectly

=====Insight=====
 
PR 5831605: Fixed a problem where a PCF file would not display in View and Markup
PR 1649542: Fixed a problem where the BOM WebPart doesn't properly export text which contains a comma.

---
End
---