#define AE_ALLOWED_REF_TYPE (AE_ERROR_BASE + 156) |
Definition at line 235 of file ae_errors.h.
#define AE_always_never_conflict (AE_ERROR_BASE + 171) |
Definition at line 255 of file ae_errors.h.
#define AE_asking_registered_actions (AE_ERROR_BASE + 53) |
Definition at line 123 of file ae_errors.h.
#define AE_attached_dataset_cico_unco_error (AE_ERROR_BASE + 175) |
Definition at line 262 of file ae_errors.h.
#define AE_attached_dataset_co_exported (AE_ERROR_BASE + 176) |
Definition at line 263 of file ae_errors.h.
#define AE_attempt_to_circular_ref (AE_ERROR_BASE + 173) |
Definition at line 258 of file ae_errors.h.
#define AE_bad_reference_tree (AE_ERROR_BASE + 143) |
Definition at line 221 of file ae_errors.h.
#define AE_bad_rev_limit (AE_ERROR_BASE + 136) |
Definition at line 214 of file ae_errors.h.
#define AE_cannot_add_tool_parms (AE_ERROR_BASE + 127) |
Definition at line 205 of file ae_errors.h.
#define AE_cannot_clear_tool_parms (AE_ERROR_BASE + 125) |
Definition at line 203 of file ae_errors.h.
#define AE_cannot_create_parm_obj (AE_ERROR_BASE + 126) |
Definition at line 204 of file ae_errors.h.
#define AE_cannot_delete_dataset (AE_ERROR_BASE + 43) |
This error would occur if we attempted to delete a dataset that was either frozen or being referenced by something other than its anchor.
Definition at line 86 of file ae_errors.h.
#define AE_cannot_export_dataset (AE_ERROR_BASE + 165) |
Definition at line 244 of file ae_errors.h.
#define AE_cannot_find_dataset (AE_ERROR_BASE + 97) |
Definition at line 180 of file ae_errors.h.
#define AE_cannot_freeze_dataset (AE_ERROR_BASE + 47) |
Definition at line 102 of file ae_errors.h.
#define AE_cannot_freeze_reference (AE_ERROR_BASE + 45) |
Definition at line 95 of file ae_errors.h.
#define AE_cannot_get_datasettype (AE_ERROR_BASE + 124) |
Definition at line 202 of file ae_errors.h.
#define AE_cannot_get_first_obj (AE_ERROR_BASE + 108) |
Definition at line 191 of file ae_errors.h.
#define AE_cannot_get_next_obj (AE_ERROR_BASE + 109) |
Definition at line 192 of file ae_errors.h.
#define AE_cannot_get_prev_obj (AE_ERROR_BASE + 111) |
Definition at line 194 of file ae_errors.h.
#define AE_cannot_get_references (AE_ERROR_BASE + 149) |
Definition at line 227 of file ae_errors.h.
#define AE_cannot_get_rev0_obj (AE_ERROR_BASE + 140) |
Definition at line 218 of file ae_errors.h.
#define AE_cannot_get_rev0_tag (AE_ERROR_BASE + 141) |
Definition at line 219 of file ae_errors.h.
#define AE_cannot_get_tool (AE_ERROR_BASE + 113) |
Definition at line 196 of file ae_errors.h.
#define AE_cannot_init_dataset (AE_ERROR_BASE + 138) |
Definition at line 216 of file ae_errors.h.
#define AE_cannot_insert_named_ref (AE_ERROR_BASE + 160) |
Definition at line 239 of file ae_errors.h.
#define AE_cannot_modify_dataset_desc (AE_ERROR_BASE + 159) |
Definition at line 238 of file ae_errors.h.
#define AE_cannot_open_dataset (AE_ERROR_BASE + 59) |
Definition at line 136 of file ae_errors.h.
#define AE_cannot_print_dataset (AE_ERROR_BASE + 58) |
This error would occur if the system cannot perform the default print method on a Dataset for some reason, such as it is a multi-file Dataset, or it points to some class of object other than ImanFile.
Definition at line 134 of file ae_errors.h.
#define AE_cannot_purge_dataset (AE_ERROR_BASE + 137) |
Definition at line 215 of file ae_errors.h.
#define AE_cannot_remove_parameters (AE_ERROR_BASE + 134) |
Definition at line 212 of file ae_errors.h.
#define AE_cannot_rename_dataset (AE_ERROR_BASE + 158) |
Definition at line 237 of file ae_errors.h.
#define AE_cannot_replace_named_ref (AE_ERROR_BASE + 161) |
Definition at line 240 of file ae_errors.h.
#define AE_cannot_replace_refs (AE_ERROR_BASE + 166) |
Definition at line 245 of file ae_errors.h.
#define AE_cannot_rev_copy (AE_ERROR_BASE + 148) |
Definition at line 226 of file ae_errors.h.
#define AE_cannot_rev_copy_frozen_dataset (AE_ERROR_BASE + 49) |
Cannot make a revision copy of a dataset whose latest revision is frozen.
Definition at line 108 of file ae_errors.h.
#define AE_cannot_save_dataset (AE_ERROR_BASE + 139) |
Definition at line 217 of file ae_errors.h.
#define AE_cannot_unfreeze_dataset (AE_ERROR_BASE + 48) |
Definition at line 103 of file ae_errors.h.
#define AE_cannot_unfreeze_reference (AE_ERROR_BASE + 46) |
Cannot freeze or unfreeze an object pointed to via a named reference.
Definition at line 100 of file ae_errors.h.
#define AE_copy_id_gen_failed (AE_idrev_error_base + 7) |
Definition at line 323 of file ae_errors.h.
#define AE_copy_revid_gen_failed (AE_idrev_error_base + 9) |
Definition at line 325 of file ae_errors.h.
#define AE_create_id_gen_failed (AE_idrev_error_base + 6) |
Definition at line 322 of file ae_errors.h.
#define AE_create_revid_gen_failed (AE_idrev_error_base + 8) |
Definition at line 324 of file ae_errors.h.
#define AE_create_shell_error (AE_ERROR_BASE + 15) |
Error occurred in the update of the newstuff folder.
Definition at line 42 of file ae_errors.h.
#define AE_dataset_archived (AE_ERROR_BASE + 9) |
Definition at line 28 of file ae_errors.h.
#define AE_dataset_copy_error (AE_ERROR_BASE + 172) |
Definition at line 257 of file ae_errors.h.
#define AE_dataset_copy_no_gen_name (AE_ERROR_BASE + 164) |
Definition at line 243 of file ae_errors.h.
#define AE_dataset_create_no_gen_name (AE_ERROR_BASE + 163) |
Definition at line 242 of file ae_errors.h.
#define AE_dataset_is_frozen (AE_ERROR_BASE + 142) |
Definition at line 220 of file ae_errors.h.
#define AE_dataset_name_too_long (AE_ERROR_BASE + 169) |
Definition at line 253 of file ae_errors.h.
#define AE_datasettype_not_found (AE_ERROR_BASE + 10) |
Definition at line 30 of file ae_errors.h.
#define AE_datasettype_not_loaded (AE_ERROR_BASE + 11) |
Definition at line 31 of file ae_errors.h.
#define AE_datasettype_renametool_failed (AE_ERROR_BASE + 152) |
Definition at line 231 of file ae_errors.h.
#define AE_datasettypetool_not_found (AE_ERROR_BASE + 12) |
This error means that a tool was entered that is not in the list of tools that the input DatasetType understands.
Definition at line 37 of file ae_errors.h.
#define AE_duplicate_id_rev (AE_idrev_error_base + 1) |
Definition at line 317 of file ae_errors.h.
#define AE_duplicate_type_name (AE_ERROR_BASE + 93) |
Definition at line 176 of file ae_errors.h.
#define AE_empty_ro_dataset (AE_ERROR_BASE + 162) |
Definition at line 241 of file ae_errors.h.
#define AE_enq_failed (AE_ERROR_BASE + 104) |
Definition at line 187 of file ae_errors.h.
#define AE_ERROR_BASE EMH_AE_error_base |
Definition at line 25 of file ae_errors.h.
#define AE_file_type_mismatch_ref (AE_ERROR_BASE + 155) |
Definition at line 234 of file ae_errors.h.
#define AE_finding_dataset (AE_ERROR_BASE + 40) |
The Dataset cannot be found.
Definition at line 67 of file ae_errors.h.
#define AE_finding_datasettype (AE_ERROR_BASE + 38) |
The Dataset type cannot be found.
Definition at line 57 of file ae_errors.h.
#define AE_finding_datasettype_children (AE_ERROR_BASE + 44) |
This error occurs when an error is encountered finding the child types of a Dasettype. It can also occur when finding root parents, since it is the same query, except the parent equals NULLTAG.
Definition at line 93 of file ae_errors.h.
#define AE_finding_tool (AE_ERROR_BASE + 39) |
The tool "%1$" cannot be found. Please contact your system administrator.
Definition at line 62 of file ae_errors.h.
#define AE_format_invalid (AE_ERROR_BASE + 13) |
Definition at line 39 of file ae_errors.h.
#define AE_get_parms_failed (AE_ERROR_BASE + 122) |
Definition at line 200 of file ae_errors.h.
#define AE_ict_error_base (AE_ERROR_BASE + 350) |
Definition at line 332 of file ae_errors.h.
#define AE_ICT_invalid_version (AE_ict_error_base + 1) |
Definition at line 334 of file ae_errors.h.
#define AE_idrev_error_base (AE_ERROR_BASE + 300) |
Definition at line 315 of file ae_errors.h.
#define AE_illegal_parameter (AE_idrev_error_base + 3) |
Definition at line 319 of file ae_errors.h.
#define AE_internal_error (AE_ERROR_BASE + 157) |
Definition at line 236 of file ae_errors.h.
#define AE_invalid_action (AE_ERROR_BASE + 55) |
Definition at line 125 of file ae_errors.h.
#define AE_invalid_data (AE_ERROR_BASE + 88) |
Definition at line 171 of file ae_errors.h.
#define AE_invalid_datasettype (AE_ERROR_BASE + 85) |
Definition at line 168 of file ae_errors.h.
#define AE_invalid_file_limit (AE_ERROR_BASE + 106) |
Definition at line 189 of file ae_errors.h.
#define AE_invalid_format (AE_ERROR_BASE + 86) |
Definition at line 169 of file ae_errors.h.
#define AE_invalid_load_method (AE_ERROR_BASE + 52) |
Definition at line 122 of file ae_errors.h.
#define AE_invalid_operation (AE_ERROR_BASE + 150) |
Definition at line 228 of file ae_errors.h.
#define AE_invalid_operator (AE_ERROR_BASE + 135) |
Definition at line 213 of file ae_errors.h.
#define AE_invalid_parameter (AE_ERROR_BASE + 81) |
Definition at line 164 of file ae_errors.h.
#define AE_invalid_program (AE_ERROR_BASE + 84) |
Definition at line 167 of file ae_errors.h.
#define AE_invalid_reference (AE_ERROR_BASE + 83) |
Definition at line 166 of file ae_errors.h.
#define AE_invalid_template (AE_ERROR_BASE + 87) |
Definition at line 170 of file ae_errors.h.
#define AE_invalid_token (AE_ERROR_BASE + 82) |
Definition at line 165 of file ae_errors.h.
#define AE_invalid_tool (AE_ERROR_BASE + 89) |
Definition at line 172 of file ae_errors.h.
#define AE_invalid_type (AE_ERROR_BASE + 96) |
Definition at line 179 of file ae_errors.h.
#define AE_listing_datasettype_refs (AE_ERROR_BASE + 56) |
Definition at line 126 of file ae_errors.h.
#define AE_lock_datasettype_failed (AE_ERROR_BASE + 151) |
Definition at line 230 of file ae_errors.h.
#define AE_max_id_exceeded (AE_idrev_error_base + 5) |
Definition at line 321 of file ae_errors.h.
#define AE_mem_alloc_failed (AE_idrev_error_base + 4) |
Definition at line 320 of file ae_errors.h.
#define AE_next_id_lock_failed (AE_idrev_error_base + 2) |
Definition at line 318 of file ae_errors.h.
#define AE_no_access (AE_ERROR_BASE + 144) |
Definition at line 222 of file ae_errors.h.
#define AE_no_add_ref (AE_ERROR_BASE + 90) |
Definition at line 173 of file ae_errors.h.
#define AE_no_change_anchor_owner (AE_ERROR_BASE + 62) |
Definition at line 140 of file ae_errors.h.
#define AE_no_change_dataset_owner (AE_ERROR_BASE + 68) |
Definition at line 146 of file ae_errors.h.
#define AE_no_change_reference_owner (AE_ERROR_BASE + 65) |
Definition at line 143 of file ae_errors.h.
#define AE_no_class_type (AE_ERROR_BASE + 101) |
Definition at line 184 of file ae_errors.h.
#define AE_no_clear_anchor_access (AE_ERROR_BASE + 145) |
Definition at line 223 of file ae_errors.h.
#define AE_no_clear_dataset_access (AE_ERROR_BASE + 147) |
Definition at line 225 of file ae_errors.h.
#define AE_no_clear_reference_access (AE_ERROR_BASE + 146) |
Definition at line 224 of file ae_errors.h.
#define AE_no_create_enq (AE_ERROR_BASE + 103) |
Definition at line 186 of file ae_errors.h.
#define AE_no_create_type (AE_ERROR_BASE + 94) |
Definition at line 177 of file ae_errors.h.
#define AE_no_datasettypes (AE_ERROR_BASE + 105) |
Definition at line 188 of file ae_errors.h.
#define AE_no_delete_access (AE_ERROR_BASE + 107) |
Definition at line 190 of file ae_errors.h.
#define AE_no_find_type (AE_ERROR_BASE + 95) |
Definition at line 178 of file ae_errors.h.
#define AE_no_get_attrs (AE_ERROR_BASE + 102) |
Definition at line 185 of file ae_errors.h.
#define AE_no_grant_anchor_access (AE_ERROR_BASE + 60) |
Definition at line 138 of file ae_errors.h.
#define AE_no_grant_dataset_access (AE_ERROR_BASE + 66) |
Definition at line 144 of file ae_errors.h.
#define AE_no_grant_reference_access (AE_ERROR_BASE + 63) |
Definition at line 141 of file ae_errors.h.
#define AE_no_load_datasettype (AE_ERROR_BASE + 74) |
Definition at line 157 of file ae_errors.h.
#define AE_no_load_program (AE_ERROR_BASE + 73) |
Definition at line 156 of file ae_errors.h.
#define AE_no_load_ref_desc (AE_ERROR_BASE + 75) |
Definition at line 158 of file ae_errors.h.
#define AE_no_load_reference (AE_ERROR_BASE + 71) |
Definition at line 154 of file ae_errors.h.
#define AE_no_load_tool_desc (AE_ERROR_BASE + 72) |
Definition at line 155 of file ae_errors.h.
#define AE_no_next_obj (AE_ERROR_BASE + 110) |
Definition at line 193 of file ae_errors.h.
#define AE_no_prev_obj (AE_ERROR_BASE + 112) |
Definition at line 195 of file ae_errors.h.
#define AE_no_references (AE_ERROR_BASE + 168) |
Definition at line 247 of file ae_errors.h.
#define AE_no_refresh (AE_ERROR_BASE + 69) |
The Dataset "%1$" cannot be refreshed.
Definition at line 151 of file ae_errors.h.
#define AE_no_remove_ref (AE_ERROR_BASE + 91) |
Definition at line 174 of file ae_errors.h.
#define AE_no_revoke_anchor_access (AE_ERROR_BASE + 61) |
Definition at line 139 of file ae_errors.h.
#define AE_no_revoke_dataset_access (AE_ERROR_BASE + 67) |
Definition at line 145 of file ae_errors.h.
#define AE_no_revoke_reference_access (AE_ERROR_BASE + 64) |
Definition at line 142 of file ae_errors.h.
#define AE_no_save_datasettype (AE_ERROR_BASE + 99) |
Definition at line 182 of file ae_errors.h.
#define AE_no_save_operations (AE_ERROR_BASE + 128) |
Definition at line 206 of file ae_errors.h.
#define AE_no_save_parameters (AE_ERROR_BASE + 80) |
Definition at line 163 of file ae_errors.h.
#define AE_no_save_refs (AE_ERROR_BASE + 92) |
Definition at line 175 of file ae_errors.h.
#define AE_no_tools (AE_ERROR_BASE + 167) |
Definition at line 246 of file ae_errors.h.
#define AE_nonfile_ref_to_file_ref (AE_ERROR_BASE + 154) |
Definition at line 233 of file ae_errors.h.
#define AE_not_initialized (AE_ERROR_BASE + 41) |
This error means that AE_init_module was not called prior to making calls to AE ITK routines.
Definition at line 73 of file ae_errors.h.
#define AE_nothing_to_delete (AE_ERROR_BASE + 132) |
Definition at line 210 of file ae_errors.h.
#define AE_nothing_to_modify (AE_ERROR_BASE + 131) |
Definition at line 209 of file ae_errors.h.
#define AE_nra_error_base (AE_ERROR_BASE + 250) |
Definition at line 305 of file ae_errors.h.
#define AE_NULL_reference (AE_ERROR_BASE + 70) |
Definition at line 153 of file ae_errors.h.
#define AE_operation_exist_in_the_list (AE_ERROR_BASE + 129) |
Definition at line 207 of file ae_errors.h.
#define AE_operation_not_defined (AE_ERROR_BASE + 130) |
Definition at line 208 of file ae_errors.h.
#define AE_owner_preference_invalid (AE_ERROR_BASE + 170) |
Definition at line 254 of file ae_errors.h.
#define AE_parameter_already_set (AE_ERROR_BASE + 77) |
Definition at line 160 of file ae_errors.h.
#define AE_parameter_not_removed (AE_ERROR_BASE + 79) |
Definition at line 162 of file ae_errors.h.
#define AE_parameter_not_set (AE_ERROR_BASE + 78) |
Definition at line 161 of file ae_errors.h.
#define AE_parameters_not_loaded (AE_ERROR_BASE + 76) |
Definition at line 159 of file ae_errors.h.
#define AE_reference_already_exists (AE_ERROR_BASE + 36) |
The named reference "%1$" cannot be added to the Dataset, because the reference already exists.
Definition at line 47 of file ae_errors.h.
#define AE_reference_does_not_exist (AE_ERROR_BASE + 37) |
The named reference, "%1$", cannot be added to the Dataset, because the reference does not exist.
Definition at line 52 of file ae_errors.h.
#define AE_reference_stub_not_augmented (AE_ERROR_BASE + 174) |
Definition at line 259 of file ae_errors.h.
#define AE_references_not_loaded (AE_ERROR_BASE + 100) |
Definition at line 183 of file ae_errors.h.
#define AE_relate_to_dataset_newstuff_folder (AE_ERROR_BASE + 177) |
Some relations cannot be established between the Datasets and their associated containers. These Datasets, therefore, are placed under the "NewStuff" folder.
Definition at line 266 of file ae_errors.h.
#define AE_revision_anchor_error_base (AE_ERROR_BASE + 200) |
Definition at line 296 of file ae_errors.h.
#define AE_save_dsparms_failed1 (AE_ERROR_BASE + 120) |
Definition at line 198 of file ae_errors.h.
#define AE_save_dsparms_failed2 (AE_ERROR_BASE + 121) |
Definition at line 199 of file ae_errors.h.
#define AE_setting_registered_actions (AE_ERROR_BASE + 54) |
Definition at line 124 of file ae_errors.h.
#define AE_sign_dataset_cannot_checkin (AE_ERROR_BASE + 180) |
The "Check-In" operation is not allowed on the Dataset object, because it is checked-out for signing. Please cancel, or complete, the signing operation.
Definition at line 289 of file ae_errors.h.
#define AE_sign_dataset_cannot_tr_checkout (AE_ERROR_BASE + 179) |
The "Transfer Checked-Out" operation is not allowed on the Dataset object, because it is checked-out for signing. Please cancel, or complete, the signing operation.
Definition at line 283 of file ae_errors.h.
#define AE_sign_dataset_cannot_undo_checkout (AE_ERROR_BASE + 178) |
The "Undo Checked-Out" operation is not allowed on the Dataset object, because it is checked-out for signing. Please cancel, or complete, the signing operation.
Definition at line 277 of file ae_errors.h.
#define AE_space_in_reference_name (AE_ERROR_BASE + 153) |
Definition at line 232 of file ae_errors.h.
#define AE_tool_name_not_unique (AE_ERROR_BASE + 57) |
Definition at line 127 of file ae_errors.h.
#define AE_tool_not_entered (AE_ERROR_BASE + 50) |
This error is returned within the Dataset Window when an action is chosen that expects a tool to be defined, but nothing has been entered yet.
Definition at line 114 of file ae_errors.h.
#define AE_tool_not_found (AE_ERROR_BASE + 8) |
Definition at line 27 of file ae_errors.h.
#define AE_unable_to_find_nra (AE_nra_error_base + 2) |
Definition at line 308 of file ae_errors.h.
#define AE_unable_to_find_nra_tag (AE_nra_error_base + 1) |
Definition at line 307 of file ae_errors.h.
#define AE_unable_to_get_parameters (AE_ERROR_BASE + 133) |
Definition at line 211 of file ae_errors.h.
#define AE_unable_to_load_rev_anchor (AE_revision_anchor_error_base + 1) |
Definition at line 298 of file ae_errors.h.
#define AE_unexplained_error (AE_ERROR_BASE + 42) |
This error will be returned when something goes wrong that never should. You should review the journal_file and will probably need to call client services.
Definition at line 80 of file ae_errors.h.
#define AE_unknown_action (AE_ERROR_BASE + 51) |
Somehow an action code was passed to the encapsulation mechanism that AE does not yet understand.
Definition at line 120 of file ae_errors.h.
#define AE_unlock_datasettype_failed (AE_ERROR_BASE + 123) |
Definition at line 201 of file ae_errors.h.