#define AOM_attrib_invalid_name (EMH_AOM_error_base + 20) |
The name of the attribute in invalid for operation
Definition at line 69 of file aom_errors.h.
#define AOM_cannot_touch_archived (EMH_AOM_error_base + 14) |
Definition at line 57 of file aom_errors.h.
#define AOM_cannot_touch_replica (EMH_AOM_error_base + 13) |
Definition at line 56 of file aom_errors.h.
#define AOM_inst_archived (EMH_AOM_error_base + 12) |
Definition at line 55 of file aom_errors.h.
#define AOM_inst_checked_out_against (EMH_AOM_error_base + 4) |
Object checked out by another user.
Definition at line 37 of file aom_errors.h.
#define AOM_inst_copy_protected (EMH_AOM_error_base + 11) |
You do not have copy access to the object.
Definition at line 53 of file aom_errors.h.
#define AOM_inst_delete_protected (EMH_AOM_error_base + 10) |
You do not have delete access to the object.
Definition at line 50 of file aom_errors.h.
#define AOM_inst_frozen (EMH_AOM_error_base + 2) |
Definition at line 31 of file aom_errors.h.
#define AOM_inst_in_use (EMH_AOM_error_base + 1) |
Object is locked for modify in another session.
Definition at line 29 of file aom_errors.h.
#define AOM_inst_in_xfer_pending (EMH_AOM_error_base + 18) |
Object is locked for modify due to ownership transfer pending.
Definition at line 63 of file aom_errors.h.
#define AOM_inst_read_protected (EMH_AOM_error_base + 5) |
You do not have read access to the object.
Definition at line 40 of file aom_errors.h.
#define AOM_inst_write_protected (EMH_AOM_error_base + 3) |
You do not have write access to the object.
Definition at line 34 of file aom_errors.h.
#define AOM_internal_error (EMH_AOM_error_base + 0) |
Definition at line 26 of file aom_errors.h.
#define AOM_invalid_attribute (EMH_AOM_error_base + 19) |
Attribute is not valid for the operation
Definition at line 66 of file aom_errors.h.
#define AOM_invalid_deferred_operation (EMH_AOM_error_base + 22) |
The operation is not allowed when deferred is turned on
Definition at line 75 of file aom_errors.h.
#define AOM_invalid_prop_index (EMH_AOM_error_base + 16) |
Definition at line 59 of file aom_errors.h.
#define AOM_locked_by (EMH_AOM_error_base + 9) |
Definition at line 47 of file aom_errors.h.
#define AOM_not_in_parent (EMH_AOM_error_base + 15) |
Definition at line 58 of file aom_errors.h.
#define AOM_read_protection_failed (EMH_AOM_error_base + 6) |
Unable to read protection.
Definition at line 43 of file aom_errors.h.
#define AOM_user_has_no_write_access_to_object (EMH_AOM_error_base + 17) |
Definition at line 60 of file aom_errors.h.
#define AOM_VLA_data_truncated (EMH_AOM_error_base + 21) |
The input VLA string size exceeds the allowed limit of 4000-48
Definition at line 72 of file aom_errors.h.
#define AOM_where_refd_on_delete_a (EMH_AOM_error_base + 7) |
Definition at line 45 of file aom_errors.h.
#define AOM_where_refd_on_delete_b (EMH_AOM_error_base + 8) |
Definition at line 46 of file aom_errors.h.