#define BIER_ambiguous_sst (BIER_ERROR_BASE + 101) |
Definition at line 154 of file bier_errors.h.
#define BIER_bulk_data_file_not_transfered (BIER_ERROR_BASE + 76) |
Definition at line 129 of file bier_errors.h.
#define BIER_cannot_export_imported_object (BIER_ERROR_BASE + 21) |
Definition at line 72 of file bier_errors.h.
#define BIER_cannot_export_modifiable (BIER_ERROR_BASE + 30) |
Definition at line 83 of file bier_errors.h.
#define BIER_cannot_import_preview_metafile (BIER_ERROR_BASE + 55) |
Definition at line 108 of file bier_errors.h.
#define BIER_cannot_import_with_missing_ref (BIER_ERROR_BASE + 12) |
Definition at line 60 of file bier_errors.h.
#define BIER_cannot_remote_co_replica (BIER_ERROR_BASE + 87) |
Definition at line 140 of file bier_errors.h.
#define BIER_cannot_transfer_archived (BIER_ERROR_BASE + 29) |
Definition at line 82 of file bier_errors.h.
#define BIER_cannot_transfer_checked_out (BIER_ERROR_BASE + 11) |
Definition at line 57 of file bier_errors.h.
#define BIER_cannot_transfer_in_process (BIER_ERROR_BASE + 33) |
Definition at line 86 of file bier_errors.h.
#define BIER_cannot_transfer_ownership_of_replica (BIER_ERROR_BASE + 88) |
Definition at line 141 of file bier_errors.h.
#define BIER_cannot_transfer_released (BIER_ERROR_BASE + 10) |
Definition at line 56 of file bier_errors.h.
#define BIER_cannot_transfer_replica_from_hub (BIER_ERROR_BASE + 64) |
Definition at line 117 of file bier_errors.h.
#define BIER_cannot_xfer_to_local_site (BIER_ERROR_BASE + 20) |
Definition at line 71 of file bier_errors.h.
#define BIER_cannot_xfer_to_multiple_sites (BIER_ERROR_BASE + 19) |
Definition at line 70 of file bier_errors.h.
#define BIER_check_out_site_not_found (BIER_ERROR_BASE + 72) |
Definition at line 125 of file bier_errors.h.
#define BIER_chkpt_transaction_in_progress (BIER_ERROR_BASE + 109) |
Definition at line 162 of file bier_errors.h.
#define BIER_class_not_directly_exportable (BIER_ERROR_BASE + 69) |
Definition at line 122 of file bier_errors.h.
#define BIER_class_not_directly_transferable (BIER_ERROR_BASE + 70) |
Definition at line 123 of file bier_errors.h.
#define BIER_class_not_storable (BIER_ERROR_BASE + 3) |
Instances of this class are not exportable/importable (archivable?)
Definition at line 35 of file bier_errors.h.
#define BIER_CntrlRep_assembly_invalid_for_replication (BIER_ERROR_BASE + 132) |
Definition at line 180 of file bier_errors.h.
#define BIER_CntrlRep_no_replication_sites (BIER_ERROR_BASE + 134) |
Definition at line 182 of file bier_errors.h.
#define BIER_CntrlRep_no_revision_rule_provided (BIER_ERROR_BASE + 133) |
Definition at line 181 of file bier_errors.h.
#define BIER_CntrlRep_not_precise (BIER_ERROR_BASE + 136) |
Definition at line 187 of file bier_errors.h.
#define BIER_CntrlRep_not_released (BIER_ERROR_BASE + 137) |
Definition at line 188 of file bier_errors.h.
#define BIER_CntrlRep_stubbed (BIER_ERROR_BASE + 138) |
Definition at line 189 of file bier_errors.h.
#define BIER_conflicting_ie_options (BIER_ERROR_BASE + 40) |
Definition at line 93 of file bier_errors.h.
#define BIER_conflicting_transfer_options (BIER_ERROR_BASE + 39) |
Definition at line 92 of file bier_errors.h.
#define BIER_dataset_export_declined_by_custom_code (BIER_ERROR_BASE + 122) |
Definition at line 175 of file bier_errors.h.
#define BIER_ERROR_BASE EMH_BIER_error_base |
Definition at line 26 of file bier_errors.h.
#define BIER_exclude_failed (BIER_ERROR_BASE + 7) |
Definition at line 46 of file bier_errors.h.
#define BIER_exported_object_missing (BIER_ERROR_BASE + 35) |
Definition at line 88 of file bier_errors.h.
#define BIER_fail_to_export (BIER_ERROR_BASE + 22) |
Definition at line 74 of file bier_errors.h.
#define BIER_failed_to_extract_instance (BIER_ERROR_BASE + 2) |
Encountered a problem extracting an instance from the file
Definition at line 32 of file bier_errors.h.
#define BIER_form_storage_class_does_not_exist (BIER_ERROR_BASE + 68) |
Definition at line 121 of file bier_errors.h.
#define BIER_fsc_proxy_error (BIER_ERROR_BASE + 78) |
Definition at line 131 of file bier_errors.h.
#define BIER_group_not_defined_at_remote_site (BIER_ERROR_BASE + 80) |
Definition at line 133 of file bier_errors.h.
#define BIER_importing_local_object (BIER_ERROR_BASE + 57) |
Definition at line 110 of file bier_errors.h.
#define BIER_instance_not_in_file (BIER_ERROR_BASE + 1) |
Instance to recover was not stored in this file
Definition at line 29 of file bier_errors.h.
#define BIER_internal_error (BIER_ERROR_BASE + 140) |
Some kind of inconsistency has been detected. This is probably a coding error we would like reported, and there is no sensible recovery available
Definition at line 196 of file bier_errors.h.
#define BIER_invalid_for_local_bier_type (BIER_ERROR_BASE + 26) |
Definition at line 79 of file bier_errors.h.
#define BIER_invalid_for_remote_bier_type (BIER_ERROR_BASE + 25) |
Definition at line 78 of file bier_errors.h.
#define BIER_invalid_option_when_not_xferring (BIER_ERROR_BASE + 42) |
Definition at line 95 of file bier_errors.h.
#define BIER_invalid_option_when_xferring (BIER_ERROR_BASE + 41) |
Definition at line 94 of file bier_errors.h.
#define BIER_invalid_read_tickets_file (BIER_ERROR_BASE + 75) |
Definition at line 128 of file bier_errors.h.
#define BIER_invalid_recover_mode (BIER_ERROR_BASE + 34) |
Definition at line 87 of file bier_errors.h.
#define BIER_invalid_recover_mode_for_export_dir (BIER_ERROR_BASE + 74) |
Definition at line 127 of file bier_errors.h.
#define BIER_invalid_revisions_when_xferring (BIER_ERROR_BASE + 135) |
Definition at line 184 of file bier_errors.h.
#define BIER_invalid_site (BIER_ERROR_BASE + 17) |
Definition at line 68 of file bier_errors.h.
#define BIER_l10n_cannot_get_locale_pref_val (BIER_ERROR_BASE + 117) |
Definition at line 170 of file bier_errors.h.
#define BIER_l10n_cannot_set_localized_attribute (BIER_ERROR_BASE + 119) |
Definition at line 172 of file bier_errors.h.
#define BIER_l10n_locale_not_available (BIER_ERROR_BASE + 118) |
Definition at line 171 of file bier_errors.h.
#define BIER_lastexp_valid_for_item_only (BIER_ERROR_BASE + 59) |
Definition at line 112 of file bier_errors.h.
#define BIER_local_site (BIER_ERROR_BASE + 16) |
Definition at line 67 of file bier_errors.h.
#define BIER_LOV_export_failed (BIER_ERROR_BASE + 120) |
Definition at line 173 of file bier_errors.h.
#define BIER_LOV_import_failed (BIER_ERROR_BASE + 121) |
Definition at line 174 of file bier_errors.h.
#define BIER_missing_item (BIER_ERROR_BASE + 14) |
Definition at line 63 of file bier_errors.h.
#define BIER_missing_ref_description (BIER_ERROR_BASE + 13) |
Definition at line 61 of file bier_errors.h.
#define BIER_no_configured_rev_for_rev_rule (BIER_ERROR_BASE + 97) |
Definition at line 150 of file bier_errors.h.
#define BIER_no_export_priv (BIER_ERROR_BASE + 31) |
Definition at line 84 of file bier_errors.h.
#define BIER_no_exportable_revs (BIER_ERROR_BASE + 46) |
Definition at line 99 of file bier_errors.h.
#define BIER_no_fms_bootstrap_urls (BIER_ERROR_BASE + 77) |
Definition at line 130 of file bier_errors.h.
#define BIER_no_post_export_script (BIER_ERROR_BASE + 60) |
Definition at line 113 of file bier_errors.h.
#define BIER_no_pre_import_script (BIER_ERROR_BASE + 61) |
Definition at line 114 of file bier_errors.h.
#define BIER_no_released_revision_to_export (BIER_ERROR_BASE + 50) |
Definition at line 103 of file bier_errors.h.
#define BIER_no_revision_export_selector (BIER_ERROR_BASE + 48) |
Definition at line 101 of file bier_errors.h.
#define BIER_no_revision_of_given_status (BIER_ERROR_BASE + 58) |
Definition at line 111 of file bier_errors.h.
#define BIER_no_revision_selected_for_export (BIER_ERROR_BASE + 51) |
Definition at line 104 of file bier_errors.h.
#define BIER_no_target_site (BIER_ERROR_BASE + 18) |
Definition at line 69 of file bier_errors.h.
#define BIER_no_target_sites_when_xferring (BIER_ERROR_BASE + 27) |
Definition at line 80 of file bier_errors.h.
#define BIER_no_transfer_out_priv (BIER_ERROR_BASE + 38) |
Definition at line 91 of file bier_errors.h.
#define BIER_no_working_revision_to_export (BIER_ERROR_BASE + 49) |
Definition at line 102 of file bier_errors.h.
#define BIER_nothing_modified_to_export (BIER_ERROR_BASE + 43) |
Definition at line 96 of file bier_errors.h.
#define BIER_nothing_to_export (BIER_ERROR_BASE + 65) |
Definition at line 118 of file bier_errors.h.
#define BIER_object_not_checked_out_by_site (BIER_ERROR_BASE + 73) |
Definition at line 126 of file bier_errors.h.
#define BIER_out_of_memory (BIER_ERROR_BASE + 23) |
Definition at line 75 of file bier_errors.h.
#define BIER_preview_metafile_is_empty (BIER_ERROR_BASE + 56) |
Definition at line 109 of file bier_errors.h.
#define BIER_remotely_checked_out_object_already_exported (BIER_ERROR_BASE + 71) |
Definition at line 124 of file bier_errors.h.
#define BIER_require_import_site_priv (BIER_ERROR_BASE + 32) |
Definition at line 85 of file bier_errors.h.
#define BIER_require_transfer_in_site_priv (BIER_ERROR_BASE + 45) |
Definition at line 98 of file bier_errors.h.
#define BIER_secondary_send_remote_checkin_failed (BIER_ERROR_BASE + 99) |
Definition at line 152 of file bier_errors.h.
#define BIER_set_export_ds_failed (BIER_ERROR_BASE + 15) |
Definition at line 65 of file bier_errors.h.
#define BIER_set_site_failed (BIER_ERROR_BASE + 6) |
Perhaps somebody removed the site half-way through the export operation?
Definition at line 44 of file bier_errors.h.
#define BIER_simulated_internal_error (BIER_ERROR_BASE + 108) |
Definition at line 161 of file bier_errors.h.
#define BIER_site_does_not_support_longer_id (BIER_ERROR_BASE + 98) |
Definition at line 151 of file bier_errors.h.
#define BIER_site_has_no_privilege_on_object (BIER_ERROR_BASE + 86) |
Definition at line 139 of file bier_errors.h.
#define BIER_site_lookup_failed (BIER_ERROR_BASE + 4) |
Perhaps somebody removed the site half-way through the export operation?
Definition at line 38 of file bier_errors.h.
#define BIER_site_mismatch_exclude_files (BIER_ERROR_BASE + 131) |
Definition at line 177 of file bier_errors.h.
#define BIER_site_no_import_priv_at_importing_site (BIER_ERROR_BASE + 93) |
Definition at line 146 of file bier_errors.h.
#define BIER_site_no_transfer_in_priv_at_importing_site (BIER_ERROR_BASE + 94) |
Definition at line 147 of file bier_errors.h.
#define BIER_site_not_defined_in_site_pref (BIER_ERROR_BASE + 90) |
Definition at line 143 of file bier_errors.h.
#define BIER_site_not_pom_object (BIER_ERROR_BASE + 5) |
Perhaps somebody removed the site half-way through the export operation?
Definition at line 41 of file bier_errors.h.
#define BIER_sst_cleanup_failed (BIER_ERROR_BASE + 104) |
Definition at line 157 of file bier_errors.h.
#define BIER_sst_client_determined_alive (BIER_ERROR_BASE + 110) |
Definition at line 163 of file bier_errors.h.
#define BIER_sst_client_determined_dead (BIER_ERROR_BASE + 111) |
Definition at line 164 of file bier_errors.h.
#define BIER_sst_client_undetermined (BIER_ERROR_BASE + 112) |
Definition at line 165 of file bier_errors.h.
#define BIER_sst_in_progress (BIER_ERROR_BASE + 103) |
Definition at line 156 of file bier_errors.h.
#define BIER_sst_prev_recovery_required (BIER_ERROR_BASE + 107) |
Definition at line 160 of file bier_errors.h.
#define BIER_sst_recovery_replica_required (BIER_ERROR_BASE + 106) |
Definition at line 159 of file bier_errors.h.
#define BIER_sst_recovery_required (BIER_ERROR_BASE + 102) |
Definition at line 155 of file bier_errors.h.
#define BIER_sst_server_determined_alive (BIER_ERROR_BASE + 113) |
Definition at line 166 of file bier_errors.h.
#define BIER_sst_server_determined_alive_is_ours (BIER_ERROR_BASE + 115) |
Definition at line 168 of file bier_errors.h.
#define BIER_sst_server_undetermined (BIER_ERROR_BASE + 114) |
Definition at line 167 of file bier_errors.h.
#define BIER_sst_session_in_use (BIER_ERROR_BASE + 116) |
Definition at line 169 of file bier_errors.h.
#define BIER_store_failed (BIER_ERROR_BASE + 8) |
Definition at line 48 of file bier_errors.h.
#define BIER_tool_does_not_exist (BIER_ERROR_BASE + 67) |
Definition at line 120 of file bier_errors.h.
#define BIER_type_does_not_exist (BIER_ERROR_BASE + 66) |
Definition at line 119 of file bier_errors.h.
#define BIER_unable_to_delete_staging_dir (BIER_ERROR_BASE + 105) |
Definition at line 158 of file bier_errors.h.
#define BIER_unable_to_exclude (BIER_ERROR_BASE + 28) |
Definition at line 81 of file bier_errors.h.
#define BIER_unable_to_execute_export_script (BIER_ERROR_BASE + 62) |
Definition at line 115 of file bier_errors.h.
#define BIER_unable_to_execute_import_script (BIER_ERROR_BASE + 63) |
Definition at line 116 of file bier_errors.h.
#define BIER_unable_to_export_unpublished (BIER_ERROR_BASE + 52) |
Definition at line 105 of file bier_errors.h.
#define BIER_unable_to_include_rel (BIER_ERROR_BASE + 36) |
Definition at line 89 of file bier_errors.h.
#define BIER_unable_to_include_sec_obj (BIER_ERROR_BASE + 37) |
Definition at line 90 of file bier_errors.h.
#define BIER_unable_to_locate (BIER_ERROR_BASE + 24) |
Definition at line 76 of file bier_errors.h.
#define BIER_unable_to_remote_checkout (BIER_ERROR_BASE + 84) |
Definition at line 137 of file bier_errors.h.
#define BIER_unable_to_remote_export (BIER_ERROR_BASE + 83) |
Definition at line 136 of file bier_errors.h.
#define BIER_unknown_object (BIER_ERROR_BASE + 141) |
Importing failure. An unknown Class/Type encountered during import
Definition at line 199 of file bier_errors.h.
#define BIER_unknown_sst_state (BIER_ERROR_BASE + 100) |
Definition at line 153 of file bier_errors.h.
#define BIER_user_and_group_not_defined_at_remote_site (BIER_ERROR_BASE + 81) |
Definition at line 134 of file bier_errors.h.
#define BIER_user_denied_remote_import_privilege_for_site (BIER_ERROR_BASE + 53) |
Definition at line 106 of file bier_errors.h.
#define BIER_user_denied_transfer_ownership_privilege_for_site (BIER_ERROR_BASE + 54) |
Definition at line 107 of file bier_errors.h.
#define BIER_user_has_no_privilege_on_object (BIER_ERROR_BASE + 85) |
Definition at line 138 of file bier_errors.h.
#define BIER_user_no_import_priv (BIER_ERROR_BASE + 95) |
Definition at line 148 of file bier_errors.h.
#define BIER_user_no_import_priv_at_importing_site (BIER_ERROR_BASE + 91) |
Definition at line 144 of file bier_errors.h.
#define BIER_user_no_transfer_in_priv (BIER_ERROR_BASE + 96) |
Definition at line 149 of file bier_errors.h.
#define BIER_user_no_transfer_in_priv_at_importing_site (BIER_ERROR_BASE + 92) |
Definition at line 145 of file bier_errors.h.
#define BIER_user_not_defined_at_remote_site (BIER_ERROR_BASE + 79) |
Definition at line 132 of file bier_errors.h.
#define BIER_user_not_defined_in_site_pref (BIER_ERROR_BASE + 89) |
Definition at line 142 of file bier_errors.h.
#define BIER_user_not_member_of_group_at_remote_site (BIER_ERROR_BASE + 82) |
Definition at line 135 of file bier_errors.h.
#define BIER_valid_for_assy_export_only (BIER_ERROR_BASE + 44) |
Definition at line 97 of file bier_errors.h.
#define BIER_valid_with_all_revs_only (BIER_ERROR_BASE + 47) |
Definition at line 100 of file bier_errors.h.
#define BIER_verify_object_at_target_fail (BIER_ERROR_BASE + 139) |
Definition at line 192 of file bier_errors.h.
#define BIER_write_failed (BIER_ERROR_BASE + 9) |
Definition at line 50 of file bier_errors.h.