#define ENQ_doNotClearText 1 |
Definition at line 27 of file enq_errors.h.
#define ENQ_ERROR_BASE ERROR_ENQ_base |
Definition at line 31 of file enq_errors.h.
#define ENQ_fail 1 |
Definition at line 24 of file enq_errors.h.
#define ENQ_internal_error ENQ_ERROR_BASE + 1 |
Cause: Anything not covered by a more specific error code. May be caused by -
Definition at line 47 of file enq_errors.h.
#define ENQ_invalid_attribute ENQ_ERROR_BASE + 4 |
Definition at line 66 of file enq_errors.h.
#define ENQ_invalid_class ENQ_ERROR_BASE + 7 |
Definition at line 68 of file enq_errors.h.
#define ENQ_invalid_date ENQ_ERROR_BASE + 24 |
Cause: The date passed is not a valid date.
Action: Correct date.
Definition at line 83 of file enq_errors.h.
#define ENQ_invalid_expression ENQ_ERROR_BASE + 20 |
Definition at line 74 of file enq_errors.h.
#define ENQ_invalid_pseudo_attr (ENQ_ERROR_BASE + 36) |
Cause: The alias is already used by an existing object.
Action: Use different alias id.
Definition at line 111 of file enq_errors.h.
#define ENQ_invalid_pseudo_calias (ENQ_ERROR_BASE + 33) |
Cause: The alias is already used by an existing object.
Action: Use different alias id.
Definition at line 104 of file enq_errors.h.
#define ENQ_invalid_query ENQ_ERROR_BASE + 11 |
Definition at line 70 of file enq_errors.h.
#define ENQ_invalid_set_expression ENQ_ERROR_BASE + 12 |
Definition at line 72 of file enq_errors.h.
#define ENQ_invalid_value ENQ_ERROR_BASE + 21 |
Definition at line 76 of file enq_errors.h.
#define ENQ_max_err_code ENQ_ERROR_BASE + 37 |
Definition at line 113 of file enq_errors.h.
#define ENQ_min_err_code ENQ_ERROR_BASE |
Definition at line 32 of file enq_errors.h.
#define ENQ_not_implemented ENQ_ERROR_BASE + 2 |
Cause: The operation may work in a future version, but not yet. This may refer to an operation being available in a particular context.
Action: Check for availability of feature in later release.
Definition at line 56 of file enq_errors.h.
#define ENQ_not_initialised ENQ_ERROR_BASE + 3 |
Cause: The ENQ has not been initialized.
Action: The function ENQ_init_module must be called prior to any other ENQ activities.
Definition at line 64 of file enq_errors.h.
#define ENQ_ok 0 |
Definition at line 23 of file enq_errors.h.
#define ENQ_okToClearText 0 |
Definition at line 26 of file enq_errors.h.
#define ENQ_out_of_memory (ENQ_ERROR_BASE + 27) |
Cause: POM out of memory caught in ENQ.
Action: Check application is freeing used memory.
Definition at line 90 of file enq_errors.h.
#define ENQ_timeout (ENQ_ERROR_BASE + 30) |
Cause: POM timeout caught.
Action: Retry operation, or setup automatic retries via POM.
Definition at line 97 of file enq_errors.h.
#define ENQ_UNKNOWN_TYPE -1 |
Definition at line 25 of file enq_errors.h.