#define FL_addEmptyEntry (EMH_FL_error_base + 133) |
Definition at line 133 of file folder_errors.h.
#define FL_alreadyCollapsed (EMH_FL_error_base + 122) |
Definition at line 123 of file folder_errors.h.
#define FL_alreadyExpanded (EMH_FL_error_base + 120) |
Definition at line 121 of file folder_errors.h.
#define FL_cannot_add_null_tag (EMH_FL_error_base + 5) |
A folder may not be added to itself nor can a NULLTAG be added.
Definition at line 45 of file folder_errors.h.
#define FL_cannot_add_self (EMH_FL_error_base + 4) |
Definition at line 42 of file folder_errors.h.
#define FL_cantCollapseNonFolder (EMH_FL_error_base + 119) |
Definition at line 120 of file folder_errors.h.
#define FL_cantCutFromInBox (EMH_FL_error_base + 150) |
Definition at line 150 of file folder_errors.h.
#define FL_cantCutHomeFolder (EMH_FL_error_base + 143) |
Definition at line 143 of file folder_errors.h.
#define FL_cantCutMailFolder (EMH_FL_error_base + 114) |
Definition at line 115 of file folder_errors.h.
#define FL_cantCutNewStuff (EMH_FL_error_base + 115) |
Definition at line 116 of file folder_errors.h.
#define FL_cantDeleteFolderOwnedByOthers (EMH_FL_error_base + 153) |
Definition at line 153 of file folder_errors.h.
#define FL_cantDestroyHomeFolder (EMH_FL_error_base + 117) |
Definition at line 118 of file folder_errors.h.
#define FL_cantDestroyMailFolder (EMH_FL_error_base + 116) |
Definition at line 117 of file folder_errors.h.
#define FL_cantDestroyNSFFolder (EMH_FL_error_base + 118) |
Definition at line 119 of file folder_errors.h.
#define FL_cantExpandNonFolder (EMH_FL_error_base + 121) |
Definition at line 122 of file folder_errors.h.
#define FL_cantExportContained (EMH_FL_error_base + 16) |
Definition at line 80 of file folder_errors.h.
#define FL_cantExportProjectBackups (EMH_FL_error_base + 155) |
Definition at line 155 of file folder_errors.h.
#define FL_cantExportSpecial (EMH_FL_error_base + 152) |
Definition at line 152 of file folder_errors.h.
#define FL_cantImportContained (EMH_FL_error_base + 17) |
Definition at line 81 of file folder_errors.h.
#define FL_cantImportMultipleObjects (EMH_FL_error_base + 141) |
Definition at line 141 of file folder_errors.h.
#define FL_cantImportNonDirectory (EMH_FL_error_base + 142) |
Definition at line 142 of file folder_errors.h.
#define FL_cantImportToNonFolder (EMH_FL_error_base + 128) |
Definition at line 129 of file folder_errors.h.
#define FL_cantInsertNonWSO (EMH_FL_error_base + 15) |
Definition at line 78 of file folder_errors.h.
#define FL_cantInsertToNonFolder (EMH_FL_error_base + 111) |
Definition at line 112 of file folder_errors.h.
#define FL_cantLatestNonFolder (EMH_FL_error_base + 127) |
Definition at line 128 of file folder_errors.h.
#define FL_cantModifyAFrozenFolder (EMH_FL_error_base + 14) |
Definition at line 77 of file folder_errors.h.
#define FL_cantMoveBlocks (EMH_FL_error_base + 108) |
Definition at line 109 of file folder_errors.h.
#define FL_cantPasteToInBox (EMH_FL_error_base + 151) |
Definition at line 151 of file folder_errors.h.
#define FL_clipboardReadFailed (EMH_FL_error_base + 110) |
Definition at line 111 of file folder_errors.h.
#define FL_clipboardWriteFailed (EMH_FL_error_base + 109) |
Definition at line 110 of file folder_errors.h.
#define FL_columnWidth (EMH_FL_error_base + 123) |
Definition at line 124 of file folder_errors.h.
#define FL_cutAccessForbidden (EMH_FL_error_base + 145) |
Definition at line 145 of file folder_errors.h.
#define FL_datasetAutoLatest (EMH_FL_error_base + 139) |
Definition at line 139 of file folder_errors.h.
#define FL_description_limit (EMH_FL_error_base + 13) |
This error is generated if a description input is more than 240 char long
Definition at line 75 of file folder_errors.h.
#define FL_dontKnowHowToSaveNonFolder (EMH_FL_error_base + 126) |
Definition at line 127 of file folder_errors.h.
#define FL_duplicate_name (EMH_FL_error_base + 8) |
When a preference of "FL_duplicates_not_allowed true" is in effect.
Definition at line 54 of file folder_errors.h.
#define FL_duplicateEntry (EMH_FL_error_base + 132) |
Definition at line 132 of file folder_errors.h.
#define FL_emptyColumnWidth (EMH_FL_error_base + 138) |
Definition at line 138 of file folder_errors.h.
#define FL_errorDelete (EMH_FL_error_base + 129) |
Definition at line 130 of file folder_errors.h.
#define FL_initialization_failed (EMH_FL_error_base + 9) |
The initialization of a folder failed.
Definition at line 57 of file folder_errors.h.
#define FL_insertNSFFailed (EMH_FL_error_base + 136) |
Definition at line 136 of file folder_errors.h.
#define FL_insertObjsFailed (EMH_FL_error_base + 134) |
Definition at line 134 of file folder_errors.h.
#define FL_invalid_FSC (EMH_FL_error_base + 1) |
Definition at line 92 of file folder_errors.h.
#define FL_invalid_FSO (EMH_FL_error_base + 2) |
Definition at line 93 of file folder_errors.h.
#define FL_invalid_index (EMH_FL_error_base + 3) |
If any of the indexes provided by the move command is invalid, this error code is generated
Definition at line 40 of file folder_errors.h.
#define FL_invalid_sort_criteria (EMH_FL_error_base + 1) |
Invalid sort criteria
Definition at line 31 of file folder_errors.h.
#define FL_invalid_sort_order (EMH_FL_error_base + 2) |
Invalid sort order
Definition at line 34 of file folder_errors.h.
#define FL_invalidColumnWidth (EMH_FL_error_base + 137) |
Definition at line 137 of file folder_errors.h.
#define FL_moveDownDiffParent (EMH_FL_error_base + 107) |
Definition at line 108 of file folder_errors.h.
#define FL_moveDownHetero (EMH_FL_error_base + 105) |
Definition at line 106 of file folder_errors.h.
#define FL_moveDownLast (EMH_FL_error_base + 106) |
Definition at line 107 of file folder_errors.h.
#define FL_moveUpDiffParent (EMH_FL_error_base + 104) |
Definition at line 105 of file folder_errors.h.
#define FL_moveUpHetero (EMH_FL_error_base + 102) |
Definition at line 103 of file folder_errors.h.
#define FL_moveUpTop (EMH_FL_error_base + 103) |
Definition at line 104 of file folder_errors.h.
#define FL_name_limit (EMH_FL_error_base + 12) |
This error is generated if a name input is more than 32 char long
Definition at line 72 of file folder_errors.h.
#define FL_name_required (EMH_FL_error_base + 10) |
This error is generated if a name is not provided when the preference for not allowing duplicate names is active. See FL_duplicate_name
Definition at line 63 of file folder_errors.h.
#define FL_no_save (EMH_FL_error_base + 11) |
This error is generated if users want to save a folder that has not yet been modified
Definition at line 69 of file folder_errors.h.
#define FL_noneToPaste (EMH_FL_error_base + 101) |
Definition at line 102 of file folder_errors.h.
#define FL_nonIntColumnWidth (EMH_FL_error_base + 140) |
Definition at line 140 of file folder_errors.h.
#define FL_noReadAccessToLatest (EMH_FL_error_base + 148) |
Definition at line 148 of file folder_errors.h.
#define FL_noStatuses (EMH_FL_error_base + 147) |
Definition at line 147 of file folder_errors.h.
#define FL_not_found (EMH_FL_error_base + 6) |
Specified object is not in the folder
Definition at line 48 of file folder_errors.h.
#define FL_notApplicableToRoot (EMH_FL_error_base + 113) |
Definition at line 114 of file folder_errors.h.
#define FL_nothingToCopy (EMH_FL_error_base + 112) |
Definition at line 113 of file folder_errors.h.
#define FL_noWriteAccessToLatest (EMH_FL_error_base + 149) |
Definition at line 149 of file folder_errors.h.
#define FL_object_already_added (EMH_FL_error_base + 7) |
Specified object for insertion in a folder already exists in the folder.
Definition at line 51 of file folder_errors.h.
#define FL_object_already_added_as (EMH_FL_error_base + 154) |
Definition at line 154 of file folder_errors.h.
#define FL_pasteAccessForbidden (EMH_FL_error_base + 144) |
Definition at line 144 of file folder_errors.h.
#define FL_requiredItemRevisons (EMH_FL_error_base + 146) |
Definition at line 146 of file folder_errors.h.
#define FL_saveColumnsPrefFailed (EMH_FL_error_base + 125) |
Definition at line 126 of file folder_errors.h.
#define FL_saveColumnWidthPrefFailed (EMH_FL_error_base + 124) |
Definition at line 125 of file folder_errors.h.
#define FL_saveWsoPrefFailed (EMH_FL_error_base + 131) |
Definition at line 131 of file folder_errors.h.
#define FL_staleObjPtr (EMH_FL_error_base + 135) |
Definition at line 135 of file folder_errors.h.