#define FORM_bad_name EMH_FORM_error_base + 12 |
Definition at line 48 of file form_errors.h.
#define FORM_bad_value EMH_FORM_error_base + 3 |
Value for attribute is bad
Definition at line 36 of file form_errors.h.
#define FORM_cannot_open_pref_file EMH_FORM_error_base + 24 |
Definition at line 62 of file form_errors.h.
#define FORM_copy_error EMH_FORM_error_base + 11 |
Definition at line 47 of file form_errors.h.
#define FORM_create_error EMH_FORM_error_base + 5 |
Definition at line 41 of file form_errors.h.
#define FORM_definition_file EMH_FORM_error_base + 1 |
Def file doesn't exist or POMClassName not defined in file
Definition at line 30 of file form_errors.h.
#define FORM_delete_error EMH_FORM_error_base + 6 |
Definition at line 42 of file form_errors.h.
#define FORM_duplicate_widget_name EMH_FORM_error_base + 13 |
Definition at line 50 of file form_errors.h.
#define FORM_invalid_class_name EMH_FORM_error_base + 17 |
Definition at line 54 of file form_errors.h.
#define FORM_invalid_form_entry_string EMH_FORM_error_base + 14 |
Definition at line 51 of file form_errors.h.
#define FORM_invalid_non_null_data EMH_FORM_error_base + 15 |
Definition at line 52 of file form_errors.h.
#define FORM_invalid_POM_class EMH_FORM_error_base + 2 |
POM class doesn't exist
Definition at line 33 of file form_errors.h.
#define FORM_load_error EMH_FORM_error_base + 7 |
Definition at line 43 of file form_errors.h.
#define FORM_no_change_type EMH_FORM_error_base + 18 |
Definition at line 55 of file form_errors.h.
#define FORM_no_field_for_label EMH_FORM_error_base + 16 |
Definition at line 53 of file form_errors.h.
#define FORM_no_form_data EMH_FORM_error_base + 29 |
Definition at line 67 of file form_errors.h.
#define FORM_no_read_values EMH_FORM_error_base + 19 |
Definition at line 56 of file form_errors.h.
#define FORM_no_top_level_dialog_widget EMH_FORM_error_base + 20 |
Definition at line 57 of file form_errors.h.
#define FORM_POMClassName EMH_FORM_error_base + 4 |
POMClassName in uil file is missing or invalid
Definition at line 39 of file form_errors.h.
#define FORM_refresh_error EMH_FORM_error_base + 10 |
Definition at line 46 of file form_errors.h.
#define FORM_save_error EMH_FORM_error_base + 9 |
Definition at line 45 of file form_errors.h.
#define FORM_type_already_exits EMH_FORM_error_base + 21 |
Definition at line 59 of file form_errors.h.
#define FORM_type_cant_modify_name EMH_FORM_error_base + 25 |
Definition at line 63 of file form_errors.h.
#define FORM_type_instance_referenced EMH_FORM_error_base + 23 |
Definition at line 61 of file form_errors.h.
#define FORM_type_name_clash_with_classname EMH_FORM_error_base + 30 |
Definition at line 68 of file form_errors.h.
#define FORM_type_no_type_exists EMH_FORM_error_base + 22 |
Definition at line 60 of file form_errors.h.
#define FORM_type_no_uid_or_class EMH_FORM_error_base + 27 |
Definition at line 65 of file form_errors.h.
#define FORM_type_nota_privileged_user EMH_FORM_error_base + 28 |
Definition at line 66 of file form_errors.h.
#define FORM_type_wrong_class EMH_FORM_error_base + 31 |
Definition at line 69 of file form_errors.h.
#define FORM_type_wrong_type EMH_FORM_error_base + 26 |
Definition at line 64 of file form_errors.h.
#define FORM_unknown EMH_FORM_error_base + 0 |
Unknown internal error in Form
Definition at line 27 of file form_errors.h.
#define FORM_unload_error EMH_FORM_error_base + 8 |
Definition at line 44 of file form_errors.h.