#define GMS_briefcase_type_import_not_allowed (EMH_GMS_error_base+57) |
Source site defination in DB and briefcase creation type are not matching with each other, Therefore the briefcase import is not allowed.
Definition at line 210 of file gms_errors.h.
#define GMS_DS_type_not_supported (EMH_GMS_error_base+56) |
The Dataset type is not supported in configured export to unmanaged site
Definition at line 204 of file gms_errors.h.
#define GMS_ERROR_BASE EMH_GMS_error_base |
Definition at line 27 of file gms_errors.h.
#define GMS_fail_to_create_import_record (EMH_GMS_error_base+44) |
GMS fail to create import record
Definition at line 144 of file gms_errors.h.
#define GMS_fail_to_invoke_global_services_method (EMH_GMS_error_base+7) |
Error while invoking Global Services Method
Definition at line 65 of file gms_errors.h.
#define GMS_fail_to_login_to_global_services (EMH_GMS_error_base+6) |
Error while logging to Global Services
Definition at line 60 of file gms_errors.h.
#define GMS_fail_to_set_new_owning_site (EMH_GMS_error_base+5) |
Error while setting new owning site on specified object
Definition at line 55 of file gms_errors.h.
#define GMS_fail_to_set_ownership_xfer_pending_state (EMH_GMS_error_base+3) |
The specified object is locked for modification, can not set ownership transfer pending state on this object
Definition at line 44 of file gms_errors.h.
#define GMS_fail_to_xfer_bcz_xclude_objs (EMH_GMS_error_base+40) |
Failed to transfer ownership since required object is in user specified exclude list
Definition at line 124 of file gms_errors.h.
#define GMS_fail_to_xfer_ownership (EMH_GMS_error_base+2) |
Site ownership transfer error code The specified object is locked for modification, Site ownership can not transfer on this object
Definition at line 38 of file gms_errors.h.
#define GMS_fsc_proxy_error (EMH_GMS_error_base+53) |
FSC proxy error
Definition at line 189 of file gms_errors.h.
#define GMS_gms_feature_not_available (EMH_GMS_error_base+42) |
GMS feature is not available
Definition at line 134 of file gms_errors.h.
#define GMS_GRM_relation_error (EMH_GMS_error_base+55) |
The GRM relation for CAD dataset is missing in the XML file
Definition at line 199 of file gms_errors.h.
#define GMS_invalid_briefcase_container (EMH_GMS_error_base+36) |
The given "TC_APPLICATION" attribute value is not Offline GMS in the container
Definition at line 104 of file gms_errors.h.
#define GMS_invalid_gsidentity_tag (EMH_GMS_error_base+43) |
GMS invalid gsidentity tag
Definition at line 139 of file gms_errors.h.
#define GMS_invalid_input (EMH_GMS_error_base+1) |
Definition at line 28 of file gms_errors.h.
#define GMS_invalid_offline_dataset_name (EMH_GMS_error_base+32) |
Error while encountering a invalid dataset name
Definition at line 84 of file gms_errors.h.
#define GMS_invalid_offline_dataset_type (EMH_GMS_error_base+33) |
Error while encountering a invalid dataset type
Definition at line 89 of file gms_errors.h.
#define GMS_invalid_offline_metadata_file (EMH_GMS_error_base+38) |
The following required attributes are missing from the ImanFile element: 1$.
Definition at line 114 of file gms_errors.h.
#define GMS_invalid_root_path (EMH_GMS_error_base+35) |
Error if root volume directory is NULL
Definition at line 99 of file gms_errors.h.
#define GMS_invalid_source_site (EMH_GMS_error_base+30) |
Offline GMS will use numbers from 30 Error while encountering a null source site id
Definition at line 74 of file gms_errors.h.
#define GMS_invalid_target_site (EMH_GMS_error_base+31) |
Error while encountering a null target site id
Definition at line 79 of file gms_errors.h.
#define GMS_invalid_uid (EMH_GMS_error_base+41) |
Error invalid UID for GSID object
Definition at line 129 of file gms_errors.h.
#define GMS_more_DS_vers_error (EMH_GMS_error_base+54) |
More than one dataset versions exported in configured export to unmanaged site
Definition at line 194 of file gms_errors.h.
#define GMS_no_ownership_xfer_pending_state (EMH_GMS_error_base+4) |
The specified object is not in ownership transfer pending state hence can not set new owning site on this object
Definition at line 50 of file gms_errors.h.
#define GMS_nothing_to_process (EMH_GMS_error_base+52) |
The GSID object to process is invalid
Definition at line 184 of file gms_errors.h.
#define GMS_offline_cannot_transfer_ownership (EMH_GMS_error_base+39) |
Error to prevent transfer of ownership if variable not set to true
Definition at line 119 of file gms_errors.h.
#define GMS_om_dataset_not_exists (EMH_GMS_error_base+49) |
Failed to find the recovery dataset
Definition at line 169 of file gms_errors.h.
#define GMS_om_dataset_too_many (EMH_GMS_error_base+50) |
Found more than one recovery datasets
Definition at line 174 of file gms_errors.h.
#define GMS_om_transaction_out_of_sync (EMH_GMS_error_base+51) |
Transaction ID recorded on the dataset is out of sync
Definition at line 179 of file gms_errors.h.
#define GMS_recovery_failed (EMH_GMS_error_base+48) |
Site Transfer on the object succeded but failed to complete the cleanup action
Definition at line 164 of file gms_errors.h.
#define GMS_recovery_required (EMH_GMS_error_base+47) |
Recovery is required for the Object
Definition at line 159 of file gms_errors.h.
#define GMS_site_transfer_export_in_progress (EMH_GMS_error_base+46) |
Site Transfer on the object with the remote site is in progress
Definition at line 154 of file gms_errors.h.
#define GMS_transaction_id_empty (EMH_GMS_error_base+45) |
Transaction ID for the Site Transfer operation is empty
Definition at line 149 of file gms_errors.h.
#define GMS_unable_to_modify_metadata_files (EMH_GMS_error_base+37) |
Unable to modify the metadata file of the given briefcase container
Definition at line 109 of file gms_errors.h.
#define GMS_zero_target_sites (EMH_GMS_error_base+34) |
Error if there are Zero target sites
Definition at line 94 of file gms_errors.h.