#define GRM_cannot_delete_relation (EMH_GRM_error_base + 11) |
Definition at line 38 of file grm_errors.h.
#define GRM_cannot_delete_relation_type (EMH_GRM_error_base + 12) |
Definition at line 39 of file grm_errors.h.
#define GRM_duplicate_relation_type (EMH_GRM_error_base + 5) |
Definition at line 32 of file grm_errors.h.
#define GRM_duplicate_relations_exist (EMH_GRM_error_base + 15) |
Definition at line 42 of file grm_errors.h.
#define GRM_internal_error (EMH_GRM_error_base + 2) |
Definition at line 29 of file grm_errors.h.
#define GRM_invalid_primary_object (EMH_GRM_error_base + 6) |
Definition at line 33 of file grm_errors.h.
#define GRM_invalid_relation_primary_for_type (EMH_GRM_error_base + 16) |
Definition at line 43 of file grm_errors.h.
#define GRM_invalid_relation_type (EMH_GRM_error_base + 3) |
Definition at line 30 of file grm_errors.h.
#define GRM_invalid_secondary_object (EMH_GRM_error_base + 7) |
Definition at line 34 of file grm_errors.h.
#define GRM_invalid_set_of_arguments (EMH_GRM_error_base + 14) |
Definition at line 41 of file grm_errors.h.
#define GRM_invalid_user_data (EMH_GRM_error_base + 8) |
Definition at line 35 of file grm_errors.h.
#define GRM_not_initialized (EMH_GRM_error_base + 1) |
Definition at line 28 of file grm_errors.h.
#define GRM_relation_already_exists (EMH_GRM_error_base + 10) |
Definition at line 37 of file grm_errors.h.
#define GRM_relation_does_not_exist (EMH_GRM_error_base + 9) |
Definition at line 36 of file grm_errors.h.
#define GRM_relation_not_allowed (EMH_GRM_error_base + 13) |
Definition at line 40 of file grm_errors.h.
#define GRM_undefined_relation_type (EMH_GRM_error_base + 4) |
Definition at line 31 of file grm_errors.h.