#define GCS_err_CP_already_exists (EMH_ICS_error_base + 804) |
Can't create GCS CP! There is already a GCS CP for this ICO/CPD/CPIndex combination!
Definition at line 808 of file ics_errors.h.
#define GCS_err_CPD_already_exists (EMH_ICS_error_base + 807) |
Can't create GCS CPD! There is already a GCS CPD with this CPDIndex for this component class.
Definition at line 817 of file ics_errors.h.
#define GCS_err_CPD_component_class_doesnt_match (EMH_ICS_error_base + 803) |
Component classes of GCS CPD and Component do not match!
Definition at line 805 of file ics_errors.h.
#define GCS_err_CT_already_exists (EMH_ICS_error_base + 800) |
Can't create GCS CT! This GCS CT name is already in use.
Definition at line 796 of file ics_errors.h.
#define GCS_err_CT_wrong_attribute_count (EMH_ICS_error_base + 801) |
Given attribute count does not match to the GCS CT attribute count.
Definition at line 799 of file ics_errors.h.
#define GCS_err_first_substring_index_out_of_range (EMH_ICS_error_base + 811) |
First substring index out of range of ICO value.
Definition at line 829 of file ics_errors.h.
#define GCS_err_incorrect_shape_setting (EMH_ICS_error_base + 808) |
Shape is not set correctly in GCS CP.
Definition at line 820 of file ics_errors.h.
#define GCS_err_multiple_CPs_found_for_occ (EMH_ICS_error_base + 810) |
Multiple GCS CP ICO tags found for occurrence.
Definition at line 826 of file ics_errors.h.
#define GCS_err_no_CP_found (EMH_ICS_error_base + 805) |
No GCS CP found for this ICO/CPD/CPIndex combination.
Definition at line 811 of file ics_errors.h.
#define GCS_err_no_CP_found_for_occ (EMH_ICS_error_base + 809) |
No GCS CP ICO tag found for occurrence.
Definition at line 823 of file ics_errors.h.
#define GCS_err_no_CT_found (EMH_ICS_error_base + 802) |
No GCS CT found with this name.
Definition at line 802 of file ics_errors.h.
#define GCS_err_second_substring_index_out_of_range (EMH_ICS_error_base + 812) |
Second substring index out of range of ICO value.
Definition at line 832 of file ics_errors.h.
#define GCS_err_system_is_inconsistent (EMH_ICS_error_base + 806) |
There are multiple GCS CPs found for this ICO/CPD/CPIndex combination.
Definition at line 814 of file ics_errors.h.
#define ICS_attr_mapping_value_formatting (EMH_ICS_error_base + 655) |
Error formatting attribute value:
Definition at line 506 of file ics_errors.h.
#define ICS_attrsync_runtime_buffer_full (EMH_ICS_error_base + 545) |
Internal error, buffer full for runtime Ico or Atrr
Definition at line 177 of file ics_errors.h.
#define ICS_autocompute_cyclicId (EMH_ICS_error_base + 863) |
cyclic id
Definition at line 878 of file ics_errors.h.
#define ICS_autocompute_invalidClass (EMH_ICS_error_base + 859) |
Invalid class
Definition at line 866 of file ics_errors.h.
#define ICS_autocompute_invalidId (EMH_ICS_error_base + 856) |
Invalid id
Definition at line 857 of file ics_errors.h.
#define ICS_autocompute_nonautocomputeId (EMH_ICS_error_base + 857) |
not an autcompute attribute id
Definition at line 860 of file ics_errors.h.
#define ICS_autocompute_nonInput_AttrId (EMH_ICS_error_base + 862) |
Attribute is not an input attribute
Definition at line 875 of file ics_errors.h.
#define ICS_autocompute_unregistered_classAttrId (EMH_ICS_error_base + 860) |
Autocompute method is not registered for class attribute
Definition at line 869 of file ics_errors.h.
#define ICS_autocompute_unregistered_method (EMH_ICS_error_base + 858) |
Method not registered for the autocompute attribute
Definition at line 863 of file ics_errors.h.
#define ICS_autocompute_unregistered_viewAttrId (EMH_ICS_error_base + 861) |
Autocompute method is not registered for class attribute
Definition at line 872 of file ics_errors.h.
#define ICS_can_not_delete_sml_objects (EMH_ICS_error_base + 546) |
Internal error, can not delete the SML object
Definition at line 180 of file ics_errors.h.
#define ICS_cannot_add_image_to_type (EMH_ICS_error_base + 508) |
Cannot add image to this type
Definition at line 66 of file ics_errors.h.
#define ICS_cannot_classify_wso (EMH_ICS_error_base + 503) |
Cannot classify the Workspace Object
Definition at line 51 of file ics_errors.h.
#define ICS_empty_name (EMH_ICS_error_base + 511) |
Empty name specified
Definition at line 75 of file ics_errors.h.
#define ICS_empty_resource_id (EMH_ICS_error_base + 510) |
Empty Resource Id
Definition at line 72 of file ics_errors.h.
#define ICS_err_all_hierarchy_shares_failed (EMH_ICS_error_base + 553) |
No hierarchy object could be shared.
Definition at line 201 of file ics_errors.h.
#define ICS_err_array_index_out_of_bounds (EMH_ICS_error_base + 611) |
Array index out of bounds.
Definition at line 375 of file ics_errors.h.
#define ICS_err_attr_mapping (EMH_ICS_error_base + 648) |
Error during Classification attribute mapping: 1$s
Definition at line 485 of file ics_errors.h.
#define ICS_err_attr_mapping_ico_creation (EMH_ICS_error_base + 660) |
Could not create ICO.
Definition at line 521 of file ics_errors.h.
#define ICS_err_attr_mapping_ico_creation_gaps (EMH_ICS_error_base + 661) |
The number of attribute mapping 'ICS_CREATE([number])' is too big (no ICO number ([number] - 1) exists).
Definition at line 524 of file ics_errors.h.
#define ICS_err_attr_mapping_ico_does_not_exist (EMH_ICS_error_base + 647) |
No ICO for attribute mapping.
Definition at line 482 of file ics_errors.h.
#define ICS_err_attr_mapping_ico_unit_mismatch (EMH_ICS_error_base + 850) |
The classification object could not be created because source and target classes have different unit systems.
Definition at line 835 of file ics_errors.h.
#define ICS_err_attr_mapping_no_ico (EMH_ICS_error_base + 650) |
There aren't any ICOs for attribute mapping.
Definition at line 491 of file ics_errors.h.
#define ICS_err_attr_mapping_no_value_set (EMH_ICS_error_base + 653) |
No attribute value set.
Definition at line 500 of file ics_errors.h.
#define ICS_err_attr_mapping_vla (EMH_ICS_error_base + 865) |
Problem during Classification attribute mapping: The given VLA position does not exist.
Definition at line 887 of file ics_errors.h.
#define ICS_err_attribute_does_not_exist (EMH_ICS_error_base + 527) |
The Attribute does not exist
Definition at line 123 of file ics_errors.h.
#define ICS_err_attribute_is_no_keylov (EMH_ICS_error_base + 612) |
The attribute is not a Key LOV.
Definition at line 378 of file ics_errors.h.
#define ICS_err_attribute_not_in_ico (EMH_ICS_error_base + 652) |
Attribute not defined in (any of) the ICO(s).
Definition at line 497 of file ics_errors.h.
#define ICS_err_attribute_not_unique (EMH_ICS_error_base + 525) |
The Attribute is not unique
Definition at line 117 of file ics_errors.h.
#define ICS_err_cannot_create_class_id_using_old_sid_but_no_cid (EMH_ICS_error_base + 688) |
To generate a unique id you must not specify the old Subclass ID but not the old Class ID.
Definition at line 605 of file ics_errors.h.
#define ICS_err_cannot_create_files (EMH_ICS_error_base + 595) |
Files cannot be created.
Definition at line 327 of file ics_errors.h.
#define ICS_err_cannot_create_pf_member_from_classifying_ico (EMH_ICS_error_base + 574) |
A classifying instance cannot be used for part family member creation (because it will not be possible to attach the item for the member part).
Definition at line 264 of file ics_errors.h.
#define ICS_err_cannot_create_pf_member_without_pft (EMH_ICS_error_base + 573) |
A part family member cannot be created without specifying a part family template.
Definition at line 261 of file ics_errors.h.
#define ICS_err_cannot_generate_class_id (EMH_ICS_error_base + 679) |
A class id could not be generated.
Definition at line 578 of file ics_errors.h.
#define ICS_err_cannot_remove_pft_with_members (EMH_ICS_error_base + 627) |
The mapping cannot be removed because Classification instances have been created.
Definition at line 423 of file ics_errors.h.
#define ICS_err_cannot_store_ico_in_view (EMH_ICS_error_base + 696) |
ICOs cannot be stored in a view.
Definition at line 629 of file ics_errors.h.
#define ICS_err_cant_put_group_under_class (EMH_ICS_error_base + 694) |
The group 1$s cannot not be moved/copied under class 1$s.
Definition at line 623 of file ics_errors.h.
#define ICS_err_class_does_not_exist (EMH_ICS_error_base + 528) |
The Class does not exist
Definition at line 126 of file ics_errors.h.
#define ICS_err_class_id_not_unique (EMH_ICS_error_base + 665) |
The id given to create a new class specifies an existing class.
Definition at line 536 of file ics_errors.h.
#define ICS_err_class_is_shared (EMH_ICS_error_base + 692) |
Class 1$s is shared.
Definition at line 617 of file ics_errors.h.
#define ICS_err_column_name_is_empty (EMH_ICS_error_base + 568) |
The column name is empty.
Definition at line 246 of file ics_errors.h.
#define ICS_err_could_not_create_file (EMH_ICS_error_base + 596) |
A file could not be created.
Definition at line 330 of file ics_errors.h.
#define ICS_err_could_not_create_item_id (EMH_ICS_error_base + 607) |
The item id could not be created.
Definition at line 363 of file ics_errors.h.
#define ICS_err_could_not_get_icos_for_attr_mapping (EMH_ICS_error_base + 649) |
Error getting ICOs for attribute mapping.
Definition at line 488 of file ics_errors.h.
#define ICS_err_could_not_open_file (EMH_ICS_error_base + 597) |
The file could not be opened.
Definition at line 333 of file ics_errors.h.
#define ICS_err_could_not_remove_object (EMH_ICS_error_base + 695) |
Could not remove object 1$s.
Definition at line 626 of file ics_errors.h.
#define ICS_err_could_not_set_tls_value (EMH_ICS_error_base + 600) |
The thread local value could not be set.
Definition at line 342 of file ics_errors.h.
#define ICS_err_could_not_share_object (EMH_ICS_error_base + 684) |
The object "%1$s" could not be shared.
Definition at line 593 of file ics_errors.h.
#define ICS_err_could_not_start_pdiserver (EMH_ICS_error_base + 569) |
The PDI Server for the graphics builder could not be started.
Definition at line 249 of file ics_errors.h.
#define ICS_err_different_value_in_duplicate (EMH_ICS_error_base + 678) |
An object to copy was given twice and the values for the new id are different.
Definition at line 575 of file ics_errors.h.
#define ICS_err_dont_convert_subclass_00 (EMH_ICS_error_base + 681) |
The subclass "00" must not be converted.
Definition at line 584 of file ics_errors.h.
#define ICS_err_duplicate_id (EMH_ICS_error_base + 672) |
The id was specified twice.
Definition at line 557 of file ics_errors.h.
#define ICS_err_empty_ior (EMH_ICS_error_base + 570) |
The IOR is empty.
Definition at line 252 of file ics_errors.h.
#define ICS_err_file_already_exists (EMH_ICS_error_base + 631) |
The file already exists
Definition at line 435 of file ics_errors.h.
#define ICS_err_function_not_implemented (EMH_ICS_error_base + 524) |
The Function is not implemented
Definition at line 114 of file ics_errors.h.
#define ICS_err_graphics_builder_invalid_option (EMH_ICS_error_base + 589) |
The graphics builder option is invalid.
Definition at line 309 of file ics_errors.h.
#define ICS_err_graphics_builder_invalid_option_value (EMH_ICS_error_base + 587) |
The graphics builder option value is invalid.
Definition at line 303 of file ics_errors.h.
#define ICS_err_graphics_builder_no_activation_method (EMH_ICS_error_base + 591) |
There is no activation method for the graphics builder.
Definition at line 315 of file ics_errors.h.
#define ICS_err_graphicsbuilder_invalid_activation_method (EMH_ICS_error_base + 586) |
The activation method for the graphics builder is invalid.
Definition at line 300 of file ics_errors.h.
#define ICS_err_graphicsbuilder_invalid_port (EMH_ICS_error_base + 588) |
The graphics builder port is invalid.
Definition at line 306 of file ics_errors.h.
#define ICS_err_graphicsbuilder_no_options (EMH_ICS_error_base + 590) |
There are no options given for the graphics builder.
Definition at line 312 of file ics_errors.h.
#define ICS_err_ico_belongs_to_part_family_member (EMH_ICS_error_base + 608) |
The Classification instance belongs to a part family member.
Definition at line 366 of file ics_errors.h.
#define ICS_err_ico_classifies_wrong_wso_for_pft (EMH_ICS_error_base + 633) |
The classification instance classifies a workspace object that is not related to the part family member.
Definition at line 441 of file ics_errors.h.
#define ICS_err_ico_not_stored_in_a_subclass (EMH_ICS_error_base + 613) |
The classification instance is not stored in a subclass.
Definition at line 381 of file ics_errors.h.
#define ICS_err_in_class_copy_operation (EMH_ICS_error_base + 697) |
Error in copy class operation. See syslog file for more information.
Definition at line 632 of file ics_errors.h.
#define ICS_err_in_class_move_operation (EMH_ICS_error_base + 698) |
Error in move class operation. See syslog file for more information.
Definition at line 635 of file ics_errors.h.
#define ICS_err_in_migrate_subclass_operation (EMH_ICS_error_base + 699) |
Error in migrate subclass operation. See syslog file for more information.
Definition at line 638 of file ics_errors.h.
#define ICS_err_in_set_read_only_meta_data (EMH_ICS_error_base + 731) |
Error while trying to set value to read only meta data for a dictionary attribute during plmxml import
Definition at line 742 of file ics_errors.h.
#define ICS_err_insert_old_mapping (EMH_ICS_error_base + 617) |
Internal error: Trying to insert a stored mapping as a new one.
Definition at line 393 of file ics_errors.h.
#define ICS_err_insert_second_mapping_for_item (EMH_ICS_error_base + 618) |
Trying to insert a second mapping for the Item.
Definition at line 396 of file ics_errors.h.
#define ICS_err_instance_neither_item_nor_revision (EMH_ICS_error_base + 626) |
The given tag neither belongs to an item nor to an item revision.
Definition at line 420 of file ics_errors.h.
#define ICS_err_internal_error (EMH_ICS_error_base + 999) |
Internal error.
Definition at line 899 of file ics_errors.h.
#define ICS_err_internal_keylov_definition_not_inserted (EMH_ICS_error_base + 605) |
Internal error: The key LOV definition was not inserted.
Definition at line 357 of file ics_errors.h.
#define ICS_err_internal_wrong_ico_id_for_pf (EMH_ICS_error_base + 577) |
Internal error: The instance ID does not match the part family.
Definition at line 273 of file ics_errors.h.
#define ICS_err_invalid_keylov_id (EMH_ICS_error_base + 630) |
The Key LOV id is invalid.
Definition at line 432 of file ics_errors.h.
#define ICS_err_invalid_parameter (EMH_ICS_error_base + 581) |
A parameter is invalid.
Definition at line 285 of file ics_errors.h.
#define ICS_err_invalid_property (EMH_ICS_error_base + 583) |
Invalid property.
Definition at line 291 of file ics_errors.h.
#define ICS_err_invalid_reference_type (EMH_ICS_error_base + 634) |
The reference type is invalid
Definition at line 444 of file ics_errors.h.
#define ICS_err_invalid_unit_id (EMH_ICS_error_base + 402) |
Unable to convert values between metric and non-metric using the specified unit
Definition at line 34 of file ics_errors.h.
#define ICS_err_invalid_value (EMH_ICS_error_base + 582) |
Invalid value.
Definition at line 288 of file ics_errors.h.
#define ICS_err_item_of_rev_already_used_as_template (EMH_ICS_error_base + 614) |
The Item of Revision is already used as part family template.
Definition at line 384 of file ics_errors.h.
#define ICS_err_item_or_rev_already_used_as_template (EMH_ICS_error_base + 616) |
Item or Revision is already used as part family template.
Definition at line 390 of file ics_errors.h.
#define ICS_err_kelov_does_not_exist (EMH_ICS_error_base + 526) |
The KeyLov does not exist
Definition at line 120 of file ics_errors.h.
#define ICS_err_keylov_key_not_unique (EMH_ICS_error_base + 629) |
The Key LOV key is not unique.
Definition at line 429 of file ics_errors.h.
#define ICS_err_keylov_key_unknown (EMH_ICS_error_base + 606) |
The Key LOV key is unknown.
Definition at line 360 of file ics_errors.h.
#define ICS_err_lock_already_obtained (EMH_ICS_error_base + 620) |
Classification lock was already obtained.
Definition at line 402 of file ics_errors.h.
#define ICS_err_lock_in_use (EMH_ICS_error_base + 622) |
Another user is querying the same data. Please try again later.
Definition at line 408 of file ics_errors.h.
#define ICS_err_lock_uninitialized (EMH_ICS_error_base + 619) |
Internal error: Classification lock is not initialized.
Definition at line 399 of file ics_errors.h.
#define ICS_err_lockobject_has_modify_lock (EMH_ICS_error_base + 628) |
The Classification lock is locked for modifying.
Definition at line 426 of file ics_errors.h.
#define ICS_err_lockobject_loaded (EMH_ICS_error_base + 621) |
Classification lock is loaded.
Definition at line 405 of file ics_errors.h.
#define ICS_err_mapping_column_not_found (EMH_ICS_error_base + 564) |
The column to map to could not be found.
Definition at line 234 of file ics_errors.h.
#define ICS_err_mapping_does_not_exist (EMH_ICS_error_base + 625) |
There is no mapping for this item / item revision.
Definition at line 417 of file ics_errors.h.
#define ICS_err_mapping_does_not_match_template (EMH_ICS_error_base + 601) |
The mapping does not match the template.
Definition at line 345 of file ics_errors.h.
#define ICS_err_mapping_is_empty (EMH_ICS_error_base + 566) |
The mapping is empty.
Definition at line 240 of file ics_errors.h.
#define ICS_err_mapping_must_not_be_used (EMH_ICS_error_base + 567) |
The mapping is not enabled. It must not be used.
Definition at line 243 of file ics_errors.h.
#define ICS_err_missing_parameter (EMH_ICS_error_base + 580) |
A parameter is missing.
Definition at line 282 of file ics_errors.h.
#define ICS_err_more_than_one_item_revision (EMH_ICS_error_base + 578) |
There is more than one item revision selected.
Definition at line 276 of file ics_errors.h.
#define ICS_err_more_than_one_part_family_template (EMH_ICS_error_base + 572) |
There is more than one part family template.
Definition at line 258 of file ics_errors.h.
#define ICS_err_more_than_one_view_for_template (EMH_ICS_error_base + 602) |
There is more than one template view.
Definition at line 348 of file ics_errors.h.
#define ICS_err_must_convert_views (EMH_ICS_error_base + 671) |
The functionality cannot be used because the views have not been converted to the new format yet.
Definition at line 554 of file ics_errors.h.
#define ICS_err_mutex_already_locked (EMH_ICS_error_base + 593) |
The mutex is already locked.
Definition at line 321 of file ics_errors.h.
#define ICS_err_mutex_locked (EMH_ICS_error_base + 592) |
The mutex is locked.
Definition at line 318 of file ics_errors.h.
#define ICS_err_mutex_not_locked (EMH_ICS_error_base + 594) |
The mutex is not locked.
Definition at line 324 of file ics_errors.h.
#define ICS_err_new_parent_not_writable (EMH_ICS_error_base + 667) |
The new parent of the class is not writable.
Definition at line 542 of file ics_errors.h.
#define ICS_err_no_attr (EMH_ICS_error_base + 656) |
No attribute with the given ID.
Definition at line 509 of file ics_errors.h.
#define ICS_err_no_attr_format (EMH_ICS_error_base + 657) |
No attribute format set.
Definition at line 512 of file ics_errors.h.
#define ICS_err_no_configured_revision (EMH_ICS_error_base + 562) |
No revision is configured.
Definition at line 228 of file ics_errors.h.
#define ICS_err_no_inclass_object (EMH_ICS_error_base + 556) |
The object is not a Classification object.
Definition at line 210 of file ics_errors.h.
#define ICS_err_no_key_lov_entries (EMH_ICS_error_base + 654) |
There are no entries in the Key LOV.
Definition at line 503 of file ics_errors.h.
#define ICS_err_no_partfile_on_item_revision (EMH_ICS_error_base + 609) |
The item revision does not contain a part file.
Definition at line 369 of file ics_errors.h.
#define ICS_err_no_tcbin (EMH_ICS_error_base + 571) |
The $TC_BIN directory was not found.
Definition at line 255 of file ics_errors.h.
#define ICS_err_no_template_of_this_name (EMH_ICS_error_base + 561) |
There is no template of this name.
Definition at line 225 of file ics_errors.h.
#define ICS_err_no_ugmaster_dataset (EMH_ICS_error_base + 563) |
No UG dataset is attached.
Definition at line 231 of file ics_errors.h.
#define ICS_err_no_view_for_template (EMH_ICS_error_base + 565) |
There is no view for the part family template.
Definition at line 237 of file ics_errors.h.
#define ICS_err_not_a_subclass (EMH_ICS_error_base + 689) |
1$s does not specify a Classification subclass ID.
Definition at line 608 of file ics_errors.h.
#define ICS_err_not_a_template_view (EMH_ICS_error_base + 632) |
The given tag does not belong to a part family template view.
Definition at line 438 of file ics_errors.h.
#define ICS_err_not_a_view (EMH_ICS_error_base + 683) |
The id given does not specify a view.
Definition at line 590 of file ics_errors.h.
#define ICS_err_not_all_icos_could_be_moved (EMH_ICS_error_base + 690) |
Not all ICOs could be moved from class 1$s to class 1$s.
Definition at line 611 of file ics_errors.h.
#define ICS_err_null_ico_in_constructor (EMH_ICS_error_base + 610) |
Null object in constructor.
Definition at line 372 of file ics_errors.h.
#define ICS_err_object_could_not_be_moved (EMH_ICS_error_base + 693) |
The class/view 1$s could not be moved.
Definition at line 620 of file ics_errors.h.
#define ICS_err_object_is_remote (EMH_ICS_error_base + 548) |
The object is remote.
Definition at line 186 of file ics_errors.h.
#define ICS_err_object_not_unique (EMH_ICS_error_base + 585) |
The object is not unique.
Definition at line 297 of file ics_errors.h.
#define ICS_err_object_referenced (EMH_ICS_error_base + 530) |
The Object is referenced
Definition at line 132 of file ics_errors.h.
#define ICS_err_only_write_part_file_or_jt_in_remote_template (EMH_ICS_error_base + 646) |
The template being used is a remote object. You cannot update the member data in the spreadsheet but only create/update the part file or jt file.
Definition at line 479 of file ics_errors.h.
#define ICS_err_out_of_tls_indexes (EMH_ICS_error_base + 599) |
There are no more indices.
Definition at line 339 of file ics_errors.h.
#define ICS_err_parent_does_not_exist (EMH_ICS_error_base + 401) |
The parent does not exist.
Definition at line 31 of file ics_errors.h.
#define ICS_err_parent_is_descendant (EMH_ICS_error_base + 674) |
The class specified to be the new parent is a descendant of the class to copy.
Definition at line 563 of file ics_errors.h.
#define ICS_err_parent_is_not_shared (EMH_ICS_error_base + 636) |
The class can't be shared, because the parent class isn't shared.
Definition at line 450 of file ics_errors.h.
#define ICS_err_parent_not_in_list (EMH_ICS_error_base + 673) |
In the copy operation a class in the hierarchy was specified to be copied without specifying its parent, too.
Definition at line 560 of file ics_errors.h.
#define ICS_err_plmxml (EMH_ICS_error_base + 645) |
PLMXML Module reported error: 1$s
Definition at line 476 of file ics_errors.h.
#define ICS_err_property_readonly (EMH_ICS_error_base + 584) |
The property is read-only.
Definition at line 294 of file ics_errors.h.
#define ICS_err_requested_pft_cannot_be_used (EMH_ICS_error_base + 575) |
The part family template cannot be used.
Definition at line 267 of file ics_errors.h.
#define ICS_err_rev_of_item_already_used_as_template (EMH_ICS_error_base + 615) |
Revision of Item is already used as part family template.
Definition at line 387 of file ics_errors.h.
#define ICS_err_set_attr_mapping_value (EMH_ICS_error_base + 651) |
Error setting attribute mapping value.
Definition at line 494 of file ics_errors.h.
#define ICS_err_share (EMH_ICS_error_base + 687) |
Error during the share operation.
Definition at line 602 of file ics_errors.h.
#define ICS_err_share_hierarchy_failed (EMH_ICS_error_base + 549) |
Error during hierarchy sharing
Definition at line 189 of file ics_errors.h.
#define ICS_err_share_views_of_class (EMH_ICS_error_base + 685) |
An error occurred during the share of the class' views.
Definition at line 596 of file ics_errors.h.
#define ICS_err_some_hierarchy_shares_failed (EMH_ICS_error_base + 551) |
Some objects in the hierarchy could not be shared.
Definition at line 195 of file ics_errors.h.
#define ICS_err_string_not_found (EMH_ICS_error_base + 658) |
Could not find the given string.
Definition at line 515 of file ics_errors.h.
#define ICS_err_subclass_could_not_be_converted (EMH_ICS_error_base + 680) |
The subclass could not be converted.
Definition at line 581 of file ics_errors.h.
#define ICS_err_target_unit_not_integer (EMH_ICS_error_base + 403) |
Value in target unit is not an Integer
Definition at line 37 of file ics_errors.h.
#define ICS_err_template_belongs_to_other_class_or_subclass (EMH_ICS_error_base + 603) |
The template belongs to a different class.
Definition at line 351 of file ics_errors.h.
#define ICS_err_template_is_already_attached (EMH_ICS_error_base + 604) |
The template is already attached to a different class.
Definition at line 354 of file ics_errors.h.
#define ICS_err_timeout (EMH_ICS_error_base + 598) |
Timeout.
Definition at line 336 of file ics_errors.h.
#define ICS_err_to_much_attribute_values (EMH_ICS_error_base + 663) |
To much values for given attribute.
Definition at line 530 of file ics_errors.h.
#define ICS_err_try_to_classify_wrong_wso_for_pft (EMH_ICS_error_base + 635) |
You can only classify the part family member part file item revision with the part family member ICO.
Definition at line 447 of file ics_errors.h.
#define ICS_err_try_to_get_mapping_without_storage (EMH_ICS_error_base + 623) |
Internal error: try to get a storage mapping with a NULLTAG storage.
Definition at line 411 of file ics_errors.h.
#define ICS_err_unexpected_error (EMH_ICS_error_base + 998) |
Unexpected error.
Definition at line 896 of file ics_errors.h.
#define ICS_err_unit_conversion (EMH_ICS_error_base + 404) |
An error has occurred during value conversion, because the conversion from the unit "%1$" to the unit "%2$" is impossible since they are not of the same measurement type.
Definition at line 41 of file ics_errors.h.
#define ICS_err_unknown_error (EMH_ICS_error_base + 579) |
Unknown error.
Definition at line 279 of file ics_errors.h.
#define ICS_err_unknown_graphicsbuilder_name (EMH_ICS_error_base + 576) |
Unknown graphics builder name.
Definition at line 270 of file ics_errors.h.
#define ICS_err_unknown_site (EMH_ICS_error_base + 686) |
The site specified is unknown.
Definition at line 599 of file ics_errors.h.
#define ICS_err_unreadable_children (EMH_ICS_error_base + 666) |
The class has unreadable children.
Definition at line 539 of file ics_errors.h.
#define ICS_err_view_does_not_exist (EMH_ICS_error_base + 529) |
The View does not exist
Definition at line 129 of file ics_errors.h.
#define ICS_err_view_id_not_unique (EMH_ICS_error_base + 664) |
The id given to create a new view specifies an existing view.
Definition at line 533 of file ics_errors.h.
#define ICS_err_wrong_store_object_tag (EMH_ICS_error_base + 624) |
Internal error: try to get a storage mapping with a wrong storage tag.
Definition at line 414 of file ics_errors.h.
#define ICS_err_wso_creation_checkfile_invalid (EMH_ICS_error_base + 638) |
Either the number check file 1$ does not exist or it has no read access.
Definition at line 460 of file ics_errors.h.
#define ICS_err_wso_creation_counter_error (EMH_ICS_error_base + 643) |
The counter 1$ has reached its limit and cannot count up.
Definition at line 470 of file ics_errors.h.
#define ICS_err_wso_creation_counter_greater_maxval (EMH_ICS_error_base + 642) |
The counter 1$ has reached its maximum value.
Definition at line 468 of file ics_errors.h.
#define ICS_err_wso_creation_failed (EMH_ICS_error_base + 644) |
A workspace object of Item/ItemRevision could not be created.
Definition at line 472 of file ics_errors.h.
#define ICS_err_wso_creation_id_exists (EMH_ICS_error_base + 640) |
The generated Item ID 1$ already exists in the check file.
Definition at line 464 of file ics_errors.h.
#define ICS_err_wso_creation_prefs_invalid (EMH_ICS_error_base + 637) |
The value for at least one of the ICS_PREFERENCE preferences is invalid.
Definition at line 458 of file ics_errors.h.
#define ICS_err_wso_creation_prefs_missing (EMH_ICS_error_base + 639) |
The preference 1$ is not set.
Definition at line 462 of file ics_errors.h.
#define ICS_err_wso_creation_seedpart_invalid (EMH_ICS_error_base + 641) |
Either the seed part does not exist or it has no read access.
Definition at line 466 of file ics_errors.h.
#define ICS_error_attr_value_greater_than_max (EMH_ICS_error_base + 854) |
Definition at line 848 of file ics_errors.h.
#define ICS_error_attr_value_lesser_than_min (EMH_ICS_error_base + 853) |
The value entered is not in min max range.
Definition at line 846 of file ics_errors.h.
#define ICS_error_keylov_entry_not_valid (EMH_ICS_error_base + 852) |
The Key LOV entry is not valid.
Definition at line 842 of file ics_errors.h.
#define ICS_error_keylov_value_unknown (EMH_ICS_error_base + 851) |
The Key LOV value is unknown.
Definition at line 838 of file ics_errors.h.
#define ICS_find_relation_failed (EMH_ICS_error_base + 501) |
Unable to find the relation
Definition at line 45 of file ics_errors.h.
#define ICS_GB_activation_failed (EMH_ICS_error_base + 760) |
Graphics builder activation failed.
Definition at line 784 of file ics_errors.h.
#define ICS_GB_already_initialized (EMH_ICS_error_base + 753) |
The graphics builder is already initialized.
Definition at line 763 of file ics_errors.h.
#define ICS_GB_exception (EMH_ICS_error_base + 750) |
Graphics builder exception
Definition at line 754 of file ics_errors.h.
#define ICS_GB_file_operation (EMH_ICS_error_base + 755) |
Graphics builder file exception
Definition at line 769 of file ics_errors.h.
#define ICS_GB_general (EMH_ICS_error_base + 756) |
General graphics builder error
Definition at line 772 of file ics_errors.h.
#define ICS_GB_internal (EMH_ICS_error_base + 757) |
Internal graphics builder error
Definition at line 775 of file ics_errors.h.
#define ICS_GB_mode (EMH_ICS_error_base + 759) |
Graphics builder mode error
Definition at line 781 of file ics_errors.h.
#define ICS_GB_parameter (EMH_ICS_error_base + 758) |
Graphics builder parameter error
Definition at line 778 of file ics_errors.h.
#define ICS_GB_system_exception (EMH_ICS_error_base + 751) |
Graphics builder system exception
Definition at line 757 of file ics_errors.h.
#define ICS_GB_unknown (EMH_ICS_error_base + 754) |
Unknown graphics builder error
Definition at line 766 of file ics_errors.h.
#define ICS_GB_user_exception (EMH_ICS_error_base + 752) |
Graphics builder user exception
Definition at line 760 of file ics_errors.h.
#define ICS_has_class_children (EMH_ICS_error_base + 668) |
The class has children that are classes.
Definition at line 545 of file ics_errors.h.
#define ICS_has_part_family_templates (EMH_ICS_error_base + 670) |
There are part family templates in the hierarchy.
Definition at line 551 of file ics_errors.h.
#define ICS_ico_already_classifying (EMH_ICS_error_base + 531) |
The Classification Object already classifies another Workspace Object
Definition at line 135 of file ics_errors.h.
#define ICS_ico_does_not_exist (EMH_ICS_error_base + 520) |
Classification Object does not exist
Definition at line 102 of file ics_errors.h.
#define ICS_ico_exists (EMH_ICS_error_base + 864) |
Localized property cannot be set on class attribute which has ICO'S
Definition at line 883 of file ics_errors.h.
#define ICS_ico_no_longer_pft_member (EMH_ICS_error_base + 691) |
Ico 1$s is no longer a part family member of template 1$s.
Definition at line 614 of file ics_errors.h.
#define ICS_insufficient_transfer_access (EMH_ICS_error_base + 866) |
Definition at line 890 of file ics_errors.h.
#define ICS_invalid_attribute (EMH_ICS_error_base + 519) |
Invalid attribute name
Definition at line 99 of file ics_errors.h.
#define ICS_invalid_attribute_id (EMH_ICS_error_base + 517) |
Invalid UNCT
Definition at line 93 of file ics_errors.h.
#define ICS_invalid_char_in_attribute (EMH_ICS_error_base + 542) |
Invalid Character in the specification for attribute value
Definition at line 168 of file ics_errors.h.
#define ICS_invalid_class (EMH_ICS_error_base + 513) |
Invalid Class
Definition at line 81 of file ics_errors.h.
#define ICS_invalid_class_id (EMH_ICS_error_base + 515) |
Invalid Class Id
Definition at line 87 of file ics_errors.h.
#define ICS_invalid_classification_property_name (EMH_ICS_error_base + 855) |
The invalid classification attribute property name.
Definition at line 852 of file ics_errors.h.
#define ICS_invalid_config_field_string (EMH_ICS_error_base + 523) |
Invalid Config Field String
Definition at line 111 of file ics_errors.h.
#define ICS_invalid_format (EMH_ICS_error_base + 518) |
Invalid Format
Definition at line 96 of file ics_errors.h.
#define ICS_invalid_group (EMH_ICS_error_base + 512) |
Invalid Group
Definition at line 78 of file ics_errors.h.
#define ICS_invalid_ico (EMH_ICS_error_base + 509) |
Invalid Classification Object
Definition at line 69 of file ics_errors.h.
#define ICS_invalid_keylov_value (EMH_ICS_error_base + 543) |
Invalid value for Key-LOV attribute
Definition at line 171 of file ics_errors.h.
#define ICS_invalid_read_operation (EMH_ICS_error_base + 532) |
Internal error: invalid read operation
Definition at line 138 of file ics_errors.h.
#define ICS_invalid_tag (EMH_ICS_error_base + 507) |
Invalid ICO
Definition at line 63 of file ics_errors.h.
#define ICS_invalid_view (EMH_ICS_error_base + 514) |
Invalid View
Definition at line 84 of file ics_errors.h.
#define ICS_invalid_view_id (EMH_ICS_error_base + 516) |
Invalid View Id
Definition at line 90 of file ics_errors.h.
#define ICS_invalid_wso (EMH_ICS_error_base + 506) |
Invalid Workspace Object
Definition at line 60 of file ics_errors.h.
#define ICS_mismatch_in_id (EMH_ICS_error_base + 522) |
Workspace Object Id and Classification Object Id do not match
Definition at line 108 of file ics_errors.h.
#define ICS_new_class_has_different_attribute_properties (EMH_ICS_error_base + 682) |
Attribute "%3$s" of the new class "%2$s" is inherited and differs in its properties from the source in "%1$s".
Definition at line 587 of file ics_errors.h.
#define ICS_no_tc_property_for_runtime_attr (EMH_ICS_error_base + 659) |
Could not get TC property for Classification runtime attribute.
Definition at line 518 of file ics_errors.h.
#define ICS_no_tc_property_for_runtime_ico (EMH_ICS_error_base + 544) |
Can not find the corresponding Teamcenter Engineering property for the runtimeIco
Definition at line 174 of file ics_errors.h.
#define ICS_note_attr_mapping (EMH_ICS_error_base + 662) |
Problem during Classification attribute mapping: s
Definition at line 527 of file ics_errors.h.
#define ICS_note_copy_or_conversion (EMH_ICS_error_base + 677) |
Problem during the copy/migrate operation: 1$s
Definition at line 572 of file ics_errors.h.
#define ICS_object_could_not_be_copied (EMH_ICS_error_base + 676) |
The object "%1$s" could not be copied.
Definition at line 569 of file ics_errors.h.
#define ICS_relation_type_does_not_exist (EMH_ICS_error_base + 505) |
Relation Type specified does not exist
Definition at line 57 of file ics_errors.h.
#define ICS_save_all_hierarchy_shares_failed (EMH_ICS_error_base + 552) |
Object was properly saved, but no hierarchy object could be shared.
Definition at line 198 of file ics_errors.h.
#define ICS_save_some_hierarchy_shares_failed (EMH_ICS_error_base + 550) |
Object was properly saved, but some objects in the hierarchy could not be shared.
Definition at line 192 of file ics_errors.h.
#define ICS_shared_objects (EMH_ICS_error_base + 669) |
There are shared objects in the hierarchy.
Definition at line 548 of file ics_errors.h.
#define ICS_SYNC_class_not_shared (EMH_ICS_error_base + 540) |
The class is not shared
Definition at line 162 of file ics_errors.h.
#define ICS_SYNC_copy_not_read_only (EMH_ICS_error_base + 537) |
Object is not read-only
Definition at line 153 of file ics_errors.h.
#define ICS_SYNC_group_not_shared (EMH_ICS_error_base + 547) |
The group is not shared.
Definition at line 183 of file ics_errors.h.
#define ICS_SYNC_ico_not_shared (EMH_ICS_error_base + 539) |
The ICO is not shared
Definition at line 159 of file ics_errors.h.
#define ICS_SYNC_missing_tag (EMH_ICS_error_base + 558) |
A tag is missing.
Definition at line 216 of file ics_errors.h.
#define ICS_SYNC_modify_date_not_set (EMH_ICS_error_base + 538) |
Modify date not set
Definition at line 156 of file ics_errors.h.
#define ICS_SYNC_more_than_one_target_site (EMH_ICS_error_base + 555) |
More than one target site given.
Definition at line 207 of file ics_errors.h.
#define ICS_SYNC_no_target_site (EMH_ICS_error_base + 554) |
No target site given.
Definition at line 204 of file ics_errors.h.
#define ICS_SYNC_not_a_header_class (EMH_ICS_error_base + 559) |
The object does not belong to class or subclass.
Definition at line 219 of file ics_errors.h.
#define ICS_SYNC_not_a_sync_class (EMH_ICS_error_base + 536) |
Object does not belong to a synchronizable class
Definition at line 150 of file ics_errors.h.
#define ICS_SYNC_object_does_not_exist (EMH_ICS_error_base + 560) |
The object does not exist.
Definition at line 222 of file ics_errors.h.
#define ICS_SYNC_object_is_local (EMH_ICS_error_base + 535) |
Object is owned by local site
Definition at line 147 of file ics_errors.h.
#define ICS_SYNC_object_is_remote (EMH_ICS_error_base + 534) |
Object is not owned by local site
Definition at line 144 of file ics_errors.h.
#define ICS_SYNC_object_not_shared (EMH_ICS_error_base + 557) |
The object must not be shared.
Definition at line 213 of file ics_errors.h.
#define ICS_SYNC_transferred_but_not_loaded (EMH_ICS_error_base + 533) |
Ownership of object was transferred but it could not be loaded
Definition at line 141 of file ics_errors.h.
#define ICS_SYNC_view_not_shared (EMH_ICS_error_base + 541) |
The view is not shared
Definition at line 165 of file ics_errors.h.
#define ICS_view_could_not_be_copied (EMH_ICS_error_base + 675) |
The view could not be copied.
Definition at line 566 of file ics_errors.h.
#define ICS_wso_already_classified (EMH_ICS_error_base + 502) |
Workspace Object already Classified
Definition at line 48 of file ics_errors.h.
#define ICS_wso_does_not_exist (EMH_ICS_error_base + 521) |
Workspace Object does not exist
Definition at line 105 of file ics_errors.h.
#define ICS_wso_not_classified (EMH_ICS_error_base + 504) |
Workspace object not Classified
Definition at line 54 of file ics_errors.h.
#define ICSX_ExpFailed (EMH_ICS_error_base + 726) |
Export Failed
Definition at line 727 of file ics_errors.h.
#define ICSX_ExpNoObject (EMH_ICS_error_base + 719) |
No object found to Export
Definition at line 706 of file ics_errors.h.
#define ICSX_ExpObject (EMH_ICS_error_base + 721) |
Exporting object 1$s 2$s.
Definition at line 712 of file ics_errors.h.
#define ICSX_ExportedObject (EMH_ICS_error_base + 724) |
Exported the Object Data Successfully
Definition at line 721 of file ics_errors.h.
#define ICSX_HookCancelAll (EMH_ICS_error_base + 729) |
Discontinued : Hook Function returns Cancel-All
Definition at line 736 of file ics_errors.h.
#define ICSX_HookCancelObj (EMH_ICS_error_base + 728) |
Ignored : Hook Function returns Cancel-Object
Definition at line 733 of file ics_errors.h.
#define ICSX_IgnObjTypeFiltOut (EMH_ICS_error_base + 727) |
Ignored : Filtered Out Object Type 1$s
Definition at line 730 of file ics_errors.h.
#define ICSX_IgnUpdate (EMH_ICS_error_base + 710) |
1$s 2$s already exists. Use the update option to overwrite.
Definition at line 679 of file ics_errors.h.
#define ICSX_ImpFailed (EMH_ICS_error_base + 725) |
Import Failed
Definition at line 724 of file ics_errors.h.
#define ICSX_ImpNewObject (EMH_ICS_error_base + 722) |
Import Created the object Successfully
Definition at line 715 of file ics_errors.h.
#define ICSX_ImpObject (EMH_ICS_error_base + 720) |
Importing object 1$s 2$s.
Definition at line 709 of file ics_errors.h.
#define ICSX_ImpUpdObject (EMH_ICS_error_base + 723) |
Import Updated the object Successfully
Definition at line 718 of file ics_errors.h.
#define ICSX_InvInput (EMH_ICS_error_base + 730) |
Invalid - Exporting this sub-set is not Supported
Definition at line 739 of file ics_errors.h.
#define ICSX_InvObjXmlElement (EMH_ICS_error_base + 706) |
Invalid XML Element
Definition at line 667 of file ics_errors.h.
#define ICSX_NoXmlData (EMH_ICS_error_base + 708) |
No Data for Xml Element
Definition at line 673 of file ics_errors.h.
#define ICSX_ParserInit (EMH_ICS_error_base + 701) |
Unable to Initialize Xml4c Parser Module
Definition at line 652 of file ics_errors.h.
#define ICSX_UnbCreateElement (EMH_ICS_error_base + 707) |
Unable to create Xml Element
Definition at line 670 of file ics_errors.h.
#define ICSX_UnbGenXmlDoc (EMH_ICS_error_base + 705) |
Unable to generate Xml Doc
Definition at line 664 of file ics_errors.h.
#define ICSX_UnbGetDocRoot (EMH_ICS_error_base + 703) |
Unable to get valid Root Element by Parsing
Definition at line 658 of file ics_errors.h.
#define ICSX_UnbGetObj (EMH_ICS_error_base + 717) |
Unable to get ICS object
Definition at line 700 of file ics_errors.h.
#define ICSX_UnbGetProp (EMH_ICS_error_base + 713) |
Unable to Get Property
Definition at line 688 of file ics_errors.h.
#define ICSX_UnbGetXmlData (EMH_ICS_error_base + 709) |
Unable to get the required Data from Xml Doc
Definition at line 676 of file ics_errors.h.
#define ICSX_UnbNewObj (EMH_ICS_error_base + 712) |
Unable to Create Object
Definition at line 685 of file ics_errors.h.
#define ICSX_UnbOpenObj (EMH_ICS_error_base + 711) |
Unable to Open existing object
Definition at line 682 of file ics_errors.h.
#define ICSX_UnbSaveObj (EMH_ICS_error_base + 716) |
Unable to Save Object 1$s.
Definition at line 697 of file ics_errors.h.
#define ICSX_UnbSetObj (EMH_ICS_error_base + 718) |
Unable to set ICS object
Definition at line 703 of file ics_errors.h.
#define ICSX_UnbSetProp (EMH_ICS_error_base + 714) |
Unable to Set Property
Definition at line 691 of file ics_errors.h.
#define ICSX_UnbUpdProp (EMH_ICS_error_base + 715) |
Unable to Set Properties 1$s.
Definition at line 694 of file ics_errors.h.
#define ICSX_XmlDataStorage (EMH_ICS_error_base + 704) |
Error traversing Xml Data objects
Definition at line 661 of file ics_errors.h.
#define ICSX_XmlParser (EMH_ICS_error_base + 700) |
Xml4c Error
Definition at line 649 of file ics_errors.h.
#define ICSX_XmlParsing (EMH_ICS_error_base + 702) |
Xml4c Parsing Error: 1$s.
Definition at line 655 of file ics_errors.h.