#define IDENTIFIER_delete_last_suppl (EMH_IDENTIFIER_error_base + 17) |
Definition at line 39 of file idfr_errors.h.
#define IDENTIFIER_duplicate_dispdefault (EMH_IDENTIFIER_error_base + 12) |
Definition at line 34 of file idfr_errors.h.
#define IDENTIFIER_duplicate_id (EMH_IDENTIFIER_error_base + 20) |
Definition at line 42 of file idfr_errors.h.
#define IDENTIFIER_idcontext_notfound (EMH_IDENTIFIER_error_base + 24) |
Definition at line 46 of file idfr_errors.h.
#define IDENTIFIER_idfbl_noaccess (EMH_IDENTIFIER_error_base + 13) |
Definition at line 35 of file idfr_errors.h.
#define IDENTIFIER_idfbl_not_modifiable (EMH_IDENTIFIER_error_base + 14) |
Definition at line 36 of file idfr_errors.h.
#define IDENTIFIER_initialization_error (EMH_IDENTIFIER_error_base + 1) |
Definition at line 23 of file idfr_errors.h.
#define IDENTIFIER_invalid_cardinality (EMH_IDENTIFIER_error_base + 26) |
Definition at line 48 of file idfr_errors.h.
#define IDENTIFIER_invalid_class (EMH_IDENTIFIER_error_base + 25) |
Definition at line 47 of file idfr_errors.h.
#define IDENTIFIER_invalid_combination (EMH_IDENTIFIER_error_base + 21) |
Definition at line 43 of file idfr_errors.h.
#define IDENTIFIER_invalid_id (EMH_IDENTIFIER_error_base + 7) |
Definition at line 29 of file idfr_errors.h.
#define IDENTIFIER_invalid_idcontext (EMH_IDENTIFIER_error_base + 9) |
Definition at line 31 of file idfr_errors.h.
#define IDENTIFIER_invalid_idfbl_tag (EMH_IDENTIFIER_error_base + 11) |
Definition at line 33 of file idfr_errors.h.
#define IDENTIFIER_invalid_supplcontext (EMH_IDENTIFIER_error_base + 19) |
Definition at line 41 of file idfr_errors.h.
#define IDENTIFIER_invalid_tag (EMH_IDENTIFIER_error_base + 3) |
Definition at line 25 of file idfr_errors.h.
#define IDENTIFIER_invalid_uid_tag (EMH_IDENTIFIER_error_base + 27) |
Definition at line 49 of file idfr_errors.h.
#define IDENTIFIER_master_nosuppl (EMH_IDENTIFIER_error_base + 16) |
Definition at line 38 of file idfr_errors.h.
#define IDENTIFIER_missing_exportinfo (EMH_IDENTIFIER_error_base + 23) |
Definition at line 45 of file idfr_errors.h.
#define IDENTIFIER_no_autogen_id (EMH_IDENTIFIER_error_base + 22) |
Definition at line 44 of file idfr_errors.h.
#define IDENTIFIER_null_id (EMH_IDENTIFIER_error_base + 6) |
Definition at line 28 of file idfr_errors.h.
#define IDENTIFIER_null_idcontext (EMH_IDENTIFIER_error_base + 8) |
Definition at line 30 of file idfr_errors.h.
#define IDENTIFIER_property_protected (EMH_IDENTIFIER_error_base + 10) |
Definition at line 32 of file idfr_errors.h.
#define IDENTIFIER_relation_not_found (EMH_IDENTIFIER_error_base + 2) |
Definition at line 24 of file idfr_errors.h.
#define IDENTIFIER_save_suppl_id (EMH_IDENTIFIER_error_base + 15) |
Definition at line 37 of file idfr_errors.h.
#define IDENTIFIER_suppl_noaccess (EMH_IDENTIFIER_error_base + 18) |
Definition at line 40 of file idfr_errors.h.
#define IDENTIFIER_type_not_found (EMH_IDENTIFIER_error_base + 4) |
Definition at line 26 of file idfr_errors.h.
#define IDENTIFIER_unable_to_create (EMH_IDENTIFIER_error_base + 5) |
Definition at line 27 of file idfr_errors.h.