#define LOV_already_attached (EMH_LOV_error_base + 10) |
Definition at line 29 of file lov_errors.h.
#define LOV_attach_error (EMH_LOV_error_base + 11) |
Definition at line 30 of file lov_errors.h.
#define LOV_cant_get_displayable_string (EMH_LOV_error_base + 21) |
Definition at line 40 of file lov_errors.h.
#define LOV_cant_get_length_of_values (EMH_LOV_error_base + 22) |
Definition at line 41 of file lov_errors.h.
#define LOV_cant_get_values (EMH_LOV_error_base + 23) |
Definition at line 42 of file lov_errors.h.
#define LOV_circular_filter (EMH_LOV_error_base + 32) |
Definition at line 51 of file lov_errors.h.
#define LOV_default_lov_not_found (EMH_LOV_error_base + 46) |
Definition at line 71 of file lov_errors.h.
#define LOV_detach_error (EMH_LOV_error_base + 12) |
Definition at line 31 of file lov_errors.h.
#define LOV_entry_not_found (EMH_LOV_error_base + 37) |
Definition at line 62 of file lov_errors.h.
#define LOV_entry_referenced (EMH_LOV_error_base + 36) |
Definition at line 61 of file lov_errors.h.
#define LOV_having_corrupted_data (EMH_LOV_error_base + 24) |
Definition at line 43 of file lov_errors.h.
#define LOV_having_duplicate_values (EMH_LOV_error_base + 34) |
Definition at line 53 of file lov_errors.h.
#define LOV_having_multiple_condition (EMH_LOV_error_base + 35) |
Definition at line 54 of file lov_errors.h.
#define LOV_having_multiple_entries (EMH_LOV_error_base + 39) |
Definition at line 64 of file lov_errors.h.
#define LOV_having_multiple_lov (EMH_LOV_error_base + 16) |
Definition at line 35 of file lov_errors.h.
#define LOV_inconsistent_filter_definition (EMH_LOV_error_base + 27) |
Definition at line 46 of file lov_errors.h.
#define LOV_inconsistent_tag (EMH_LOV_error_base + 19) |
Definition at line 38 of file lov_errors.h.
#define LOV_inconsistent_value (EMH_LOV_error_base + 7) |
Definition at line 26 of file lov_errors.h.
#define LOV_inconsistent_value_descs (EMH_LOV_error_base + 30) |
Definition at line 49 of file lov_errors.h.
#define LOV_inconsistent_value_index (EMH_LOV_error_base + 28) |
Definition at line 47 of file lov_errors.h.
#define LOV_incorrect_lov_value_property (EMH_LOV_error_base + 57) |
The dynamic LOV "%1$" has an invalid configuration: the LOV value property "%2$" does not exist. Please contact your business modeler administrator about this issue.
Definition at line 99 of file lov_errors.h.
#define LOV_incostistant_lovdps (EMH_LOV_error_base + 42) |
Definition at line 67 of file lov_errors.h.
#define LOV_insert_msg_not_supported (EMH_LOV_error_base + 25) |
Definition at line 44 of file lov_errors.h.
#define LOV_invalid_argument (EMH_LOV_error_base + 15) |
Definition at line 34 of file lov_errors.h.
#define LOV_invalid_filter (EMH_LOV_error_base + 31) |
Definition at line 50 of file lov_errors.h.
#define LOV_invalid_lov_name (EMH_LOV_error_base + 4) |
Definition at line 23 of file lov_errors.h.
#define LOV_invalid_reference (EMH_LOV_error_base + 18) |
Definition at line 37 of file lov_errors.h.
#define LOV_invalid_search_value (EMH_LOV_error_base + 33) |
Definition at line 52 of file lov_errors.h.
#define LOV_invalid_sort_order (EMH_LOV_error_base + 51) |
The specified LOV sort order "%1$" is invalid. A valid sort order is either 1 (for ascending) or 2 (for descending).
Definition at line 89 of file lov_errors.h.
#define LOV_invalid_sort_property_name (EMH_LOV_error_base + 52) |
The property "%1$" is not a valid sort property. The property must be one of the following: "%2$".
Definition at line 91 of file lov_errors.h.
#define LOV_invalid_type (EMH_LOV_error_base + 13) |
Definition at line 32 of file lov_errors.h.
#define LOV_invalid_usage (EMH_LOV_error_base + 6) |
Definition at line 25 of file lov_errors.h.
#define LOV_invalid_value_description (EMH_LOV_error_base + 50) |
The LOV value description "%1$" is not a string type property.
Definition at line 87 of file lov_errors.h.
#define LOV_invalid_value_type (EMH_LOV_error_base + 5) |
Definition at line 24 of file lov_errors.h.
#define LOV_is_not_localized (EMH_LOV_error_base + 44) |
Definition at line 69 of file lov_errors.h.
#define LOV_is_referenced (EMH_LOV_error_base + 38) |
Definition at line 63 of file lov_errors.h.
#define LOV_lovdp_attr_not_found (EMH_LOV_error_base + 47) |
Definition at line 72 of file lov_errors.h.
#define LOV_lovdp_not_found (EMH_LOV_error_base + 41) |
Definition at line 66 of file lov_errors.h.
#define LOV_need_master_display_to_set (EMH_LOV_error_base + 40) |
Definition at line 65 of file lov_errors.h.
#define LOV_no_attachments (EMH_LOV_error_base + 43) |
Definition at line 68 of file lov_errors.h.
#define LOV_no_create (EMH_LOV_error_base + 8) |
Definition at line 27 of file lov_errors.h.
#define LOV_no_create_enquiry (EMH_LOV_error_base + 9) |
Definition at line 28 of file lov_errors.h.
#define LOV_no_load_class (EMH_LOV_error_base + 2) |
Definition at line 21 of file lov_errors.h.
#define LOV_no_load_lov (EMH_LOV_error_base + 3) |
Definition at line 22 of file lov_errors.h.
#define LOV_no_memory (EMH_LOV_error_base + 20) |
Definition at line 39 of file lov_errors.h.
#define LOV_no_right_to_do (EMH_LOV_error_base + 14) |
Definition at line 33 of file lov_errors.h.
#define LOV_not_initialized (EMH_LOV_error_base + 1) |
Definition at line 20 of file lov_errors.h.
#define LOV_not_registed_for_lookup (EMH_LOV_error_base + 45) |
Definition at line 70 of file lov_errors.h.
#define LOV_not_registered_reference (EMH_LOV_error_base + 17) |
Definition at line 36 of file lov_errors.h.
#define LOV_operation_not_supported (EMH_LOV_error_base + 29) |
Definition at line 48 of file lov_errors.h.
#define LOV_prop_sorting_not_supported (EMH_LOV_error_base + 58) |
Sorting is not supported for column quot;1$quot;, because it represents an array property.
Definition at line 101 of file lov_errors.h.
#define LOV_select_value_for_property (EMH_LOV_error_base + 53) |
Select a value for the property "%1$".
Definition at line 93 of file lov_errors.h.
#define LOV_selected_value_not_valid (EMH_LOV_error_base + 55) |
The value "%1$" is not a valid value for the property "%2$" of type "%3$".
Definition at line 95 of file lov_errors.h.
#define LOV_selected_value_not_valid_in_range (EMH_LOV_error_base + 56) |
The value "%1$" is not in the range "%2$".
Definition at line 97 of file lov_errors.h.
#define LOV_set_msg_not_supported (EMH_LOV_error_base + 26) |
Definition at line 45 of file lov_errors.h.
#define LOV_value_auto_populated_for_property (EMH_LOV_error_base + 63) |
This field is automatically populated when selecting a value for the "%1$" property.
Definition at line 111 of file lov_errors.h.
#define LOV_values_for_type_only_valid_in_range (EMH_LOV_error_base + 61) |
Valid values are of type "%1$" within a range of "%2$" to "%3$".
Definition at line 107 of file lov_errors.h.
#define LOV_values_not_available (EMH_LOV_error_base + 59) |
No value is available for the LOV. Please enter a value.
Definition at line 103 of file lov_errors.h.
#define LOV_values_not_available_call_admin (EMH_LOV_error_base + 60) |
No values are available for the LOV with the internal name "%1$". Please contact your system administrator.
Definition at line 105 of file lov_errors.h.
#define LOV_values_not_available_for_input (EMH_LOV_error_base + 62) |
No LOV value matches the input text "%1$".
Definition at line 109 of file lov_errors.h.
#define LOVValueDesc_display_value_for_non_existent_value (EMH_LOV_error_base + 49) |
Definition at line 79 of file lov_errors.h.