#define NR_autogen_not_set (NR_ERROR_BASE + 18) |
Definition at line 51 of file nr_errors.h.
#define NR_cannot_set_autogen (NR_ERROR_BASE + 20) |
Definition at line 53 of file nr_errors.h.
#define NR_duplicate_attach (NR_ERROR_BASE + 4) |
Definition at line 37 of file nr_errors.h.
#define NR_duplicate_pattern (NR_ERROR_BASE + 19) |
Definition at line 52 of file nr_errors.h.
#define NR_duplicate_rule (NR_ERROR_BASE + 3) |
Definition at line 36 of file nr_errors.h.
#define NR_ERROR_BASE EMH_NR_error_base |
Definition at line 32 of file nr_errors.h.
#define NR_excluded_letters (NR_ERROR_BASE + 28) |
Definition at line 61 of file nr_errors.h.
#define NR_initialize_failed (NR_ERROR_BASE + 1) |
Definition at line 34 of file nr_errors.h.
#define NR_invalid_case (NR_ERROR_BASE + 2) |
Definition at line 35 of file nr_errors.h.
#define NR_invalid_esc (NR_ERROR_BASE + 10) |
Definition at line 43 of file nr_errors.h.
#define NR_invalid_init_or_max_value (NR_ERROR_BASE + 24) |
Definition at line 57 of file nr_errors.h.
#define NR_invalid_pattern (NR_ERROR_BASE + 15) |
Definition at line 48 of file nr_errors.h.
#define NR_invalid_prop_for_rev_nr (NR_ERROR_BASE + 31) |
The Revision Naming Rule information cannot be obtained for the property "%1$". Revision Naming Rules can only be configured on the "item_revision_id" property.
Definition at line 70 of file nr_errors.h.
#define NR_invalid_rule_suffix (NR_ERROR_BASE + 30) |
The value "%1$" is not a valid rule suffix. It must be "PDR".
Definition at line 65 of file nr_errors.h.
#define NR_invalid_sysvar (NR_ERROR_BASE + 9) |
Definition at line 42 of file nr_errors.h.
#define NR_invalid_vartype (NR_ERROR_BASE + 14) |
Definition at line 47 of file nr_errors.h.
#define NR_key_info (NR_ERROR_BASE + 25) |
Definition at line 58 of file nr_errors.h.
#define NR_max_counter_value (NR_ERROR_BASE + 16) |
Definition at line 49 of file nr_errors.h.
#define NR_max_nesting (NR_ERROR_BASE + 22) |
Definition at line 55 of file nr_errors.h.
#define NR_missing_delimiter (NR_ERROR_BASE + 11) |
Definition at line 44 of file nr_errors.h.
#define NR_missing_rule (NR_ERROR_BASE + 5) |
Definition at line 38 of file nr_errors.h.
#define NR_missing_variable (NR_ERROR_BASE + 12) |
Definition at line 45 of file nr_errors.h.
#define NR_never_matched (NR_ERROR_BASE + 7) |
Definition at line 40 of file nr_errors.h.
#define NR_no_autogen (NR_ERROR_BASE + 29) |
Definition at line 62 of file nr_errors.h.
#define NR_no_counters_found (NR_ERROR_BASE + 17) |
Definition at line 50 of file nr_errors.h.
#define NR_not_matched (NR_ERROR_BASE + 6) |
Definition at line 39 of file nr_errors.h.
#define NR_not_string_var (NR_ERROR_BASE + 13) |
Definition at line 46 of file nr_errors.h.
#define NR_not_valid_pattern_for_autogen (NR_ERROR_BASE + 21) |
Definition at line 54 of file nr_errors.h.
#define NR_out_of_range (NR_ERROR_BASE + 26) |
Definition at line 59 of file nr_errors.h.
#define NR_rev_exausted (NR_ERROR_BASE + 27) |
Definition at line 60 of file nr_errors.h.
#define NR_rule_name_referenced (NR_ERROR_BASE + 23) |
Definition at line 56 of file nr_errors.h.
#define NR_undefined_prop (NR_ERROR_BASE + 8) |
Definition at line 41 of file nr_errors.h.