AE_API logical HOOKUP_can_auto_login | ( | void | ) |
AE_API int HOOKUP_create_nxprocessdata | ( | void | ) |
AE_API void HOOKUP_display_error | ( | int | ) |
AE_API int HOOKUP_is_apiserver_reusable | ( | void | ) |
AE_API void HOOKUP_kill_apiserver | ( | int | ) |
AE_API int HOOKUP_print | ( | tag_t | ) |
AE_API int HOOKUP_print_using | ( | tag_t | ) |
AE_API int HOOKUP_reset_export_dir | ( | void | ) |
AE_API int HOOKUP_set_base_dir_name | ( | const char * | ) |
AE_API int HOOKUP_set_dir_name | ( | int * | , | |
char * | ||||
) |
AE_API int HOOKUP_start_apiserver | ( | int | ) |
AE_API int NXMsgHandler_init_module | ( | void | ) |
AE_API int NXPV_batch_tessellation | ( | int | , | |
tag_t * | ||||
) |
AE_API int NXPV_tessellation | ( | tag_t | rev | ) |
AE_API int NXSM_create_nx_image | ( | tag_t * | , | |
int | ||||
) |
This function allows two dimensional images of Unigraphics parts to be generated from Teamcenter. These images are intended to be viewed on Web Access pages. The generated images will be stored as Named References to the UGMASTER dataset. Preferences for types and sizes of images desired can be modified in .tc_env.
AE_API int NXSM_create_nxpart | ( | tag_t | dataset | ) |
AE_API void NXSM_get_nx_switch | ( | char * | data | ) |