#define PROP_bad_date_range (EMH_PROP_error_base + 63) |
Definition at line 90 of file prop_errors.h.
#define PROP_bad_object_hierarchy (EMH_PROP_error_base + 114) |
Definition at line 115 of file prop_errors.h.
#define PROP_cannot_traverse_object_hierarchy (EMH_PROP_error_base + 115) |
Definition at line 116 of file prop_errors.h.
#define PROP_cant_alloc_space (EMH_PROP_error_base + 47) |
Definition at line 73 of file prop_errors.h.
#define PROP_cant_modify_saved (EMH_PROP_error_base + 64) |
Definition at line 91 of file prop_errors.h.
#define PROP_compound_prop_is_not_allowed_as_source (EMH_PROP_error_base + 118) |
Definition at line 119 of file prop_errors.h.
#define PROP_cpdef_instance_not_found (EMH_PROP_error_base + 111) |
Definition at line 112 of file prop_errors.h.
#define PROP_display_name_error (EMH_PROP_error_base + 215) |
Definition at line 141 of file prop_errors.h.
#define PROP_duplicate_rule (EMH_PROP_error_base + 200) |
Definition at line 126 of file prop_errors.h.
#define PROP_edit_delete_propagated_is_not_allowed (EMH_PROP_error_base + 72) |
Definition at line 96 of file prop_errors.h.
#define PROP_error_autogenerate (EMH_PROP_error_base + 502) |
An error has occurred while generating the value for the following properties: 1$. Please provide valid combination of input values.
Definition at line 185 of file prop_errors.h.
#define PROP_exceeds_array_limit (EMH_PROP_error_base + 71) |
Definition at line 95 of file prop_errors.h.
#define PROP_fail_to_define_operation_input_property (EMH_PROP_error_base + 212) |
Definition at line 138 of file prop_errors.h.
#define PROP_fail_to_define_relation_property (EMH_PROP_error_base + 213) |
Definition at line 139 of file prop_errors.h.
#define PROP_fail_to_define_runtime_property (EMH_PROP_error_base + 211) |
Definition at line 137 of file prop_errors.h.
#define PROP_failed_get_value (EMH_PROP_error_base + 43) |
Definition at line 69 of file prop_errors.h.
#define PROP_failed_to_create_cpdesc (EMH_PROP_error_base + 110) |
Definition at line 111 of file prop_errors.h.
#define PROP_id_name_exceeds_allowed_length (EMH_PROP_error_base + 208) |
Definition at line 134 of file prop_errors.h.
#define PROP_incomplete_date (EMH_PROP_error_base + 58) |
Definition at line 85 of file prop_errors.h.
#define PROP_initialize_failed (EMH_PROP_error_base + 201) |
Definition at line 127 of file prop_errors.h.
#define PROP_input_data_not_well_organized (EMH_PROP_error_base + 305) |
Definition at line 153 of file prop_errors.h.
#define PROP_integer_out_of_range (EMH_PROP_error_base + 65) |
Definition at line 92 of file prop_errors.h.
#define PROP_invalid_attr (EMH_PROP_error_base + 42) |
Definition at line 68 of file prop_errors.h.
#define PROP_invalid_complex_prop_token (EMH_PROP_error_base + 204) |
Definition at line 130 of file prop_errors.h.
#define PROP_invalid_complex_property (EMH_PROP_error_base + 206) |
Definition at line 132 of file prop_errors.h.
#define PROP_invalid_date (EMH_PROP_error_base + 57) |
Definition at line 84 of file prop_errors.h.
#define PROP_invalid_date_format (EMH_PROP_error_base + 51) |
Definition at line 78 of file prop_errors.h.
#define PROP_invalid_day (EMH_PROP_error_base + 50) |
Definition at line 77 of file prop_errors.h.
#define PROP_invalid_descriptor (EMH_PROP_error_base + 40) |
Definition at line 66 of file prop_errors.h.
#define PROP_invalid_display_name_token (EMH_PROP_error_base + 214) |
Definition at line 140 of file prop_errors.h.
#define PROP_invalid_hour (EMH_PROP_error_base + 52) |
Definition at line 79 of file prop_errors.h.
#define PROP_invalid_index (EMH_PROP_error_base + 70) |
Definition at line 94 of file prop_errors.h.
#define PROP_invalid_init_value (EMH_PROP_error_base + 205) |
Definition at line 131 of file prop_errors.h.
#define PROP_invalid_minute (EMH_PROP_error_base + 54) |
Definition at line 81 of file prop_errors.h.
#define PROP_invalid_month (EMH_PROP_error_base + 53) |
Definition at line 80 of file prop_errors.h.
#define PROP_invalid_name (EMH_PROP_error_base + 20) |
Definition at line 52 of file prop_errors.h.
#define PROP_invalid_object (EMH_PROP_error_base + 41) |
Definition at line 67 of file prop_errors.h.
#define PROP_invalid_object_type (EMH_PROP_error_base + 22) |
Definition at line 54 of file prop_errors.h.
#define PROP_invalid_operation_input_field_type (EMH_PROP_error_base + 210) |
Definition at line 136 of file prop_errors.h.
#define PROP_invalid_operation_input_source (EMH_PROP_error_base + 209) |
Definition at line 135 of file prop_errors.h.
#define PROP_invalid_prop_name (EMH_PROP_error_base + 116) |
Definition at line 117 of file prop_errors.h.
#define PROP_invalid_prop_type (EMH_PROP_error_base + 27) |
Definition at line 62 of file prop_errors.h.
#define PROP_invalid_reference (EMH_PROP_error_base + 100) |
The type of the input object does not match the type expected by the given property.
Definition at line 101 of file prop_errors.h.
#define PROP_invalid_relation_type (EMH_PROP_error_base + 23) |
Definition at line 55 of file prop_errors.h.
#define PROP_invalid_second (EMH_PROP_error_base + 55) |
Definition at line 82 of file prop_errors.h.
#define PROP_invalid_value (EMH_PROP_error_base + 59) |
Definition at line 86 of file prop_errors.h.
#define PROP_invalid_value_type (EMH_PROP_error_base + 29) |
Definition at line 64 of file prop_errors.h.
#define PROP_invalid_year (EMH_PROP_error_base + 56) |
Definition at line 83 of file prop_errors.h.
#define PROP_is_marked_localizable (EMH_PROP_error_base + 311) |
Definition at line 159 of file prop_errors.h.
#define PROP_is_required_err (EMH_PROP_error_base + 203) |
Definition at line 129 of file prop_errors.h.
#define PROP_locale_not_supported (EMH_PROP_error_base + 302) |
Definition at line 150 of file prop_errors.h.
#define PROP_multivalued (EMH_PROP_error_base + 45) |
Definition at line 71 of file prop_errors.h.
#define PROP_no_attr_defn (EMH_PROP_error_base + 21) |
Definition at line 53 of file prop_errors.h.
#define PROP_no_display (EMH_PROP_error_base + 14) |
Definition at line 49 of file prop_errors.h.
#define PROP_no_locale_value_specified (EMH_PROP_error_base + 309) |
Definition at line 157 of file prop_errors.h.
#define PROP_no_master_locale (EMH_PROP_error_base + 308) |
Definition at line 156 of file prop_errors.h.
#define PROP_no_properties (EMH_PROP_error_base + 13) |
Definition at line 48 of file prop_errors.h.
#define PROP_no_status_value_specified (EMH_PROP_error_base + 310) |
Definition at line 158 of file prop_errors.h.
#define PROP_not_a_char (EMH_PROP_error_base + 6) |
Definition at line 41 of file prop_errors.h.
#define PROP_not_a_conjunction (EMH_PROP_error_base + 11) |
Definition at line 46 of file prop_errors.h.
#define PROP_not_a_date (EMH_PROP_error_base + 7) |
Definition at line 42 of file prop_errors.h.
#define PROP_not_a_double (EMH_PROP_error_base + 8) |
Definition at line 43 of file prop_errors.h.
#define PROP_not_a_logical (EMH_PROP_error_base + 10) |
Definition at line 45 of file prop_errors.h.
#define PROP_not_a_tag (EMH_PROP_error_base + 62) |
Definition at line 89 of file prop_errors.h.
#define PROP_not_an_integer (EMH_PROP_error_base + 9) |
Definition at line 44 of file prop_errors.h.
#define PROP_not_an_operator (EMH_PROP_error_base + 12) |
Definition at line 47 of file prop_errors.h.
#define PROP_not_autoassignable (EMH_PROP_error_base + 500) |
The value for the property "%1$" cannot be autogenerated, because neither Naming Rules nor User Exits are configured on this property.
Definition at line 178 of file prop_errors.h.
#define PROP_not_created (EMH_PROP_error_base + 49) |
Definition at line 75 of file prop_errors.h.
#define PROP_not_found (EMH_PROP_error_base + 15) |
Definition at line 50 of file prop_errors.h.
#define PROP_not_implemented (EMH_PROP_error_base + 99) |
Definition at line 98 of file prop_errors.h.
#define PROP_not_marked_localizable (EMH_PROP_error_base + 300) |
Definition at line 148 of file prop_errors.h.
#define PROP_not_modifiable (EMH_PROP_error_base + 60) |
Definition at line 87 of file prop_errors.h.
#define PROP_null_input_not_allowed (EMH_PROP_error_base + 101) |
An invalid object reference was passed to the property operation. Please refer to the Teamcenter syslog file for more information, and report this error to your system administrator.
Definition at line 105 of file prop_errors.h.
#define PROP_null_inputs_not_allowed (EMH_PROP_error_base + 117) |
Definition at line 118 of file prop_errors.h.
#define PROP_null_value (EMH_PROP_error_base + 44) |
Definition at line 70 of file prop_errors.h.
#define PROP_objects_in_different_types (EMH_PROP_error_base + 306) |
Definition at line 154 of file prop_errors.h.
#define PROP_PVM_value_excluded (EMH_PROP_error_base + 400) |
Definition at line 167 of file prop_errors.h.
#define PROP_register_failed (EMH_PROP_error_base + 24) |
Definition at line 56 of file prop_errors.h.
#define PROP_required_prop_not_set (EMH_PROP_error_base + 207) |
Definition at line 133 of file prop_errors.h.
#define PROP_singular (EMH_PROP_error_base + 46) |
Definition at line 72 of file prop_errors.h.
#define PROP_source_object_missing (EMH_PROP_error_base + 501) |
The value for the property "%1$" cannot be autogenerated during revise/save as action, because the revised or saved object is missing.
Definition at line 181 of file prop_errors.h.
#define PROP_translations_out_of_index (EMH_PROP_error_base + 303) |
Definition at line 151 of file prop_errors.h.
#define PROP_type_already_set (EMH_PROP_error_base + 26) |
Definition at line 61 of file prop_errors.h.
#define PROP_unable_to_get_cp_value (EMH_PROP_error_base + 113) |
Definition at line 114 of file prop_errors.h.
#define PROP_unable_to_set_cp_value (EMH_PROP_error_base + 112) |
Definition at line 113 of file prop_errors.h.
#define PROP_use_date_format (EMH_PROP_error_base + 61) |
Definition at line 88 of file prop_errors.h.
#define PROP_value_not_set (EMH_PROP_error_base + 48) |
Definition at line 74 of file prop_errors.h.
#define PROP_value_type_already_set (EMH_PROP_error_base + 28) |
Definition at line 63 of file prop_errors.h.
#define PROP_VLA_adapter_error (EMH_PROP_error_base + 301) |
Definition at line 149 of file prop_errors.h.
#define PROP_write_once_err (EMH_PROP_error_base + 202) |
Definition at line 128 of file prop_errors.h.
#define PROP_wrong_number_of_values (EMH_PROP_error_base + 307) |
Definition at line 155 of file prop_errors.h.
#define PROP_zero_objects_props_locales (EMH_PROP_error_base + 304) |
Definition at line 152 of file prop_errors.h.