#define TCEVENTMGR_name_size_c 32 |
Definition at line 28 of file tceventmgr.h.
SUB_MGR_API int TCEVENTMGR_post_assign_status_event | ( | tag_t | object, | |
const char * | release_status_type_name | |||
) |
This function is used for posting an Assign Status event.
Restrictions:
The routine is used only for posting Assign Status event.
object | (I) Tag of the object that the release status is assigned to |
release_status_type_name | (I) Name of the release status type |
SUB_MGR_API int TCEVENTMGR_post_attach_event | ( | tag_t | relation | ) |
This function is used for posting an Attach event.
Restrictions:
This routine is used only for posting Attach event.
relation | (I) Tag of the relation instance that is being created, and the secondary object of the relation is being attached to the primary object of the relation. |
SUB_MGR_API int TCEVENTMGR_post_event | ( | tag_t | objectType, | |
const char | eventTypeName[TCEVENTMGR_name_size_c+1] | |||
) |
objectType | (I) |
eventTypeName | (I) |
SUB_MGR_API int TCEVENTMGR_post_event2 | ( | tag_t | primaryObject, | |
tag_t | secondaryObject, | |||
const char | eventTypeName[TCEVENTMGR_name_size_c+1], | |||
int | attrCount, | |||
const char ** | attrNames, | |||
const char ** | attrValues, | |||
int | errorCode, | |||
const char * | errorMsg | |||
) |
primaryObject | (I) |
secondaryObject | (I) |
eventTypeName | (I) |
attrCount | (I) |
attrNames | (I) |
attrValues | (I) |
errorCode | (I) |
errorMsg | (I) |
SUB_MGR_API int TCEVENTMGR_post_event2_2 | ( | tag_t | primaryObject, | |
tag_t | secondaryObject, | |||
const char * | eventTypeName, | |||
int | attrCount, | |||
const char ** | attrNames, | |||
const char ** | attrValues, | |||
int | errorCode, | |||
const char * | errorMsg | |||
) |
post an event
primaryObject | (I) |
secondaryObject | (I) |
eventTypeName | (I) |
attrCount | (I) |
attrNames | (I) |
attrValues | (I) |
errorCode | (I) |
errorMsg | (I) |
SUB_MGR_API int TCEVENTMGR_post_event_2 | ( | tag_t | objectType, | |
const char * | eventTypeName | |||
) |
post an event
objectType | (I) |
eventTypeName | (I) |