#define TYPE_cannot_delete_system_rule (EMH_TYPE_error_base + 20) |
Definition at line 54 of file tctype_errors.h.
#define TYPE_class_already_exists (EMH_TYPE_error_base + 9) |
Definition at line 34 of file tctype_errors.h.
#define TYPE_class_names_not_same ( EMH_TYPE_error_base + 26) |
Definition at line 60 of file tctype_errors.h.
#define TYPE_cpdef_results_duplicate_prop (EMH_TYPE_error_base + 17) |
Definition at line 49 of file tctype_errors.h.
#define TYPE_duplicate_prop_name (EMH_TYPE_error_base + 15) |
Definition at line 42 of file tctype_errors.h.
#define TYPE_failed_to_create_cpdefinition (EMH_TYPE_error_base + 18) |
Definition at line 50 of file tctype_errors.h.
#define TYPE_instances_exist (EMH_TYPE_error_base + 16) |
Definition at line 43 of file tctype_errors.h.
#define TYPE_invalid_accessor (EMH_TYPE_error_base + 19) |
Definition at line 53 of file tctype_errors.h.
#define TYPE_invalid_class (EMH_TYPE_error_base + 5) |
Definition at line 30 of file tctype_errors.h.
#define TYPE_invalid_class_name (EMH_TYPE_error_base + 6) |
Definition at line 31 of file tctype_errors.h.
#define TYPE_invalid_context_name ( EMH_TYPE_error_base + 31 ) |
The requested context is not supported. The supported context names are: "subtypes".
Definition at line 70 of file tctype_errors.h.
#define TYPE_invalid_Preference (EMH_TYPE_error_base + 23) |
Definition at line 57 of file tctype_errors.h.
#define TYPE_invalid_props (EMH_TYPE_error_base + 24) |
Definition at line 58 of file tctype_errors.h.
#define TYPE_invalid_type_name (EMH_TYPE_error_base + 7) |
Definition at line 32 of file tctype_errors.h.
#define TYPE_msg_not_supported (EMH_TYPE_error_base + 25) |
Definition at line 59 of file tctype_errors.h.
#define TYPE_no_create_enquiry (EMH_TYPE_error_base + 13) |
Definition at line 40 of file tctype_errors.h.
#define TYPE_no_create_type (EMH_TYPE_error_base + 22) |
Definition at line 56 of file tctype_errors.h.
#define TYPE_no_expandable_paste_relations_found ( EMH_TYPE_error_base + 29) |
No expandable paste relations were found for the type "%1$". Please contact your system administrator.
Definition at line 65 of file tctype_errors.h.
#define TYPE_no_extent (EMH_TYPE_error_base + 12) |
Definition at line 39 of file tctype_errors.h.
#define TYPE_no_find_type (EMH_TYPE_error_base + 21) |
Definition at line 55 of file tctype_errors.h.
#define TYPE_no_load_class (EMH_TYPE_error_base + 2) |
Definition at line 27 of file tctype_errors.h.
#define TYPE_no_load_type (EMH_TYPE_error_base + 4) |
Definition at line 29 of file tctype_errors.h.
#define TYPE_no_paste_relations_found ( EMH_TYPE_error_base + 28) |
No paste relations were found for the type "%1$". Please contact your system administrator.
Definition at line 63 of file tctype_errors.h.
#define TYPE_no_preferred_paste_relations_found ( EMH_TYPE_error_base + 30) |
No preferred paste relations were found for the type "%1$". Please contact your system administrator.
Definition at line 67 of file tctype_errors.h.
#define TYPE_no_register_object (EMH_TYPE_error_base + 3) |
Definition at line 28 of file tctype_errors.h.
#define TYPE_not_initialized (EMH_TYPE_error_base + 1) |
Definition at line 26 of file tctype_errors.h.
#define TYPE_primary_type_not_allowed ( EMH_TYPE_error_base + 27) |
Definition at line 61 of file tctype_errors.h.
#define TYPE_privileged_operation (EMH_TYPE_error_base + 11) |
Definition at line 38 of file tctype_errors.h.
#define TYPE_type_already_exists (EMH_TYPE_error_base + 8) |
Definition at line 33 of file tctype_errors.h.
#define TYPE_unknown_type (EMH_TYPE_error_base + 14) |
Definition at line 41 of file tctype_errors.h.