#define TRANSACTIONPROCESSING_can_not_approve_a_child (TRANSACTIONPROCESSING_error_base + 3) |
Can not APPROVE a child object directly. Please approve the parent.
Definition at line 41 of file transactionprocessing_errors.h.
#define TRANSACTIONPROCESSING_can_not_approve_object_that_is_already_approved (TRANSACTIONPROCESSING_error_base + 2) |
Can not APPROVE an object that is already approved.
Definition at line 35 of file transactionprocessing_errors.h.
#define TRANSACTIONPROCESSING_duplicate_transactionid (TRANSACTIONPROCESSING_error_base + 5) |
Can not create this object because the transaction id is not unique.
Definition at line 53 of file transactionprocessing_errors.h.
#define TRANSACTIONPROCESSING_error_base EMH_TRANSACTIONPROCESSING_error_base |
Definition at line 23 of file transactionprocessing_errors.h.
#define TRANSACTIONPROCESSING_finding_classid_of_transaction_element_class (TRANSACTIONPROCESSING_error_base + 1) |
Error trying to find the class id of Transaction Element class.
Definition at line 29 of file transactionprocessing_errors.h.
#define TRANSACTIONPROCESSING_object_is_remote (TRANSACTIONPROCESSING_error_base + 4) |
Can not APPROVE a remote object.
Definition at line 47 of file transactionprocessing_errors.h.
#define TRANSACTIONPROCESSING_user_missing_author_license (TRANSACTIONPROCESSING_error_base + 6) |
The user does not have an Author License to perform this action.
Definition at line 59 of file transactionprocessing_errors.h.