tc/iman.h File Reference
Detailed Description
- Deprecated:
- This function is deprecated and will be removed from Teamcenter 2009.
- Deprecated:
- Do not use this header file anymore. Include tc.h.
- Deprecated:
- Use the following replacement chart for every symbol, type or API:
Old | New |
IMAN_ask_memory_in_use | TC_ask_memory_in_use |
IMAN_ask_memory_statistics | TC_ask_memory_statistics |
IMAN_dump_objects | TC_dump_objects |
IMAN_report_serious_error | TC_report_serious_error |
IMAN_write_syslog | TC_write_syslog |
Definition in file iman.h.
#include <fclasses/iman_basic.h>
#include <tc/tc_startup.h>
Go to the source code of this file.
Defines
Define Documentation
#define IMAN_ask_memory_in_use TC_ask_memory_in_use |
#define IMAN_ask_memory_statistics TC_ask_memory_statistics |
#define IMAN_dump_objects TC_dump_objects |
#define IMAN_report_serious_error TC_report_serious_error |
#define IMAN_write_syslog TC_write_syslog |