Definition in file rdv_errors.h.
#include <common/emh_const.h>
#include <rdv/iman_rdv_errors.h>
Go to the source code of this file.
#define RDV_auditlines_notfound (EMH_RDV_error_base + 100) |
Definition at line 96 of file rdv_errors.h.
#define RDV_balancing_mismatch (EMH_RDV_error_base + 207) |
Definition at line 121 of file rdv_errors.h.
#define RDV_bracket_mismatch (EMH_RDV_error_base + 205) |
Definition at line 119 of file rdv_errors.h.
#define RDV_cannot_create_apr (EMH_RDV_error_base + 91) |
Definition at line 91 of file rdv_errors.h.
#define RDV_cannot_create_topline_absoccdata_object (EMH_RDV_error_base + 110) |
Definition at line 108 of file rdv_errors.h.
#define RDV_cannot_find_ABE (EMH_RDV_error_base + 218) |
Definition at line 133 of file rdv_errors.h.
#define RDV_cannot_find_Architecture (EMH_RDV_error_base + 213) |
Definition at line 127 of file rdv_errors.h.
#define RDV_cannot_modify_nve (EMH_RDV_error_base + 212) |
Definition at line 126 of file rdv_errors.h.
#define RDV_cannot_open_file (EMH_RDV_error_base + 101) |
Definition at line 97 of file rdv_errors.h.
#define RDV_cannot_save_sco_without_ownership (EMH_RDV_error_base + 217) |
Definition at line 132 of file rdv_errors.h.
#define RDV_cannot_save_sco_without_topline_ownership (EMH_RDV_error_base + 223) |
The Structure Context Object (SCO) cannot be saved with Absolute Path Nodes (APN), because the ownership of a top line (Product Item) is not transferred from the owning site. Please set the value of preference "RDV_CREATE_SCO_WITHOUT_APN" to "true" in order to create the SCO on the replicated product.
Definition at line 143 of file rdv_errors.h.
#define RDV_failed_to_lock (EMH_RDV_error_base + 109) |
Definition at line 107 of file rdv_errors.h.
#define RDV_garbage_at_end (EMH_RDV_error_base + 102) |
Definition at line 98 of file rdv_errors.h.
#define RDV_import_permission_issue (EMH_RDV_error_base + 221) |
The logged-in user does not have permission to import the object "%1$".
Definition at line 139 of file rdv_errors.h.
#define RDV_invalid_input (EMH_RDV_error_base + 215) |
Definition at line 130 of file rdv_errors.h.
#define RDV_invalid_meta_expr (EMH_RDV_error_base + 209) |
Definition at line 123 of file rdv_errors.h.
#define RDV_invalid_nve_reference (EMH_RDV_error_base + 204) |
Definition at line 118 of file rdv_errors.h.
#define RDV_invalid_object (EMH_RDV_error_base + 222) |
The validation for the object "%1$" has failed because of data corruption. Please contact your system administrator.
Definition at line 141 of file rdv_errors.h.
#define RDV_invalid_sco_tag (EMH_RDV_error_base + 92) |
Definition at line 92 of file rdv_errors.h.
#define RDV_invalid_TC_max_number_of_retries (EMH_RDV_error_base + 108) |
Definition at line 106 of file rdv_errors.h.
#define RDV_invalid_tc_plmxml_sync_dataset_preference (EMH_RDV_error_base + 216) |
Definition at line 131 of file rdv_errors.h.
#define RDV_invalid_TC_retry_time (EMH_RDV_error_base + 107) |
Definition at line 105 of file rdv_errors.h.
#define RDV_invalid_view_type (EMH_RDV_error_base + 111) |
Definition at line 111 of file rdv_errors.h.
#define RDV_meta_expr_always_false (EMH_RDV_error_base + 211) |
Definition at line 125 of file rdv_errors.h.
#define RDV_meta_expr_always_true (EMH_RDV_error_base + 210) |
Definition at line 124 of file rdv_errors.h.
#define RDV_meta_expr_syntax_error (EMH_RDV_error_base + 208) |
Definition at line 122 of file rdv_errors.h.
#define RDV_no_revision_rule (EMH_RDV_error_base + 93) |
Definition at line 93 of file rdv_errors.h.
#define RDV_null_nve_tag (EMH_RDV_error_base + 200) |
Definition at line 114 of file rdv_errors.h.
#define RDV_nve_ref_expected (EMH_RDV_error_base + 206) |
Definition at line 120 of file rdv_errors.h.
#define RDV_nve_remotely_owned (EMH_RDV_error_base + 90) |
Definition at line 90 of file rdv_errors.h.
#define RDV_plmxml_export_error (EMH_RDV_error_base + 219) |
The object "%1$" could not be exported to PLMXML because its data is corrupted. Please contact your system administrator.
Definition at line 135 of file rdv_errors.h.
#define RDV_plmxml_import_error (EMH_RDV_error_base + 220) |
The element "%1$" could not be imported from PLMXML, because its data is corrupted. Please check the plmxml file and contact your system administrator.
Definition at line 137 of file rdv_errors.h.
#define RDV_preference_has_no_value (EMH_RDV_error_base + 70) |
Definition at line 89 of file rdv_errors.h.
#define RDV_special_chars_in_code (EMH_RDV_error_base + 214) |
Definition at line 128 of file rdv_errors.h.
#define RDV_token_is_not_nve (EMH_RDV_error_base + 202) |
Definition at line 116 of file rdv_errors.h.
#define RDV_token_is_out_of_range (EMH_RDV_error_base + 203) |
Definition at line 117 of file rdv_errors.h.
#define RDV_unconfig_plmxml_not_found_in_dataset (EMH_RDV_error_base + 105) |
Definition at line 101 of file rdv_errors.h.
#define RDV_variant_expr_is_not_meta_expr (EMH_RDV_error_base + 201) |
Definition at line 115 of file rdv_errors.h.
#define RDV_VAS_not_defined_global_option (EMH_RDV_error_base + 106) |
Definition at line 102 of file rdv_errors.h.