MROCORE_characteristics_data_s Struct Reference
[MRO Core]
#include <mrocore.h>
Detailed Description
This structure is used to pass on the parameters for Record utilization action.
Definition at line 118 of file mrocore.h.
Data Fields
Field Documentation
Tag of Characteristics Definition
Definition at line 120 of file mrocore.h.
Value for the Characteristic
Definition at line 121 of file mrocore.h.
Date Value for the Characteristic
Definition at line 122 of file mrocore.h.
The documentation for this struct was generated from the following file: