#include <validationrule.h>
Definition at line 261 of file validationrule.h.
Attribute class clause. For example: ITEMREVISION:owning_group
Definition at line 262 of file validationrule.h.
The application which rule apply to>
Definition at line 263 of file validationrule.h.
The condition which rule apply to>
Definition at line 264 of file validationrule.h.
TRUE: value list is exclusive. FALSE: value list is inclusive (default) When exclude == TRUE, no wildcard allowed in value list
Definition at line 265 of file validationrule.h.
List of event values (or attribute values if attribute class clause defined). "*" is translated as wildcard. Special characters such as "^" or "$" are not allowed.
Definition at line 267 of file validationrule.h.
The number of event values >
Definition at line 270 of file validationrule.h.