#include <workspaceobject.h>
If object type is ItemVersionFolder, the id attribute will be mapped to "id_string" field and the name attribute will be mapped to "object_name" field. For some other object types, the name attribute will be mapped to "id_string" field and the "object_name" field will be null.
Definition at line 205 of file workspaceobject.h.
char WSO_description_s::object_name[WSO_name_size_c+1] |
Definition at line 206 of file workspaceobject.h.
char WSO_description_s::object_type[WSO_name_size_c+1] |
Definition at line 207 of file workspaceobject.h.
char WSO_description_s::owners_name[WSO_name_size_c+1] |
Definition at line 209 of file workspaceobject.h.
char WSO_description_s::application[WSO_name_size_c+1] |
Definition at line 210 of file workspaceobject.h.
char WSO_description_s::date_created[WSO_date_size_c+1] |
Definition at line 212 of file workspaceobject.h.
char WSO_description_s::date_modified[WSO_date_size_c+1] |
Definition at line 213 of file workspaceobject.h.
char WSO_description_s::date_released[WSO_date_size_c+1] |
Definition at line 214 of file workspaceobject.h.
char WSO_description_s::released_for[WSO_release_status_size_c+1] |
Definition at line 215 of file workspaceobject.h.
char WSO_description_s::id_string[WSO_name_size_c+19] |
Definition at line 217 of file workspaceobject.h.
Dataset stuff
Definition at line 218 of file workspaceobject.h.
Dataset stuff
Definition at line 219 of file workspaceobject.h.
char WSO_description_s::owning_group_name[WSO_name_size_c+1] |
Definition at line 221 of file workspaceobject.h.
char WSO_description_s::last_modifying_user_name[WSO_name_size_c+1] |
Definition at line 222 of file workspaceobject.h.
char WSO_description_s::archive_date[WSO_date_size_c+1] |
Definition at line 223 of file workspaceobject.h.
char WSO_description_s::backup_date[WSO_date_size_c+1] |
Definition at line 224 of file workspaceobject.h.
char WSO_description_s::description[WSO_desc_size_c+1] |
Definition at line 225 of file workspaceobject.h.
Definition at line 226 of file workspaceobject.h.
Definition at line 227 of file workspaceobject.h.
char WSO_description_s::revision_id[WSO_name_size_c+1] |
Item revision
Definition at line 228 of file workspaceobject.h.
char WSO_description_s::owning_site_name[WSO_name_size_c+1] |
Definition at line 229 of file workspaceobject.h.