Solid Edge Assembly Type Library
CamFollowerRelation3d Object
Members 
Description
Defines a cam-follower relationship between two objects.
Object Model
CamFollowerRelation3d ObjectOccurrence ObjectAdjustablePart ObjectTube ObjectAdjustablePart ObjectSubassemblyBodies CollectionSubOccurrences CollectionAssemblyDocument ObjectOccurrence ObjectAdjustablePart ObjectTube ObjectAdjustablePart ObjectSubassemblyBodies CollectionSubOccurrences CollectionAssemblyDocument Object
Remarks
The CamFollowerRelation3d object applies a cam relationship between a closed loop of tangent faces on one part and a single follower face on another part. The follower face can be a plane, a cylinder, a sphere, or a point.
See Also

CamFollowerRelation3d Members

Send comments on this topic.