Solid Edge Assembly Type Library
Project Overview
Description
Solid Edge Assembly Type Library
Object Model
AssemblyDocument ObjectMeasureVariable ObjectApplication ObjectArcSegments CollectionAsmRefPlanes CollectionAssemblyBodies CollectionAssemblyCopies CollectionAssemblyDrivenPartFeatures ObjectAssemblyFamilyEvents ObjectAssemblyFamilyMembers CollectionAssemblyFeatures ObjectAssemblyGroups CollectionAssemblyMirrors ObjectAssemblyPatterns CollectionAssemblyProperties CollectionAssemblyRecomputeEvents ObjectAttributeQuery ObjectOccurrence ObjectComponentLayouts CollectionConfigurations CollectionConstructions CollectionCoordinateSystems CollectionCurveSegments CollectionDocumentEvents ObjectFastenerSystems CollectionHarnesses CollectionHighlightSets CollectionHoleDataCollection CollectionItemNumbers ObjectLabelWeldDataCollection CollectionLayers CollectionLayouts CollectionLineSegments CollectionOccurrences CollectionApplication ObjectPaths CollectionPhysicalProperties ObjectPipes CollectionQueries CollectionRelations3d CollectionSelectSet CollectionSectionViews CollectionSegmentRelations3d CollectionSegments CollectionSelectSet CollectionSensors CollectionSimplifiedAssemblies CollectionStructuralFrames CollectionStudyOwner CollectionUnitsOfMeasure CollectionVirtualComponentOccurrences CollectionWindows CollectionWirePaths CollectionWireRuns CollectionZones Collection
Classes
Class ModuleDescription
AdjustablePartAdjustable part object.
AFGrooveWeld
AFGrooveWelds
AngularRelation3dA 3-D relation object.
ArcSegmentRepresents an occurrence of an ArcSegment element in an Assembly document.
ArcSegmentsRepresents a collection of ArcSegment objects.
AsmRefPlaneA planar object that provides a flat surface on which to create a profile within profile-based features.
AsmRefPlanesA collection of Assembly RefPlane objects.
AssemblyBodies
AssemblyBody
AssemblyCopies
AssemblyCopy
AssemblyDocumentA document type used exclusively for assemblies.
AssemblyDrivenPartFeatures
AssemblyDrivenPartFeaturesExtrudedCutout
AssemblyDrivenPartFeaturesExtrudedCutouts
AssemblyDrivenPartFeaturesHole
AssemblyDrivenPartFeaturesHoles
AssemblyDrivenPartFeaturesRevolvedCutout
AssemblyDrivenPartFeaturesRevolvedCutouts
AssemblyFamilyMemberRepresents an occurrence of a member assembly in a family of assemblies.
AssemblyFamilyMembersRepresents a collection of AssemblyFamilyMember objects.
AssemblyFeatures
AssemblyFeaturesExtrudedCutout
AssemblyFeaturesExtrudedCutouts
AssemblyFeaturesExtrudedProtrusion
AssemblyFeaturesExtrudedProtrusions
AssemblyFeaturesHole
AssemblyFeaturesHoles
AssemblyFeaturesMirror
AssemblyFeaturesMirrors
AssemblyFeaturesPattern
AssemblyFeaturesPatterns
AssemblyFeaturesRevolvedCutout
AssemblyFeaturesRevolvedCutouts
AssemblyFeaturesRevolvedProtrusion
AssemblyFeaturesRevolvedProtrusions
AssemblyFeaturesSweptProtrusion
AssemblyFeaturesSweptProtrusions
AssemblyFilletWeld
AssemblyFilletWelds
AssemblyGroupThe AssemblyGroup object consists of methods that add components to or removes components from a group.
AssemblyGroupsThe AssemblyGroups object represents a collection of AssemblyGroup objects.
AssemblyMirror
AssemblyMirrors
AssemblyPatternRepresents an assembly pattern.
AssemblyPatternOccurrenceAn assembly pattern occurrence.
AssemblyPatternsRepresents a collection of AssemblyPattern objects.
AssemblyPropertiesCollection of AssemblyProperty objects.
AssemblyPropertyAllows creation and manipulation of wiring attributes.
AssemblyStitchWeld
AssemblyStitchWelds
AssemblyThread
AssemblyThreads
AxialRelation3dMakes the cylindrical axis of a feature on one part colinear with the cylindrical axis of a feature on another part.
Bundle
Bundles
Cable
Cables
CamFollowerRelation3dDefines a cam-follower relationship between two objects.
CenterPlaneRelation3dDefines a center-plane relationship between objects.
ComponentLayout
ComponentLayouts
ConfigurationA set of assembly configuration settings.
ConfigurationsRepresents a collection of Configuration objects.
CurveSegmentRepresents an occurrence of a curve segment element.
CurveSegmentsCollection of CurveSegment objects.
FastenerSystemRepresents Fastener System.
FastenerSystemsRepresents Fastener Systems.
GearRelation3dDefines a gear relationship between two objects.
GroundRelation3dDefines that a part remains fixed in its current position and orientation.
Harness
Harnesses
ItemNumbers
LayoutAn Assembly Layout object
LayoutsCollection of Assembly Layouts.
LineSegmentRepresents an occurrence of a LineSegment element in an Assembly document.
LineSegmentsRepresents a collection of LineSegment objects.
OccurrenceAn instance of an Occurrence or subassembly within an assembly.
OccurrencesA collection of occurrence objects.
PartAn instance of a part or subassembly within an assembly.
PartsA collection of Part objects.
PathRepresents an occurrence of a curve segment element.
PathRelation3dDefines a Path relationship between two objects.
PathsCollection of keypoint curve objects.
PhysicalPropertiesContains the results of physical property calculations on the referenced object.
Pipe
Pipes
PlanarRelation3dMakes the planar face of a feature on one part parallel with the planar face of a feature on another part.
PointRelation3dAn assembly 3-D point relation helper object.
QueriesRepresents a collection of Query objects.
QueryRepresents an instance of a Query on an associated AssemblyDocument object.
Relations3dA collection of relationships for parts and subassemblies that are contained in the referenced assembly.
RigidSetRelation3d
SegmentAngularRelation3dRepresents an occurrence of an Segment Angular constraint in an Assembly document.
SegmentDirectionRelation3dRepresents a relationship for which the specified relative orientations between constrained elements is maintained.
SegmentDistanceRelation3dRepresents a relationship for which the distance between constrained elements is maintained.
SegmentPointRelation3dRepresents a relationship for which the specified point relationship for a constrained element is maintained.
SegmentRadiusRelation3dRepresents a relationship for which a specified radius is maintained for a constrained element.
SegmentRelations3dRepresents a collection of all relationships applied to tubing segments within an AssemblyDocument object.
SegmentsRepresents a collection of all segment-based objects (ex. LineSegment, ArcSegment) for the associated Assembly document.
SegmentTangentRelation3dRepresents a relationship for which the specified tangency condition for constrained elements is maintained.
SimplifiedAssembliesSimplified Assemblies
SimplifiedAssemblySimplified Assembly
StructuralFrameThe StructuralFrame object represents a structural frame constructed along path segments in an assembly document.
StructuralFramesThe StructuralFrames object represents a collection of StructuralFrame objects.
SubassemblyBodies
SubassemblyBody
SubOccurrenceAn instance of an SubOccurrence or subassembly within an assembly.
SubOccurrencesA collection of sub occurrence objects.
TangentRelation3dDefines a tangent relationship between two objects.
TopologyReferenceRepresents an object that references a topological object (an edge or a face, for example).
TubeAn object that encapsulates all tube-related information (for example, Tube path, material, bend radii, and wall thickness) in the associated Occurrence object.
VirtualComponentA virtual component object.
VirtualComponentOccurrenceA virtual component occurrence object.
VirtualComponentOccurrencesA collection of VirtualComponentOccurrence objects.
Wire
WirePathAn occurrence of a wire path.
WirePathCableMembersRepresents a collection of cable member WirePath objects.
WirePathsA collection of WirePath objects.
WirePathSegmentsRepresents a collection of segment WirePath objects.
WireRunAn occurrence of a wire run.
WireRunPathsRepresents a collection of WireRun path objects.
WireRunsA collection of WireRun objects.
Wires
ZoneThe Zone object represents a zone in an assembly document.
ZonesThe Zones object returns a collection of all the zones defined for the assembly document.
Public Enumerations
EnumerationDescription
AssemblyBaseStylesConstantsAssembly Base Styles Constants
AssemblyCopyActionConstants
AssemblyCopyComponentConstants
AssemblyCopyStatusConstants
AssemblyCopyTypeConstants
AssemblyFamilyMemberPropertyConstantsAssembly Family Member Property Constants
AssemblyGlobalConstantsAssembly Global constants
AssemblyPathfinderUpdateConstantsAssembly Pathfinder Update Constants
AssemblyReportTypeConstantsAssembly Report Type Constants
AssemblyWireHarnessReportTypeConstantsAssembly Wire Harness Report Type Constants
ConfigurationTypeConstantsConfiguration Type Constants
ConstraintReplacementConstants
CurveSegmentPathAdditionStatusConstantsCurve Segment Path Addition Status Constants
CurveSegmentPathRemovalStatusConstantsCurve Segment Path Removal Status Constants
CurveSegmentValidationConstantsCurve Segment Validation Constants
CurveSegmentWhichKeypointsConstantsCurve Segment Which Keypoints Constants
HarnessSaveAsEcadStatusConstantsHarness Save As ECAD Status Constants
HarnessTypeConstantsHarness Type Constants
InterferenceStatusConstantsInterference Status constants
ItemNumberModeConstants
MoveMultipleMoveTypeConstantsMove Multiple Move Type Constants
MoveMultipleRelationshipConstantsMove Multiple Relationship Constants
OccurrenceStatusConstantsAssembly Occurrence Status Constants
PipeFittingEndTreatmentConstantsPipe Fitting End Treatment Constants
PipeFittingTypeConstantsPipe Fitting Type Constants
QueryConditionConstantsQuery Condition Constants
QueryPropertyConstantsQuery Property Constants
QueryScopeConstantsQuery Scope Constants
Relation3dDetailedStatusConstantsAssembly Relation3d Detailed Status Constants
Relation3dGearRatioTypeConstantsRelation3d Gear Ratio Type Constants
Relation3dGearTypeConstantsRelation3d Gear Type Constants
Relation3dGeometryConstantsAssembly Relation3d Geometry Constants
Relation3dOrientationConstantsRelation3d Orientation Constants
Relation3dStatusConstantsAssembly Relation3d Status Constants
seAssemblyBodyTypeConstantsAssembly Body Type Constants
SegmentRelation3dDirectionConstantsSegment Relation3d Direction Constants
SegmentRelation3dDistanceConstantsSegment Relation3d Distance Constants
SegmentRelation3dGeometryConstantsSegment Relation3d Geometry Constants
SegmentRelation3dStatusConstantsSegment Relation3d Status Constants
SimplifiedAssemblyModeDefines the whether the particular document has modeled or visible simplification
StructuralFrameEndConditionConstantsStructural Frame End Condition Constants
TubePropertyPidConstantsTube Property Pid Constants
TubeSegmentAdditionStatusConstantsTube Segment Addition Status Constants
TubeSegmentRemovalStatusConstantsTube Segment Removal Status Constants
UpdateStructureCacheConstantsUpdate Structure Cache Constants
VirtualComponentPublishConstantsVirtual Component Publish Constants
VirtualComponentStatusConstantsVirtual Component Status Constants
VirtualComponentTypeConstantsVirtual Component Type Constants
VisibilityBasedSimplifiedAssemblyCopyTypeDefines the whether faces or bodies are copied to the simplified assembly representation after visibility processing
WirePathConstantsWire Path Constants
Send comments on this topic.