Solid Edge Assembly Type Library
PhysicalProperties Object
Members 
Description
Contains the results of physical property calculations on the referenced object.
Remarks
It also provides properties to control the display of the physical properties symbol. Properties and methods of the PhysicalProperties object provide a way to determine if the assembly contains parts whose physical properties are current. This object also provides methods for updating the physical properties and returning the physical properties for a selection set. Through the PhysicalProperties object, you can also display or hide the graphics for center of mass, center of volume, and principal axes. The center of mass, center of volume, and orientation of the principal axes are all calculated with respect to the global origin. Mass moment of inertia and radii of gyration are calculated with respect to the principal axes.
See Also

PhysicalProperties Members

Send comments on this topic.