Solid Edge Framework Type Library
Application Object
Members 
Description
Provides the properties and methods necessary for a Visual Basic user to drive Solid Edge programmatically.
Object Model
Application ObjectSelectSet CollectionAddIns CollectionApplication ObjectSelectSet CollectionAddIns CollectionApplication ObjectApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectCommand ObjectCustomization ObjectDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSEECEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows CollectionApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectCommand ObjectMouse ObjectCommandWindow ObjectCustomization ObjectApplication ObjectApplication ObjectRadialMenu CollectionRibbonBarThemes CollectionSwitchWindowCust CollectionDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSelectSet CollectionAddIns CollectionApplication ObjectApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectCommand ObjectCustomization ObjectDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSEECEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows CollectionSEECEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows Collection
Remarks
All of the exposed objects for the application can be accessed once you have accessed the Application object. The Application object contains application-wide options and settings, including access to preference sets, version information, window states, status and toolbar controls, mail and routing slip access, and so forth. All top-level objects (ActiveDocument, ActiveEnvironment, and so forth) can be retrieved from the Application object.
Example
Imports SolidEdgeFramework
Imports System.Runtime.InteropServices

Module Example
    <STAThread()> _
    Sub Main()
        Dim objApplication As SolidEdgeFramework.Application = Nothing

        Try
            OleMessageFilter.Register()

            ' Connect to a running instance of Solid Edge.
            objApplication = Marshal.GetActiveObject("SolidEdge.Application")

        Catch ex As Exception
            ' Write any errors to console.
            Console.WriteLine(ex.Message)
        Finally
            OleMessageFilter.Revoke()
        End Try
    End Sub
End Module
See Also

Application Members

Send comments on this topic.