Solid Edge Framework Type Library
Project Overview
Description
Solid Edge Framework Type Library
Object Model
Application ObjectSelectSet CollectionAddIns CollectionApplication ObjectApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectCommand ObjectCustomization ObjectDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSEECEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows Collection
Classes
Class ModuleDescription
AcceleratorRepresents a collection of KeyBinding objects.
AcceleratorsRepresents a collection of Accelerator objects.
AddInA control that represents a command added to Solid Edge through the AddIn interface.
AddInEdgeBarEvents
AddInEventsA collection of AddInEvent objects.
AddInsA collection of AddIn objects.
ApplicationProvides the properties and methods necessary for a Visual Basic user to drive Solid Edge programmatically.
ApplicationEventsFires application events.
ApplicationV8DocumentOpenEventFires document open event
ApplicationWindowEventsProvides access to the application window events.
AssemblyFamilyEvents
AssemblyRecomputeEventsRepresents a collection of assembly recompute events.
AttributeRepresents an occurrence of a user-defined attribute.
AttributeQueryContains the QueryByName method, which enables you to locate attribute sets and individual attributes.
AttributeSetRepresents an occurrence of a user-defined attribute set.
AttributeSetsRepresents a collection of AttributeSet objects.
BlockTableEventsContains the AfterUpdate event.
CommandProvides interfaces for Visual Basic users to capture user input to process Solid Edge events.
CommandBarRepresents all menus, toolbars, and pop-up menus in Solid Edge.
CommandBarButtonRepresents buttons on toolbars and menus.
CommandBarButtonEventsA collection of CommandBarButtonEvent objects.
CommandBarControlContains the properties and methods that are applicable to both CommandBarButton and CommandBarPopup objects.
CommandBarControlsContains all of the buttons and pop-ups on a specific command bar.
CommandBarPopupRepresents pop-ups on toolbars and menus.
CommandBarsA collection of all of the command bars within a specific environment.
CommandCategoriesA collection of command categories
CommandCategory
CommandInfo
CommandWindowTriggers Command Window events.
ConnectorTableEventsContains the AfterUpdate event.
CPDInitializer
CPDInitializerInsightXT
CustomizationAn object that is sued to Customize the UI
DashStyleThe DashStyle object represents a custom dash style in a Draft document.
DashStylesThe DashStyles object represents a collection of DashStyle objects.
DISEAddInEventsA collection of AddInEvent objects.
DISEAddInEventsExA collection of AddInEvent objects.
DISEApplicationEventsFires application events.
DISEApplicationWindowEventsProvides access to the application window events.
DISEAssemblyFamilyEvents
DISEAssemblyRecomputeEventsRepresents a collection of assembly recompute events.
DISECommandProvides interfaces for Visual Basic users to capture user input to process Solid Edge events.
DISECommandBarButtonEventsA collection of CommandBarButtonEvent objects.
DISECommandEvents
DISECommandWindowEvents
DISEDocumentEventsFires document events.
DISEFileUIEventsFires file user interface events.
DISEhDCDisplayEventsFires display events.
DISEMouseProvides interfaces for Visual Basic users to capture user input to process Solid Edge mouse events.
DISEMouseEvents
DISEViewEventsFires view events.
DisplayEventsFires display events.
DividePartEventsRepresents a collection of DividedPart-based events.
DocumentEventsFires document events.
DocumentsA collection of Document objects.
DraftBendTableEventsContains the AfterUpdate event.
DrawingViewEventsRepresents a collection of DrawingView events.
EnvironmentThe menus and accelerators to a Window object. Defines the set of commands that can be run while a window associated to an environment is active.
EnvironmentsA collection of Environment objects.
FaceStyleAn object in the FaceStyles collection.
FaceStylesA collection of FaceStyle objects.
FamilyOfPartsEventsRepresents a collection of Family of Parts events.
FamilyOfPartsExEvents
FeatureLibraryEventsRepresents a collection of Feature Library-based events.
FileUIEventsFires file user interface events.
FillStyleDefines the fill characteristics of an enclosed object.
FillStylesA collection of FillStyle objects.
GLDisplayEventsRepresents a collection of GLDisplay events.
HatchPatternStyleA vector pattern that is used to fill a closed boundary.
HatchPatternStylesA collection of HatchPatternStyle objects.
HighlightSetRepresents an occurrence of a Highlight set in Assembly, Draft, Part, or Sheet Metal documents.
HighlightSetsA collection of HighLightSet objects.
InsightInsight Automation Object
InterpartLink
InterpartLinks
ISEAcceleratorRepresents a collection of KeyBinding objects.
ISEAcceleratorsRepresents a collection of Accelerator objects.
ISEAddInA control that represents a command added to Solid Edge through the AddIn interface.
ISEAddInEdgeBarEvents
ISEAddInEdgeBarEventsEx
ISEAddInEventsA collection of AddInEvent objects.
ISEAddInEventsExA collection of AddInEvent objects.
ISEAddInExA control that represents a command added to Solid Edge through the AddIn interface.
ISEAddInsA collection of AddIn objects.
ISEApplicationEventsFires application events.
ISEApplicationV8AfterDocumentOpenEventFires document open event
ISEApplicationWindowEventsProvides access to the application window events.
ISEAssemblyFamilyEvents
ISEAssemblyRecomputeEventsRepresents a collection of assembly recompute events.
ISEBlockTableEventsContains the AfterUpdate event.
ISECommandProvides interfaces for Visual Basic users to capture user input to process Solid Edge events.
ISECommandBarRepresents all menus, toolbars, and pop-up menus in Solid Edge.
ISECommandBarButtonRepresents buttons on toolbars and menus.
ISECommandBarButtonEventsA collection of CommandBarButtonEvent objects.
ISECommandBarControlContains the properties and methods that are applicable to both CommandBarButton and CommandBarPopup objects.
ISECommandBarControlsContains all of the buttons and pop-ups on a specific command bar.
ISECommandBarPopupRepresents pop-ups on toolbars and menus.
ISECommandBarsA collection of all of the command bars within a specific environment.
ISECommandCategoriesA collection of command categories
ISECommandCategory
ISECommandEvents
ISECommandExProvides interfaces for Visual Basic users to capture user input to process Solid Edge events.
ISECommandInfo
ISECommandWindowEvents
ISEConnectorTableEventsContains the AfterUpdate event.
ISEDividePartEventsRepresents a collection of DividedPart-based events.
ISEDocumentEventsFires document events.
ISEDraftBendTableEventsContains the AfterUpdate event.
ISEDrawingViewEventsRepresents a collection of DrawingView events.
ISEDynamicEditEventsFires dynamic edit events.
ISEECEventsSEEC Events
ISEFamilyOfPartsEventsRepresents a collection of Family of Parts events.
ISEFamilyOfPartsExEvents
ISEFeatureLibraryEventsRepresents a collection of Feature Library-based events.
ISEFileUIEventsFires file user interface events.
ISEhDCDisplayEventsFires display events.
ISEIGLDisplayEventsRepresents a collection of GLDisplay events.
ISEKeyBindingProvides information about an existing key binding.
ISELocateFilterEvents
ISEModelRecomputeEventsFires model recompute events.
ISEMouseProvides interfaces for Visual Basic users to capture user input to process Solid Edge mouse events.
ISEMouseEvents
ISEMouseEx
ISENewFileUIEvents
ISEPartsListEventsContains the AfterUpdate event.
ISERenderEventsRepresents a collection of rendering events.
ISEShortCutMenuEventsEvent set for short-cut menu manipulations
ISEViewEventsFires view events.
ISolidEdgeAddInProvides an interface for add-ins to implement for Solid Edge to connect to them.
ISolidEdgeBar
ISolidEdgeBarEx
ISolidEdgeBarEx2
ISolidEdgeCommandBar
ISolidEdgeRibbonBar
ISolidEdgeRibbonBarEx
KeyBindingProvides information about an existing key binding.
LayerAn object in the Layers collection object.
LayersA collection of Layer objects.
LinearStyleConsists of the information required to represent a line graphically.
LinearStylesA collection of LinearStyle objects.
MatTable
ModelRecomputeEventsFires model recompute events.
MouseProvides interfaces for Visual Basic users to capture user input to process Solid Edge mouse events.
NewFileUIEvents
PartsListEventsContains the AfterUpdate event.
PropertiesA collection of Property objects.
PropertyA user-defined document attribute.
PropertySetsA collection of PropertySet objects.
QueryObjectsRepresents the collection of objects returned by a query.
RadialMenu
ReferenceRepresents an object that references another object (a part or assembly, for example).
RenderEventsRepresents a collection of rendering events.
RibbonBar
RibbonBarControl
RibbonBarControls
RibbonBarGroup
RibbonBarGroups
RibbonBars
RibbonBarTab
RibbonBarTabs
RibbonBarTheme
RibbonBarThemes
RoutingSlipDistributes a document to recipients either at one time or sequentially.
SectionViewAutomation object for a section view in a Part or Assembly document.
SectionViewsCollection of section views.
SEECEventsSEEC Events
SEGenericCollectionRepresents a collection of AttachedProperty objects.
SelectSetA temporary grouping of one or more selected objects.
SensorRepresents an occurrence of a Sensor feature in an Assembly document, a Part document, or a Sheet Metal document.
SensorsA collection of Sensor objects.
SheetMetalSensorsRepresents a collection of sensors on a SheetMetalDocument.
ShortcutMenuEvents
SolidEdgeDocument
SolidEdgeInsightXTInsightXT Automation Object.
SolidEdgeTCE
SummaryInfoContains information about a document.
SwitchWindowCust
Symbol2dAllows you to review or manipulate the symbol geometry, the attachment between a symbol and a source document, and the user property.
SymbolPropertiesA collection of SymbolProperty objects.
SymbolsA collection of Symbol objects.
TextCharStyleContains a set of character characteristics that can be applied as a set to the active text.
TextCharStylesA collection of TextCharStyle objects.
TextStyleContains characteristics to apply to the active paragraph.
TextStylesA collection of TextStyle objects.
UnitOfMeasureThe UnitOfMeasure object allows you to set and return the unit type and precision for each category, depending on the index of the unit.
UnitsOfMeasureAllows you to convert internal measurement units to user-specified measurement units.
variableAssociates a name with a numeric value.
VariableListA list of Variable objects returned from a query.
VariablesA collection of Variable objects.
ViewProvides methods and properties that allow you to manipulate Solid Edge window views.
ViewEventsFires view events.
ViewStyleContains a collection of properties that control view rendering.
ViewStylesA collection of ViewStyle objects.
WindowProvides support for adjusting the size of the actual viewing area.
WindowsA collection of Window objects.
Public Enumerations
EnumerationDescription
AcceleratorTypeConstants
ApplicationGlobalConstantsApplication global constants
ArrangeWindowsStylesStyles for window arrangement.
AssemblyEventConstantsAssembly Event constants
AttributeTypeConstants
BulkMigrationTypeConstantsBulk Migration Type Constants
CheckInOptions
CommandBarHeaderDialogControlIDs 
CookieDataToGet 
DisplayTypeConstant Display types for a placeholder object.
DocumentAccessDocument Access Constants
DocumentDownloadLevel
DocumentStatusDocument Status Constants
DocumentTypeConstantsDocument Type Constants
eCPDMode 
HatchElementTypeDefines the type of hatch element - Linear or Radial
InsightSPUserRights
KeyPointTypeKeypoint Type Constants
LinksUpdateOptionLinks Update Options
MatTablePropIndexMaterial Property Index Constants
MatTablePropIndexConstantsMaterial Property Index Constants
NotifyOptionNotify Options
ObjectTypeObject Types
OLEInsertionTypeConstantInsertion types for an OLE object into a placeholder.
OLEUpdateOptionConstantUpdate options of the placeholder when source is modified.
OverWriteFilesOption
RadialHatchElementCenterLocationDefines the location of hatch ellipse center
RevisionRuleType
RibbonBarControlSizeThe size of a control.
RibbonBarControlTextThe text style of a control.
RibbonBarInsertModeOperation that is done on the item being inserted.
RouteStatusRoute Status Constants
RouteTypeRoute Type Constants
SeAnalysisModeTypeAnalysis Mode Types
SeAnalysisStateTypeAnalysis State Types
SeAntiAliasLevel
seAssemblyEventConstantsAssembly Event constants
SeBackgroundTypeBackground Types
SeBarPositionSolid Edge CommandBar Positions
SeBarTypeSolid Edge CommandBar Types
SeButtonStateSolid Edge Control Types
SeButtonStyleSolid Edge Button Styles
SeConnectModeSolid Edge AddIn Connect Modes
SeControlTypeSolid Edge Control Types
SectionViewExtentSideExtent side options.
SectionViewProfileSideProfile side options.
SeDisconnectModeSolid Edge AddIn Disconnect Modes
SeFeatureAddFlagSolid Edge Model Recompute, feature add flags
SeFeatureDeleteFlagSolid Edge Model Recompute, feature delete flags
SeFeatureModifyFlagSolid Edge Model Recompute, feature modification flags
SeGradientType
SeHiddenLineMode
SeImageQualityTypeSolid Edge Image Quality Types
SensorDisplayTypeConstantsSensor Display Type constants
SensorOperatorConstantsSensor Operator constants
SensorStatusConstantsSensor Status constants
SensorTypeConstantsSensor Type constants
SensorUpdateMechanismConstantsSensor Update Mechanism constants
SeObjectTypeSolid Edge Object Types
SeRenderModeTypeSolid Edge Render Mode Types
SeSkyboxType
seStyleTypeConstantsStyle types.
SheetMetalSensorFeatureTypeConstants
ShortCutMenuContextConstantsConstants for context of short-cut menu event
SolidEdgeCommandConstantsSolid Edge Command Constants
SPServerTypeSharePoint ServerTypeConstants
StyleUnitsConstantStyle Units Type constant
SurfaceAreaSensorAreaTypeConstantsSensor Surface Area Type - Positive / Negative
SurfaceAreaSensorSelectionTypeConstantsSensor Surface Area Selection Type - Face / Face Chain
SyncOption 
TCESETypes 
TextStyleNumberJustificationConstantsText Number Justification
UnitTypeConstantsUnit Type Constants
UploadType
Send comments on this topic.