Solid Edge Framework Type Library
ApplicationGlobalConstants Enumeration
Description
Application global constants
Members
MemberValueDescription
seApplicationGlobalActivateAllParts66Activate All Parts
seApplicationGlobalAdminFileLocation53AdminFileLocation
seApplicationGlobalANSIInchToleranceFile97ANSI Inch Tolerance File
seApplicationGlobalANSIMetricToleranceFile98ANSI Metric Tolerance File
seApplicationGlobalApplicationDisplay18Application display mode for new windows
seApplicationGlobalApplyActivationOverridesToParts65Apply Activation Overrides To Parts
seApplicationGlobalApplySimplifyOverridesToParts67Apply Simplify Overrides To Parts
seApplicationGlobalApplySimplifyOverridesToSubAssemblies69Apply Simplify Overrides To SubAssemblies
seApplicationGlobalApplyStatusToLinks36Apply Status To Links
seApplicationGlobalAutomaticSave12Automatic Save
seApplicationGlobalAutomaticSaveTime13Automatic Save Time
seApplicationGlobalAutoSharpenLevel110Automatic sharpen level
seApplicationGlobalAvailableRootFolder39Available Root Folder
seApplicationGlobalBaselinedRootFolder44Baselined Root Folder
seApplicationGlobalChangedPartActivation140
seApplicationGlobalCheckInOnClose20Check In On Close
seApplicationGlobalColorActive2The color for active elements
seApplicationGlobalColorBackground3The color for the background
seApplicationGlobalColorConstruction4The color for construction elements
seApplicationGlobalColorDisabled5The color for disabled items
seApplicationGlobalColorFailed6The color for failed items
seApplicationGlobalColorHandle7The color for handles
seApplicationGlobalColorHighlight8The color for highlighted elements
seApplicationGlobalColorLiveSectionCenterline92
seApplicationGlobalColorLiveSectionEdge91
seApplicationGlobalColorLiveSectionOpacity94
seApplicationGlobalColorLiveSectionRegion93
seApplicationGlobalColorManagerCopyIndividualFaceColors58Color Manager Copy Individual Face Colors
seApplicationGlobalColorManagerShowAssemblyStyleOverrides57Color Manager Show Assembly Style Overrides
seApplicationGlobalColorManagerShowPartFaceColors56Color Manager Show Part Face Colors
seApplicationGlobalColorManagerUseIndividualPartStyles55ColorManager Use Individual Part Styles
seApplicationGlobalColorManagerUseToolsOptionsColorSettings54Color Manager Use Tools Options Color Settings
seApplicationGlobalColorProfile9The color for profiles, sketches and layouts
seApplicationGlobalColorRefPlane31Color RefPlane
seApplicationGlobalColorSelected10The color for items in the select set
seApplicationGlobalColorSheet11The color for the sheet
seApplicationGlobalColorSheetTab1138Specifies the first of two alternating colors for the sheet tabs.
seApplicationGlobalColorSheetTab2139Specifies the second of two alternating colors for the sheet tabs.
seApplicationGlobalCommandBarMode105Displays mode in command bar or quick bar.
seApplicationGlobalCurvatureCombDensity34Curvature Comb Density
seApplicationGlobalCurvatureCombMagnitude35Curvature Comb Magnitude
seApplicationGlobalCustomSettingFile63Custom Setting File
seApplicationGlobalDefaultSharpness19Default sharpness for new windows
seApplicationGlobalDisplayArcQuality1Display Arc Quality
seApplicationGlobalDisplayQuality0Display Quality
seApplicationGlobalDisplaySectionCaps15Enable the display of section caps with dynamic sections
seApplicationGlobalDisplayStatistics14Enable display timing statistics in the status bar
seApplicationGlobalDocumentNameFormula88
seApplicationGlobalDynamicTransition17Dynamic view transition smoothness
seApplicationGlobalECORootFolder50ECO Root Folder
seApplicationGlobalECRRootFolder49ECR Root Folder
seApplicationGlobalEnableDynamicTolerance45Enable dynamic tolerancing of facet data
seApplicationGlobalEnableThreadedDisplay30Enable multithreaded displays
seApplicationGlobalHideAllComponents64Hide All Components
seApplicationGlobalHoleSizeFile61Hole Size File
seApplicationGlobalInReviewRootFolder43In Review Root Folder
seApplicationGlobalInsightCacheLocation22Set InsightCacheLocation
seApplicationGlobalInsightFolderMappingFileLocation23Set InsightFolderMappingFileLocation
seApplicationGlobalInWorkRootFolder41Obsolete Root Folder
seApplicationGlobalISOToleranceFile99ISO Tolerance File
seApplicationGlobalLogFilesLocation21Set LogFilesLocation
seApplicationGlobalLookAheadVersion26LookAheadVersion
seApplicationGlobalMakeRevisionsObsolete38Make Revisions Obsolete
seApplicationGlobalObsoleteRootFolder40Obsolete Root Folder
seApplicationGlobalOfflineMode25Set OfflineMode
seApplicationGlobalOnLineHelpLocation144
seApplicationGlobalOpacityRefPlane32Opacity RefPlane
seApplicationGlobalOpenAsReadOnly3DFile89
seApplicationGlobalOpenAsReadOnly3DFile_IndirectFiles95
seApplicationGlobalOpenAsReadOnlyDftFile90
seApplicationGlobalOpenAsReadOnlyDftFile_IndirectFiles96
seApplicationGlobalOverlayColor28The color for visible edge overlay
seApplicationGlobalOverlayColorMode29The color mode for visible edge overlay [1=Absolute, 2=Relative]
seApplicationGlobalPackagedCollaborationRootFolder48Packaged Collaboration Root Folder
seApplicationGlobalPipeThreadfsFile62PipeThreadfsFile
seApplicationGlobalPrereleaseRootFolder47Prerelease Root Folder
seApplicationGlobalReleasedRootFolder42Released Root Folder
seApplicationGlobalRevisionDelimiter33Sets Revision Delimiter
seApplicationGlobalSaveMultiCADDatasettoTC135
seApplicationGlobalSearchScope24Set SearchScope
seApplicationGlobalSectionCurvatureCombDensity141
seApplicationGlobalSectionCurvatureCombMagnitude142
seApplicationGlobalSessionDraftOpenInactive60Draft inactive mode on open (boolean)
seApplicationGlobalSheetTabDisplayInfo136Specifies what information is displayed in the sheet tab : 0 = sheet number; 1 = sheet name; 2 = sheet number and sheet name
seApplicationGlobalSheetTabDisplayInfoSeparator137Specifies the separator string used between the sheet number and sheet name when both are displayed in the sheet tabs.
seApplicationGlobalShowUnitsInValueFields104Shows units of measure in value fields.
seApplicationGlobalSoftwareVHL16Enable software VHL/Disable hardware VHL
seApplicationGlobalStatusBarCmdFinder84Status Bar Command Finder
seApplicationGlobalStatusBarCommonViews78Status Bar Common Views
seApplicationGlobalStatusBarFit73Status Bar Fit
seApplicationGlobalStatusBarLookAtFace77Status Bar Look At Face
seApplicationGlobalStatusBarNamedViews80Status Bar Named View
seApplicationGlobalStatusBarPan74Status Bar Pan
seApplicationGlobalStatusBarPreviousView79Status Bar Previous View
seApplicationGlobalStatusBarRecordVideo145
seApplicationGlobalStatusBarRotateView75Status Bar Rotate View
seApplicationGlobalStatusBarSketchView86Status Bar Sketch View
seApplicationGlobalStatusBarSpinAbout76Status Bar Spin About
seApplicationGlobalStatusBarUploadToYouTube146
seApplicationGlobalStatusBarViewStyles81Status Bar View Styles
seApplicationGlobalStatusBarZoom71Status Bar Zoom
seApplicationGlobalStatusBarZoomArea72Status Bar Zoom Area
seApplicationGlobalStatusBarZoomSlider82Status Bar Zoom Slider
seApplicationGlobalStatusBarZoomTool83Status Bar Zoom Tool
seApplicationGlobalSystemInfo46Retrieve system information [readonly]
seApplicationGlobalTeamcenterFormula87
seApplicationGlobalTeamCenterMode59TeamCenter Mode
seApplicationGlobalTemplateRootFolder51Template Root Folder
seApplicationGlobalUpdateDraft37Update draft files also
seApplicationGlobalUploadOnClose27Upload On Close
seApplicationGlobalUseAllSimplifiedParts68Use All Simplified Parts
seApplicationGlobalUseAllSimplifiedSubAssemblies70Use All Simplified SubAssemblies
seApplicationGlobalUseDetailEnvelopeDisplayAsCircle102Show Detail Envelope as Circle when TRUE.
seApplicationGlobalUseDetailEnvelopeStandard101Use to set the Detail Envelope Standard Constants. Valid values are defined by enum DetailEnvelopeStandardConstants.
seApplicationGlobalUseDimensionStyleElementMapAngularCoordinateDim118
seApplicationGlobalUseDimensionStyleElementMapAngularDim117
seApplicationGlobalUseDimensionStyleElementMapBalloon123
seApplicationGlobalUseDimensionStyleElementMapBHC122
seApplicationGlobalUseDimensionStyleElementMapBlockLabels134
seApplicationGlobalUseDimensionStyleElementMapCallouts124
seApplicationGlobalUseDimensionStyleElementMapCenterline120
seApplicationGlobalUseDimensionStyleElementMapCenterMark121
seApplicationGlobalUseDimensionStyleElementMapChamferDim119
seApplicationGlobalUseDimensionStyleElementMapCircularDiameterDim114
seApplicationGlobalUseDimensionStyleElementMapConnectors126
seApplicationGlobalUseDimensionStyleElementMapCoordinateDim116
seApplicationGlobalUseDimensionStyleElementMapDatumFrames130
seApplicationGlobalUseDimensionStyleElementMapDatumPoints131
seApplicationGlobalUseDimensionStyleElementMapDatumTargets132
seApplicationGlobalUseDimensionStyleElementMapEdgeCondition129
seApplicationGlobalUseDimensionStyleElementMapFCF133
seApplicationGlobalUseDimensionStyleElementMapLeaders125
seApplicationGlobalUseDimensionStyleElementMapLinDim111
seApplicationGlobalUseDimensionStyleElementMapRadialDiameterDim113
seApplicationGlobalUseDimensionStyleElementMapRadialDim112
seApplicationGlobalUseDimensionStyleElementMapSTSymbols127
seApplicationGlobalUseDimensionStyleElementMapSymmetricDiameterDim115
seApplicationGlobalUseDimensionStyleElementMapWeldSymbols128
seApplicationGlobalUseDimensionStyleMapping52Use Dimension Style Mapping
seApplicationGlobalUseDrawingViewShowCroppingEdges103Show cropping edges when TRUE.
seApplicationGlobalUseDrawingViewShowEdgesHiddenTangentEdgesHiddenByOtherParts107Show tangent edges that are hidden by other parts when TRUE.
seApplicationGlobalUseDrawingViewShowEdgesHiddenTangentEdgesSelfHidden106Show the hidden tangent edges when TRUE.
seApplicationGlobalUseISOToleranceTable100Use ISO Tolerance Table when TRUE. Use ANSI Tolerance Table when FALSE.
seApplicationGlobalUseOnLineHelp143
seApplicationGlobalUserType85User Type
seApplicationGlobalZebraFolderMapping109Set ZebraFolderMapping
seApplicationGlobalZebraFormula108
See Also

Solid Edge ST5 - What's New  | Solid Edge ST4 - What's New  | Solid Edge ST3 - What's New  | Solid Edge ST2 - What's New  | Solid Edge ST - What's New  | Solid Edge V20 - What's New  | Solid Edge V19 - What's New  | Solid Edge V18 - What's New  | Solid Edge V18 SP4 - What's New  | Solid Edge V17 - What's New

Send comments on this topic.