Solid Edge Framework Type Library
CommandBarControl Object
Members 
Description
Contains the properties and methods that are applicable to both CommandBarButton and CommandBarPopup objects.
Object Model
CommandBarControl ObjectCommandBar ObjectCommandBarControls CollectionCommandBarControl ObjectEnvironment Object
Remarks
It provides a way to access most of the properties that are associated with either a CommandBarButton or a CommandBarPopup without having to specify an object type.
See Also

CommandBarControl Members

Send comments on this topic.